The QSPI_EDMA module provide a method for QSPI transfer operation based on EDMA. 
 | 
| void  | QSPI_MasterTransferCreateHandleEDMA (QSPI_Type *base, qspi_master_edma_handle_t *psHandle, qspi_edma_transfer_callback_t pfCallback, void *pUserData, DMA_Type *psEdmaBase, edma_channel_t eEdmaTxChannel, edma_channel_t eEdmaRxChannel) | 
|   | Initialize the QUEUEDSPI master EDMA handle.  More...
  | 
|   | 
| status_t  | QSPI_MasterTransferEDMA (qspi_master_edma_handle_t *psHandle, qspi_transfer_t *psXfer) | 
|   | EDMA method of QUEUEDSPI master transfer.  More...
  | 
|   | 
| status_t  | QSPI_MasterTransferGetCountEDMA (qspi_master_edma_handle_t *psHandle, uint16_t *pu16Count) | 
|   | Get the master EDMA transfer count.  More...
  | 
|   | 
| void  | QSPI_MasterTransferAbortEDMA (qspi_master_edma_handle_t *psHandle) | 
|   | Abort a transfer that uses EDMA for master.  More...
  | 
|   | 
| void  | QSPI_SlaveTransferCreateHandleEDMA (QSPI_Type *base, qspi_slave_edma_handle_t *psHandle, qspi_edma_transfer_callback_t pfCallback, void *pUserData, DMA_Type *psEdmaBase, edma_channel_t eEdmaTxChannel, edma_channel_t eEdmaRxChannel) | 
|   | Initialize the QUEUEDSPI slave EDMA handle.  More...
  | 
|   | 
| status_t  | QSPI_SlaveTransferEDMA (qspi_slave_edma_handle_t *handle, qspi_transfer_t *psXfer) | 
|   | EDMA method of QUEUEDSPI slave transfer.  More...
  | 
|   | 
| status_t  | QSPI_SlaveTransferGetCountEDMA (qspi_slave_edma_handle_t *handle, uint16_t *pu16Count) | 
|   | Get the slave EDMA transfer count.  More...
  | 
|   | 
| void  | QSPI_SlaveTransferAbortEDMA (qspi_slave_edma_handle_t *handle) | 
|   | Abort a transfer that uses EDMA for slave.  More...
  | 
|   | 
      
        
          | struct _qspi_master_edma_handle | 
        
      
 
Forward declaration of the _qspi_master_edma_handle typedefs.
 
      
        
          | volatile uint8_t qspi_slave_edma_handle_t::u8State | 
        
      
 
 
      
        
          | uint16_t qspi_slave_edma_handle_t::u16TotalByteCount | 
        
      
 
 
      
        
          | uint16_t qspi_slave_edma_handle_t::u16TxDummyData | 
        
      
 
 
      
        
          | uint16_t qspi_slave_edma_handle_t::u16RxDummyData | 
        
      
 
 
      
        
          | edma_handle_t qspi_slave_edma_handle_t::sTxHandle | 
        
      
 
 
      
        
          | edma_handle_t qspi_slave_edma_handle_t::sRxHandle | 
        
      
 
 
      
        
          | bool qspi_slave_edma_handle_t::bIsTxInProgress | 
        
      
 
 
      
        
          | bool qspi_slave_edma_handle_t::bIsRxInProgress | 
        
      
 
 
      
        
          | void* qspi_slave_edma_handle_t::pUserData | 
        
      
 
 
      
        
          | volatile bool qspi_slave_edma_handle_t::bIsPcsActiveAfterTransfer | 
        
      
 
 
 
 
      
        
          | typedef void(* qspi_edma_transfer_callback_t)(qspi_master_edma_handle_t *psHandle, status_t eCompletionStatus, void *pUserData) | 
        
      
 
- Parameters
 - 
  
    | base | QUEUEDSPI peripheral base address.  | 
    | psHandle | Pointer to the handle for the QUEUEDSPI master.  | 
    | eCompletionStatus | Success or error code describing whether the transfer completed.  | 
    | pUserData | Arbitrary pointer-dataSized value passed from the application.  | 
  
   
 
 
This function initializes the QUEUEDSPI EDMA master handle which can be used for QUEUEDSPI EDMA master transactional APIs. Usually, for a specified QUEUEDSPI instance, call this API once to get the initialized handle.
- Parameters
 - 
  
    | base | QUEUEDSPI peripheral base address.  | 
    | psHandle | QUEUEDSPI handle pointer to qspi_master_edma_handle_t.  | 
    | pfCallback | QUEUEDSPI callback.  | 
    | pUserData | callback function parameter.  | 
    | psEdmaBase | base address for the EDMA  | 
    | eEdmaTxChannel | Channel of the EDMA used for QSPI Tx  | 
    | eEdmaRxChannel | Channel of the EDMA used for QSPI Rx  | 
  
   
 
 
This function transfers data using EDMA. This is a non-blocking function, which returns right away. When all data is transferred, the callback function is called.
: The transfer data size should be even, if the transfer data width is larger than 8.
- Parameters
 - 
  
    | psHandle | pointer to qspi_master_edma_handle_t structure which stores the transfer state.  | 
    | psXfer | pointer to qspi_transfer_t structure.  | 
  
   
- Returns
 - status of status_t. 
 
 
 
      
        
          | status_t QSPI_MasterTransferGetCountEDMA  | 
          ( | 
          qspi_master_edma_handle_t *  | 
          psHandle,  | 
        
        
           | 
           | 
          uint16_t *  | 
          pu16Count  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
- Parameters
 - 
  
    | psHandle | Pointer to the qspi_master_edma_handle_t structure which stores the transfer state.  | 
    | pu16Count | The number of bytes transferred by using the EDMA transaction.  | 
  
   
- Returns
 - status of status_t. 
 
 
 
      
        
          | void QSPI_MasterTransferAbortEDMA  | 
          ( | 
          qspi_master_edma_handle_t *  | 
          psHandle | ) | 
           | 
        
      
 
- Parameters
 - 
  
    | psHandle | Pointer to the qspi_master_edma_handle_t structure which stores the transfer state.  | 
  
   
 
 
This function initializes the QUEUEDSPI EDMA handle which can be used for other QUEUEDSPI transactional APIs. Usually, for a specified QUEUEDSPI instance, call this API once to get the initialized handle.
- Parameters
 - 
  
    | psHandle | QUEUEDSPI handle pointer to qspi_slave_edma_handle_t.  | 
    | pfCallback | QUEUEDSPI callback.  | 
    | pUserData | callback function parameter.  | 
    | psEdmaBase | base address for the EDMA  | 
    | eEdmaTxChannel | Channel of the EDMA used for QSPI Tx  | 
    | eEdmaRxChannel | Channel of the EDMA used for QSPI Rx  | 
  
   
 
 
This function transfers data using EDMA. This is a non-blocking function, which returns right away. When all data is transferred, the callback function is called.
: The transfer data size should be even if the transfer data width is larger than 8.
- Parameters
 - 
  
    | psHandle | pointer to qspi_slave_edma_handle_t structure which stores the transfer state.  | 
    | psXfer | pointer to qspi_transfer_t structure.  | 
  
   
- Returns
 - status of status_t. 
 
 
 
      
        
          | status_t QSPI_SlaveTransferGetCountEDMA  | 
          ( | 
          qspi_slave_edma_handle_t *  | 
          handle,  | 
        
        
           | 
           | 
          uint16_t *  | 
          pu16Count  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
- Parameters
 - 
  
    | base | QUEUEDSPI peripheral base address.  | 
    | psHandle | Pointer to the qspi_slave_edma_handle_t structure which stores the transfer state.  | 
    | pu16Count | The number of bytes transferred by using the EDMA transaction.  | 
  
   
- Returns
 - status of status_t. 
 
 
 
      
        
          | void QSPI_SlaveTransferAbortEDMA  | 
          ( | 
          qspi_slave_edma_handle_t *  | 
          handle | ) | 
           | 
        
      
 
- Parameters
 - 
  
    | psHandle | Pointer to the qspi_slave_edma_handle_t structure which stores the transfer state.  |