![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
This document consists of sections titled with Driver Overview, Data Structures, Enumerations, Functions, etc., each with an overview list and detailed documentation. It is recommended to read the Driver Overview first for it includes a comprehensive description of the peripheral, driver and driver changes. Other sections give detailed information for APIs, enums, macros, etc., for your further reference.
Driver Overview | |
INTC Peripheral and Driver Overview | |
Content including 1) peripheral features; 2) driver design logic and use method; 3) typical use case. | |
The Driver Change Log | |
The current INTC driver version is 2.0.1. | |
Macros | |
#define | INTC_DisableIRQ(x) INTC_SetIRQPriorityLevel(x, 0U) |
Macro to disable the IRQ. More... | |
#define | INTC_PEND_REG_INDEX(x) ((((uint16_t)(x)) - 1U) >> 4U) |
Helper Macro function to extract IRQ pending register index comparing to INTC_IRQP0. More... | |
#define | INTC_PEND_BIT_INDEX(x) ((((uint16_t)(x)) - 1U) & 0x0FU) |
Helper Macro function to extract pending IRQs bit index. More... | |
Typedefs | |
typedef void(* | fast_irq_handler )(void) |
The handle of the fast irq handler function. More... | |
Driver version | |
#define | FSL_INTC_DRIVER_VERSION (MAKE_VERSION(2, 0, 1)) |
INTC driver version 2.0.1. More... | |
Normal Interrupt Interfaces | |
static void | INTC_SetIRQPriorityNum (IRQn_Type eIrq, uint8_t u8PriorityNum) |
Disable IRQ or Enable IRQ with priority. More... | |
static void | INTC_SetVectorBaseAddress (uint32_t u32VectorBaseAddr) |
Set the base address vector table. More... | |
Fast Interrupt Interfaces | |
static void | INTC_SetFastIRQVectorHandler0 (vector_type_t eVector, fast_irq_handler pfHandler) |
Set the IRQ handler for fast IRQ0. More... | |
static void | INTC_SetFastIRQVectorHandler1 (vector_type_t eVector, fast_irq_handler pfHandler) |
Set the IRQ handler for fast IRQ1. More... | |
Interrupt Status Interfaces | |
static uint8_t | INTC_GetIRQPermittedPriorityLevel (void) |
Get IRQ permitted priority levels. More... | |
static bool | INTC_GetPendingIRQ (vector_type_t eVector) |
Check if IRQ is pending for execution. More... | |
static uint16_t | INTC_GetLatestRespondedVectorNumber (void) |
Get the latest responded IRQ's vector number. More... | |
#define FSL_INTC_DRIVER_VERSION (MAKE_VERSION(2, 0, 1)) |
#define INTC_DisableIRQ | ( | x | ) | INTC_SetIRQPriorityLevel(x, 0U) |
#define INTC_PEND_REG_INDEX | ( | x | ) | ((((uint16_t)(x)) - 1U) >> 4U) |
#define INTC_PEND_BIT_INDEX | ( | x | ) | ((((uint16_t)(x)) - 1U) & 0x0FU) |
typedef void(* fast_irq_handler)(void) |
Normally this function should be guarded by: #pragma interrupt fast and #pragma interrupt off.
|
inlinestatic |
There are similar function in fsl_common:
This function is faster and simpler than those in fsl_common. Generally, this function and IRQ functions in fsl_common are either-or, don't use them together for same IRQn type, but feasible that different IRQn type use them simultaneously, for example: It is OK OCCS_IRQn use INTC_SetIRQPriorityLevel, and ADC12_CC1_IRQn use EnableIRQWithPriority. It is NOT OK that OCCS_IRQn use INTC_SetIRQPriorityLevel and EnableIRQWithPriority simultaneously.
eIrq | The IRQ number. |
u8PriorityNum | IRQ interrupt priority number.
|
|
inlinestatic |
The value in INTC_VBA is used as the upper 13 bits of the interrupt vector VAB[20:0].
u32VectorBaseAddr | Vector table base address. The address requires 256 words (512 bytes) aligned. Take the vector table in MC56F83xxx_Vectors.c as example for how to implement this table. |
|
inlinestatic |
The INTC takes the vector address from the appropriate FIVAL0 and FIVAH0 registers, instead of generating an address that is an offset from the vector base address (VBA).
eVector | The vector number. |
pfHandler | Pointer to the fast IRQ handler function, see fast_irq_handler definition for more info. |
|
inlinestatic |
The INTC takes the vector address from the appropriate FIVAL1 and FIVAH1 registers, instead of generating an address that is an offset from the vector base address (VBA).
eVector | The eVector number. |
pfHandler | Pointer to the fast IRQ handler function, see @ ref fast_irq_handler definition for more info. |
|
inlinestatic |
Interrupt exceptions may be nested to allow the servicing of an IRQ with higher priority than the current exception.
The return value indicate the priority level needed for a new IRQ to interrupt the current interrupt being sent to the Core.
0 | Required nested exception priority levels are 0, 1, 2, or 3. |
1 | Required nested exception priority levels are 1, 2, or 3. |
2 | Required nested exception priority levels are 2 or 3. |
3 | Required nested exception priority level is 3. |
|
inlinestatic |
Before the ISR is entered, IRQ is pending. After the ISR is entered, the IRQ is not pending.
eVector | The IRQ vector number. |
True | if interrupt is pending, otherwise return false. |
|
inlinestatic |
It shows the Vector Address Bus used at the time the last IRQ was taken.