The MCUXpresso SDK provides a peripheral driver for the Quad Serial Peripheral Interface (QSPI) module of MCUXpresso SDK devices.
QSPI driver includes functional APIs and EDMA transactional APIs.
Functional APIs are feature/property target low level APIs. Functional APIs can be used for QSPI initialization/configuration/operation for optimization/customization purpose. Using the functional API requires the knowledge of the QSPI peripheral and how to organize functional APIs to meet the application requirements. All functional API use the peripheral base address as the first parameter. QSPI functional operation groups provide the functional API set.
Transactional APIs are transaction target high level APIs. Transactional APIs can be used to enable the peripheral and in the application if the code size and performance of transactional APIs satisfy the requirements. If the code size and performance are a critical requirement, see the transactional API implementation and write a custom code. All transactional APIs use the qspi_handle_t as the first parameter. Initialize the handle by calling the QSPI_TransferTxCreateHandleEDMA() or QSPI_TransferRxCreateHandleEDMA() API.
Transactional APIs support asynchronous transfer. This means that the functions QSPI_TransferSendEDMA() and QSPI_TransferReceiveEDMA() set up EDMA for data transfer. When the transfer completes, the upper layer is notified through a callback function with the kStatus_QSPI_Idle status.
|
|
#define | QSPI_LUT_SEQ(cmd0, pad0, op0, cmd1, pad1, op1) |
| | Macro functions for LUT table.
|
| |
|
#define | QSPI_CMD (0x1U) |
| | Macro for QSPI LUT command.
|
| |
|
#define | QSPI_PAD_1 (0x0U) |
| | Macro for QSPI PAD.
|
| |
|
| enum | _status_t {
kStatus_QSPI_Idle = MAKE_STATUS(kStatusGroup_QSPI, 0),
kStatus_QSPI_Busy = MAKE_STATUS(kStatusGroup_QSPI, 1),
kStatus_QSPI_Error = MAKE_STATUS(kStatusGroup_QSPI, 2)
} |
| | Status structure of QSPI. More...
|
| |
| enum | qspi_read_area_t {
kQSPI_ReadAHB = 0x0U,
kQSPI_ReadIP
} |
| | QSPI read data area, from IP FIFO or AHB buffer. More...
|
| |
| enum | qspi_command_seq_t {
kQSPI_IPSeq = QuadSPI_SPTRCLR_IPPTRC_MASK,
kQSPI_BufferSeq = QuadSPI_SPTRCLR_BFPTRC_MASK
} |
| | QSPI command sequence type. More...
|
| |
| enum | qspi_fifo_t {
kQSPI_TxFifo = QuadSPI_MCR_CLR_TXF_MASK,
kQSPI_RxFifo = QuadSPI_MCR_CLR_RXF_MASK,
kQSPI_AllFifo = QuadSPI_MCR_CLR_TXF_MASK | QuadSPI_MCR_CLR_RXF_MASK
} |
| | QSPI buffer type. More...
|
| |
| enum | qspi_endianness_t {
kQSPI_64BigEndian = 0x0U,
kQSPI_32LittleEndian,
kQSPI_32BigEndian,
kQSPI_64LittleEndian
} |
| | QSPI transfer endianess. More...
|
| |
| enum | _qspi_error_flags {
kQSPI_DataLearningFail = QuadSPI_FR_DLPFF_MASK,
kQSPI_TxBufferFill = QuadSPI_FR_TBFF_MASK,
kQSPI_TxBufferUnderrun = QuadSPI_FR_TBUF_MASK,
kQSPI_IllegalInstruction = QuadSPI_FR_ILLINE_MASK,
kQSPI_RxBufferOverflow = QuadSPI_FR_RBOF_MASK,
kQSPI_RxBufferDrain = QuadSPI_FR_RBDF_MASK,
kQSPI_AHBSequenceError = QuadSPI_FR_ABSEF_MASK,
kQSPI_AHBIllegalTransaction = QuadSPI_FR_AITEF_MASK,
kQSPI_AHBIllegalBurstSize = QuadSPI_FR_AIBSEF_MASK,
kQSPI_AHBBufferOverflow = QuadSPI_FR_ABOF_MASK,
kQSPI_IPCommandUsageError = QuadSPI_FR_IUEF_MASK,
kQSPI_IPCommandTriggerDuringAHBAccess = QuadSPI_FR_IPAEF_MASK,
kQSPI_IPCommandTriggerDuringIPAccess = QuadSPI_FR_IPIEF_MASK,
kQSPI_IPCommandTriggerDuringAHBGrant = QuadSPI_FR_IPGEF_MASK,
kQSPI_IPCommandTransactionFinished = QuadSPI_FR_TFF_MASK,
kQSPI_FlagAll = 0x8C83F8D1U
} |
| | QSPI error flags. More...
|
| |
| enum | _qspi_flags {
kQSPI_DataLearningSamplePoint = QuadSPI_SR_DLPSMP_MASK,
kQSPI_TxBufferFull = QuadSPI_SR_TXFULL_MASK,
kQSPI_TxDMA = QuadSPI_SR_TXDMA_MASK,
kQSPI_TxWatermark = QuadSPI_SR_TXWA_MASK,
kQSPI_TxBufferEnoughData = QuadSPI_SR_TXEDA_MASK,
kQSPI_RxDMA = QuadSPI_SR_RXDMA_MASK,
kQSPI_RxBufferFull = QuadSPI_SR_RXFULL_MASK,
kQSPI_RxWatermark = QuadSPI_SR_RXWE_MASK,
kQSPI_AHB3BufferFull = QuadSPI_SR_AHB3FUL_MASK,
kQSPI_AHB2BufferFull = QuadSPI_SR_AHB2FUL_MASK,
kQSPI_AHB1BufferFull = QuadSPI_SR_AHB1FUL_MASK,
kQSPI_AHB0BufferFull = QuadSPI_SR_AHB0FUL_MASK,
kQSPI_AHB3BufferNotEmpty = QuadSPI_SR_AHB3NE_MASK,
kQSPI_AHB2BufferNotEmpty = QuadSPI_SR_AHB2NE_MASK,
kQSPI_AHB1BufferNotEmpty = QuadSPI_SR_AHB1NE_MASK,
kQSPI_AHB0BufferNotEmpty = QuadSPI_SR_AHB0NE_MASK,
kQSPI_AHBTransactionPending = QuadSPI_SR_AHBTRN_MASK,
kQSPI_AHBCommandPriorityGranted = QuadSPI_SR_AHBGNT_MASK,
kQSPI_AHBAccess = QuadSPI_SR_AHB_ACC_MASK,
kQSPI_IPAccess = QuadSPI_SR_IP_ACC_MASK,
kQSPI_Busy = QuadSPI_SR_BUSY_MASK,
kQSPI_StateAll = 0xEF897FE7U
} |
| | QSPI state bit. More...
|
| |
| enum | _qspi_interrupt_enable {
kQSPI_DataLearningFailInterruptEnable,
kQSPI_TxBufferFillInterruptEnable = QuadSPI_RSER_TBFIE_MASK,
kQSPI_TxBufferUnderrunInterruptEnable = QuadSPI_RSER_TBUIE_MASK,
kQSPI_IllegalInstructionInterruptEnable,
kQSPI_RxBufferOverflowInterruptEnable = QuadSPI_RSER_RBOIE_MASK,
kQSPI_RxBufferDrainInterruptEnable = QuadSPI_RSER_RBDIE_MASK,
kQSPI_AHBSequenceErrorInterruptEnable = QuadSPI_RSER_ABSEIE_MASK,
kQSPI_AHBIllegalTransactionInterruptEnable,
kQSPI_AHBIllegalBurstSizeInterruptEnable,
kQSPI_AHBBufferOverflowInterruptEnable = QuadSPI_RSER_ABOIE_MASK,
kQSPI_IPCommandUsageErrorInterruptEnable = QuadSPI_RSER_IUEIE_MASK,
kQSPI_IPCommandTriggerDuringAHBAccessInterruptEnable,
kQSPI_IPCommandTriggerDuringIPAccessInterruptEnable,
kQSPI_IPCommandTriggerDuringAHBGrantInterruptEnable,
kQSPI_IPCommandTransactionFinishedInterruptEnable,
kQSPI_AllInterruptEnable = 0x8C83F8D1U
} |
| | QSPI interrupt enable. More...
|
| |
| enum | _qspi_dma_enable {
kQSPI_TxBufferFillDMAEnable = QuadSPI_RSER_TBFDE_MASK,
kQSPI_RxBufferDrainDMAEnable = QuadSPI_RSER_RBDDE_MASK,
kQSPI_AllDDMAEnable = QuadSPI_RSER_TBFDE_MASK | QuadSPI_RSER_RBDDE_MASK
} |
| | QSPI DMA request flag. More...
|
| |
| enum | qspi_dqs_phrase_shift_t {
kQSPI_DQSNoPhraseShift = 0x0U,
kQSPI_DQSPhraseShift45Degree,
kQSPI_DQSPhraseShift90Degree,
kQSPI_DQSPhraseShift135Degree
} |
| | Phrase shift number for DQS mode. More...
|
| |
|
| static void | QSPI_SetIPCommandAddress (QuadSPI_Type *base, uint32_t addr) |
| | Sets the IP command address. More...
|
| |
| static void | QSPI_SetIPCommandSize (QuadSPI_Type *base, uint32_t size) |
| | Sets the IP command size. More...
|
| |
| void | QSPI_ExecuteIPCommand (QuadSPI_Type *base, uint32_t index) |
| | Executes IP commands located in LUT table. More...
|
| |
| void | QSPI_ExecuteAHBCommand (QuadSPI_Type *base, uint32_t index) |
| | Executes AHB commands located in LUT table. More...
|
| |
| static void | QSPI_EnableIPParallelMode (QuadSPI_Type *base, bool enable) |
| | Enables/disables the QSPI IP command parallel mode. More...
|
| |
| static void | QSPI_EnableAHBParallelMode (QuadSPI_Type *base, bool enable) |
| | Enables/disables the QSPI AHB command parallel mode. More...
|
| |
| void | QSPI_UpdateLUT (QuadSPI_Type *base, uint32_t index, uint32_t *cmd) |
| | Updates the LUT table. More...
|
| |
| static void | QSPI_ClearFifo (QuadSPI_Type *base, uint32_t mask) |
| | Clears the QSPI FIFO logic. More...
|
| |
| static void | QSPI_ClearCommandSequence (QuadSPI_Type *base, qspi_command_seq_t seq) |
| | @ brief Clears the command sequence for the IP/buffer command. More...
|
| |
| static void | QSPI_EnableDDRMode (QuadSPI_Type *base, bool enable) |
| | Enable or disable DDR mode. More...
|
| |
| void | QSPI_SetReadDataArea (QuadSPI_Type *base, qspi_read_area_t area) |
| | @ brief Set the RX buffer readout area. More...
|
| |
| void | QSPI_WriteBlocking (QuadSPI_Type *base, uint32_t *buffer, size_t size) |
| | Sends a buffer of data bytes using a blocking method. More...
|
| |
| static void | QSPI_WriteData (QuadSPI_Type *base, uint32_t data) |
| | Writes data into FIFO. More...
|
| |
| void | QSPI_ReadBlocking (QuadSPI_Type *base, uint32_t *buffer, size_t size) |
| | Receives a buffer of data bytes using a blocking method. More...
|
| |
| uint32_t | QSPI_ReadData (QuadSPI_Type *base) |
| | Receives data from data FIFO. More...
|
| |
| struct qspi_flash_timing_t |
Data Fields |
|
uint32_t | dataHoldTime |
| | Serial flash data in hold time.
|
| |
|
uint32_t | CSHoldTime |
| | Serial flash CS hold time in terms of serial flash clock cycles.
|
| |
|
uint32_t | CSSetupTime |
| | Serial flash CS setup time in terms of serial flash clock cycles.
|
| |
| uint8_t qspi_config_t::rxWatermark |
| uint32_t qspi_config_t::AHBbufferSize[FSL_FEATURE_QSPI_AHB_BUFFER_COUNT] |
| uint8_t qspi_config_t::AHBbufferMaster[FSL_FEATURE_QSPI_AHB_BUFFER_COUNT] |
| bool qspi_config_t::enableAHBbuffer3AllMaster |
| struct qspi_flash_config_t |
| uint32_t qspi_flash_config_t::dataHoldTime |
| bool qspi_flash_config_t::enableWordAddress |
Data Fields |
|
uint32_t * | data |
| | Pointer to data to transmit.
|
| |
|
size_t | dataSize |
| | Bytes to be transmit.
|
| |
| Enumerator |
|---|
| kStatus_QSPI_Idle |
QSPI is in idle state.
|
| kStatus_QSPI_Busy |
QSPI is busy.
|
| kStatus_QSPI_Error |
Error occurred during QSPI transfer.
|
| Enumerator |
|---|
| kQSPI_ReadAHB |
QSPI read from AHB buffer.
|
| kQSPI_ReadIP |
QSPI read from IP FIFO.
|
| Enumerator |
|---|
| kQSPI_IPSeq |
IP command sequence.
|
| kQSPI_BufferSeq |
Buffer command sequence.
|
| Enumerator |
|---|
| kQSPI_TxFifo |
QSPI Tx FIFO.
|
| kQSPI_RxFifo |
QSPI Rx FIFO.
|
| kQSPI_AllFifo |
QSPI all FIFO, including Tx and Rx.
|
| Enumerator |
|---|
| kQSPI_64BigEndian |
64 bits big endian
|
| kQSPI_32LittleEndian |
32 bit little endian
|
| kQSPI_32BigEndian |
32 bit big endian
|
| kQSPI_64LittleEndian |
64 bit little endian
|
| Enumerator |
|---|
| kQSPI_DataLearningFail |
Data learning pattern failure flag.
|
| kQSPI_TxBufferFill |
Tx buffer fill flag.
|
| kQSPI_TxBufferUnderrun |
Tx buffer underrun flag.
|
| kQSPI_IllegalInstruction |
Illegal instruction error flag.
|
| kQSPI_RxBufferOverflow |
Rx buffer overflow flag.
|
| kQSPI_RxBufferDrain |
Rx buffer drain flag.
|
| kQSPI_AHBSequenceError |
AHB sequence error flag.
|
| kQSPI_AHBIllegalTransaction |
AHB illegal transaction error flag.
|
| kQSPI_AHBIllegalBurstSize |
AHB illegal burst error flag.
|
| kQSPI_AHBBufferOverflow |
AHB buffer overflow flag.
|
| kQSPI_IPCommandUsageError |
IP command usage error flag.
|
| kQSPI_IPCommandTriggerDuringAHBAccess |
IP command trigger during AHB access error.
|
| kQSPI_IPCommandTriggerDuringIPAccess |
IP command trigger cannot be executed.
|
| kQSPI_IPCommandTriggerDuringAHBGrant |
IP command trigger during AHB grant error.
|
| kQSPI_IPCommandTransactionFinished |
IP command transaction finished flag.
|
| kQSPI_FlagAll |
All error flag.
|
| Enumerator |
|---|
| kQSPI_DataLearningSamplePoint |
Data learning sample point.
|
| kQSPI_TxBufferFull |
Tx buffer full flag.
|
| kQSPI_TxDMA |
Tx DMA is requested or running.
|
| kQSPI_TxWatermark |
Tx buffer watermark available.
|
| kQSPI_TxBufferEnoughData |
Tx buffer enough data available.
|
| kQSPI_RxDMA |
Rx DMA is requesting or running.
|
| kQSPI_RxBufferFull |
Rx buffer full.
|
| kQSPI_RxWatermark |
Rx buffer watermark exceeded.
|
| kQSPI_AHB3BufferFull |
AHB buffer 3 full.
|
| kQSPI_AHB2BufferFull |
AHB buffer 2 full.
|
| kQSPI_AHB1BufferFull |
AHB buffer 1 full.
|
| kQSPI_AHB0BufferFull |
AHB buffer 0 full.
|
| kQSPI_AHB3BufferNotEmpty |
AHB buffer 3 not empty.
|
| kQSPI_AHB2BufferNotEmpty |
AHB buffer 2 not empty.
|
| kQSPI_AHB1BufferNotEmpty |
AHB buffer 1 not empty.
|
| kQSPI_AHB0BufferNotEmpty |
AHB buffer 0 not empty.
|
| kQSPI_AHBTransactionPending |
AHB access transaction pending.
|
| kQSPI_AHBCommandPriorityGranted |
AHB command priority granted.
|
| kQSPI_AHBAccess |
AHB access.
|
| kQSPI_IPAccess |
IP access.
|
| kQSPI_Busy |
Module busy.
|
| kQSPI_StateAll |
All flags.
|
| Enumerator |
|---|
| kQSPI_DataLearningFailInterruptEnable |
Data learning pattern failure interrupt enable.
|
| kQSPI_TxBufferFillInterruptEnable |
Tx buffer fill interrupt enable.
|
| kQSPI_TxBufferUnderrunInterruptEnable |
Tx buffer underrun interrupt enable.
|
| kQSPI_IllegalInstructionInterruptEnable |
Illegal instruction error interrupt enable.
|
| kQSPI_RxBufferOverflowInterruptEnable |
Rx buffer overflow interrupt enable.
|
| kQSPI_RxBufferDrainInterruptEnable |
Rx buffer drain interrupt enable.
|
| kQSPI_AHBSequenceErrorInterruptEnable |
AHB sequence error interrupt enable.
|
| kQSPI_AHBIllegalTransactionInterruptEnable |
AHB illegal transaction error interrupt enable.
|
| kQSPI_AHBIllegalBurstSizeInterruptEnable |
AHB illegal burst error interrupt enable.
|
| kQSPI_AHBBufferOverflowInterruptEnable |
AHB buffer overflow interrupt enable.
|
| kQSPI_IPCommandUsageErrorInterruptEnable |
IP command usage error interrupt enable.
|
| kQSPI_IPCommandTriggerDuringAHBAccessInterruptEnable |
IP command trigger during AHB access error.
|
| kQSPI_IPCommandTriggerDuringIPAccessInterruptEnable |
IP command trigger cannot be executed.
|
| kQSPI_IPCommandTriggerDuringAHBGrantInterruptEnable |
IP command trigger during AHB grant error.
|
| kQSPI_IPCommandTransactionFinishedInterruptEnable |
IP command transaction finished interrupt enable.
|
| kQSPI_AllInterruptEnable |
All error interrupt enable.
|
| Enumerator |
|---|
| kQSPI_TxBufferFillDMAEnable |
Tx buffer fill DMA.
|
| kQSPI_RxBufferDrainDMAEnable |
Rx buffer drain DMA.
|
| kQSPI_AllDDMAEnable |
All DMA source.
|
| Enumerator |
|---|
| kQSPI_DQSNoPhraseShift |
No phase shift.
|
| kQSPI_DQSPhraseShift45Degree |
Select 45 degree phase shift.
|
| kQSPI_DQSPhraseShift90Degree |
Select 90 degree phase shift.
|
| kQSPI_DQSPhraseShift135Degree |
Select 135 degree phase shift.
|
| void QSPI_Init |
( |
QuadSPI_Type * |
base, |
|
|
qspi_config_t * |
config, |
|
|
uint32_t |
srcClock_Hz |
|
) |
| |
This function enables the clock for QSPI and also configures the QSPI with the input configure parameters. Users should call this function before any QSPI operations.
- Parameters
-
| base | Pointer to QuadSPI Type. |
| config | QSPI configure structure. |
| srcClock_Hz | QSPI source clock frequency in Hz. |
- Parameters
-
| config | QSPI configuration structure. |
| void QSPI_Deinit |
( |
QuadSPI_Type * |
base | ) |
|
Clears the QSPI state and QSPI module registers.
- Parameters
-
| base | Pointer to QuadSPI Type. |
This function configures the serial flash relevant parameters, such as the size, command, and so on. The flash configuration value cannot have a default value. The user needs to configure it according to the QSPI features.
- Parameters
-
| base | Pointer to QuadSPI Type. |
| config | Flash configuration parameters. |
| void QSPI_SoftwareReset |
( |
QuadSPI_Type * |
base | ) |
|
This function sets the software reset flags for both AHB and buffer domain and resets both AHB buffer and also IP FIFOs.
- Parameters
-
| base | Pointer to QuadSPI Type. |
| static void QSPI_Enable |
( |
QuadSPI_Type * |
base, |
|
|
bool |
enable |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | Pointer to QuadSPI Type. |
| enable | True means enable QSPI, false means disable. |
| static uint32_t QSPI_GetStatusFlags |
( |
QuadSPI_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | Pointer to QuadSPI Type. |
- Returns
- status flag, use status flag to AND _qspi_flags could get the related status.
| static uint32_t QSPI_GetErrorStatusFlags |
( |
QuadSPI_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | Pointer to QuadSPI Type. |
- Returns
- status flag, use status flag to AND _qspi_error_flags could get the related status.
| static void QSPI_ClearErrorFlag |
( |
QuadSPI_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | Pointer to QuadSPI Type. |
| mask | Which kind of QSPI flags to be cleared, a combination of _qspi_error_flags. |
| static void QSPI_EnableInterrupts |
( |
QuadSPI_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | Pointer to QuadSPI Type. |
| mask | QSPI interrupt source. |
| static void QSPI_DisableInterrupts |
( |
QuadSPI_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | Pointer to QuadSPI Type. |
| mask | QSPI interrupt source. |
| static void QSPI_EnableDMA |
( |
QuadSPI_Type * |
base, |
|
|
uint32_t |
mask, |
|
|
bool |
enable |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | Pointer to QuadSPI Type. |
| mask | QSPI DMA source. |
| enable | True means enable DMA, false means disable. |
| static uint32_t QSPI_GetTxDataRegisterAddress |
( |
QuadSPI_Type * |
base | ) |
|
|
inlinestatic |
It is used for DMA operation.
- Parameters
-
| base | Pointer to QuadSPI Type. |
- Returns
- QSPI Tx data register address.
| uint32_t QSPI_GetRxDataRegisterAddress |
( |
QuadSPI_Type * |
base | ) |
|
This function returns the Rx data register address or Rx buffer address according to the Rx read area settings.
- Parameters
-
| base | Pointer to QuadSPI Type. |
- Returns
- QSPI Rx data register address.
| static void QSPI_SetIPCommandAddress |
( |
QuadSPI_Type * |
base, |
|
|
uint32_t |
addr |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | Pointer to QuadSPI Type. |
| addr | IP command address. |
| static void QSPI_SetIPCommandSize |
( |
QuadSPI_Type * |
base, |
|
|
uint32_t |
size |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | Pointer to QuadSPI Type. |
| size | IP command size. |
| void QSPI_ExecuteIPCommand |
( |
QuadSPI_Type * |
base, |
|
|
uint32_t |
index |
|
) |
| |
- Parameters
-
| base | Pointer to QuadSPI Type. |
| index | IP command located in which LUT table index. |
| void QSPI_ExecuteAHBCommand |
( |
QuadSPI_Type * |
base, |
|
|
uint32_t |
index |
|
) |
| |
- Parameters
-
| base | Pointer to QuadSPI Type. |
| index | AHB command located in which LUT table index. |
| static void QSPI_EnableIPParallelMode |
( |
QuadSPI_Type * |
base, |
|
|
bool |
enable |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | Pointer to QuadSPI Type. |
| enable | True means enable parallel mode, false means disable parallel mode. |
| static void QSPI_EnableAHBParallelMode |
( |
QuadSPI_Type * |
base, |
|
|
bool |
enable |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | Pointer to QuadSPI Type. |
| enable | True means enable parallel mode, false means disable parallel mode. |
| void QSPI_UpdateLUT |
( |
QuadSPI_Type * |
base, |
|
|
uint32_t |
index, |
|
|
uint32_t * |
cmd |
|
) |
| |
- Parameters
-
| base | Pointer to QuadSPI Type. |
| index | Which LUT index needs to be located. It should be an integer divided by 4. |
| cmd | Command sequence array. |
| static void QSPI_ClearFifo |
( |
QuadSPI_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | Pointer to QuadSPI Type. |
| mask | Which kind of QSPI FIFO to be cleared. |
This function can reset the command sequence.
- Parameters
-
| base | QSPI base address. |
| seq | Which command sequence need to reset, IP command, buffer command or both. |
| static void QSPI_EnableDDRMode |
( |
QuadSPI_Type * |
base, |
|
|
bool |
enable |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | QSPI base pointer |
| eanble | True means enable DDR mode, false means disable DDR mode. |
This function can set the RX buffer readout, from AHB bus or IP Bus.
- Parameters
-
| base | QSPI base address. |
| area | QSPI Rx buffer readout area. AHB bus buffer or IP bus buffer. |
| void QSPI_WriteBlocking |
( |
QuadSPI_Type * |
base, |
|
|
uint32_t * |
buffer, |
|
|
size_t |
size |
|
) |
| |
- Note
- This function blocks via polling until all bytes have been sent.
- Parameters
-
| base | QSPI base pointer |
| buffer | The data bytes to send |
| size | The number of data bytes to send |
| static void QSPI_WriteData |
( |
QuadSPI_Type * |
base, |
|
|
uint32_t |
data |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | QSPI base pointer |
| data | The data bytes to send |
| void QSPI_ReadBlocking |
( |
QuadSPI_Type * |
base, |
|
|
uint32_t * |
buffer, |
|
|
size_t |
size |
|
) |
| |
- Note
- This function blocks via polling until all bytes have been sent. Users shall notice that this receive size shall not bigger than 64 bytes. As this interface is used to read flash status registers. For flash contents read, please use AHB bus read, this is much more efficiency.
- Parameters
-
| base | QSPI base pointer |
| buffer | The data bytes to send |
| size | The number of data bytes to receive |
| uint32_t QSPI_ReadData |
( |
QuadSPI_Type * |
base | ) |
|
- Parameters
-
- Returns
- The data in the FIFO.
| static void QSPI_TransferSendBlocking |
( |
QuadSPI_Type * |
base, |
|
|
qspi_transfer_t * |
xfer |
|
) |
| |
|
inlinestatic |
This function writes a continuous data to the QSPI transmit FIFO. This function is a block function and can return only when finished. This function uses polling methods.
- Parameters
-
| base | Pointer to QuadSPI Type. |
| xfer | QSPI transfer structure. |
| static void QSPI_TransferReceiveBlocking |
( |
QuadSPI_Type * |
base, |
|
|
qspi_transfer_t * |
xfer |
|
) |
| |
|
inlinestatic |
This function reads continuous data from the QSPI receive buffer/FIFO. This function is a blocking function and can return only when finished. This function uses polling methods. Users shall notice that this receive size shall not bigger than 64 bytes. As this interface is used to read flash status registers. For flash contents read, please use AHB bus read, this is much more efficiency.
- Parameters
-
| base | Pointer to QuadSPI Type. |
| xfer | QSPI transfer structure. |