![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
| struct | qspi_edma_handle_t |
| QSPI DMA transfer handle, users should not touch the content of the handle. More... | |
Typedefs | |
| typedef void(* | qspi_edma_callback_t )(QuadSPI_Type *base, qspi_edma_handle_t *handle, status_t status, void *userData) |
| QSPI eDMA transfer callback function for finish and error. | |
eDMA Transactional | |
| void | QSPI_TransferTxCreateHandleEDMA (QuadSPI_Type *base, qspi_edma_handle_t *handle, qspi_edma_callback_t callback, void *userData, edma_handle_t *dmaHandle) |
| Initializes the QSPI handle for send which is used in transactional functions and set the callback. More... | |
| void | QSPI_TransferRxCreateHandleEDMA (QuadSPI_Type *base, qspi_edma_handle_t *handle, qspi_edma_callback_t callback, void *userData, edma_handle_t *dmaHandle) |
| Initializes the QSPI handle for receive which is used in transactional functions and set the callback. More... | |
| status_t | QSPI_TransferSendEDMA (QuadSPI_Type *base, qspi_edma_handle_t *handle, qspi_transfer_t *xfer) |
| Transfers QSPI data using an eDMA non-blocking method. More... | |
| status_t | QSPI_TransferReceiveEDMA (QuadSPI_Type *base, qspi_edma_handle_t *handle, qspi_transfer_t *xfer) |
| Receives data using an eDMA non-blocking method. More... | |
| void | QSPI_TransferAbortSendEDMA (QuadSPI_Type *base, qspi_edma_handle_t *handle) |
| Aborts the sent data using eDMA. More... | |
| void | QSPI_TransferAbortReceiveEDMA (QuadSPI_Type *base, qspi_edma_handle_t *handle) |
| Aborts the receive data using eDMA. More... | |
| status_t | QSPI_TransferGetSendCountEDMA (QuadSPI_Type *base, qspi_edma_handle_t *handle, size_t *count) |
| Gets the transferred counts of send. More... | |
| status_t | QSPI_TransferGetReceiveCountEDMA (QuadSPI_Type *base, qspi_edma_handle_t *handle, size_t *count) |
| Gets the status of the receive transfer. More... | |
| struct _qspi_edma_handle |
Data Fields | |
| edma_handle_t * | dmaHandle |
| eDMA handler for QSPI send | |
| size_t | transferSize |
| Bytes need to transfer. More... | |
| uint8_t | nbytes |
| eDMA minor byte transfer count initially configured. More... | |
| uint8_t | count |
| The transfer data count in a DMA request. | |
| uint32_t | state |
| Internal state for QSPI eDMA transfer. | |
| qspi_edma_callback_t | callback |
| Callback for users while transfer finish or error occurred. | |
| void * | userData |
| User callback parameter. | |
| size_t qspi_edma_handle_t::transferSize |
| uint8_t qspi_edma_handle_t::nbytes |
| void QSPI_TransferTxCreateHandleEDMA | ( | QuadSPI_Type * | base, |
| qspi_edma_handle_t * | handle, | ||
| qspi_edma_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | dmaHandle | ||
| ) |
| base | QSPI peripheral base address |
| handle | Pointer to qspi_edma_handle_t structure |
| callback | QSPI callback, NULL means no callback. |
| userData | User callback function data. |
| rxDmaHandle | User requested eDMA handle for eDMA transfer |
| void QSPI_TransferRxCreateHandleEDMA | ( | QuadSPI_Type * | base, |
| qspi_edma_handle_t * | handle, | ||
| qspi_edma_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | dmaHandle | ||
| ) |
| base | QSPI peripheral base address |
| handle | Pointer to qspi_edma_handle_t structure |
| callback | QSPI callback, NULL means no callback. |
| userData | User callback function data. |
| rxDmaHandle | User requested eDMA handle for eDMA transfer |
| status_t QSPI_TransferSendEDMA | ( | QuadSPI_Type * | base, |
| qspi_edma_handle_t * | handle, | ||
| qspi_transfer_t * | xfer | ||
| ) |
This function writes data to the QSPI transmit FIFO. This function is non-blocking.
| base | Pointer to QuadSPI Type. |
| handle | Pointer to qspi_edma_handle_t structure |
| xfer | QSPI transfer structure. |
| status_t QSPI_TransferReceiveEDMA | ( | QuadSPI_Type * | base, |
| qspi_edma_handle_t * | handle, | ||
| qspi_transfer_t * | xfer | ||
| ) |
This function receive data from the QSPI receive buffer/FIFO. This function is non-blocking. Users shall notice that this receive size shall not bigger than 64 bytes. As this interface is used to read flash status registers. For flash contents read, please use AHB bus read, this is much more efficiency.
| base | Pointer to QuadSPI Type. |
| handle | Pointer to qspi_edma_handle_t structure |
| xfer | QSPI transfer structure. |
| void QSPI_TransferAbortSendEDMA | ( | QuadSPI_Type * | base, |
| qspi_edma_handle_t * | handle | ||
| ) |
This function aborts the sent data using eDMA.
| base | QSPI peripheral base address. |
| handle | Pointer to qspi_edma_handle_t structure |
| void QSPI_TransferAbortReceiveEDMA | ( | QuadSPI_Type * | base, |
| qspi_edma_handle_t * | handle | ||
| ) |
This function abort receive data which using eDMA.
| base | QSPI peripheral base address. |
| handle | Pointer to qspi_edma_handle_t structure |
| status_t QSPI_TransferGetSendCountEDMA | ( | QuadSPI_Type * | base, |
| qspi_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
| base | Pointer to QuadSPI Type. |
| handle | Pointer to qspi_edma_handle_t structure. |
| count | Bytes sent. |
| kStatus_Success | Succeed get the transfer count. |
| kStatus_NoTransferInProgress | There is not a non-blocking transaction currently in progress. |
| status_t QSPI_TransferGetReceiveCountEDMA | ( | QuadSPI_Type * | base, |
| qspi_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
| base | Pointer to QuadSPI Type. |
| handle | Pointer to qspi_edma_handle_t structure |
| count | Bytes received. |
| kStatus_Success | Succeed get the transfer count. |
| kStatus_NoTransferInProgress | There is not a non-blocking transaction currently in progress. |