![]() |
MCUXpresso SDK API Reference Manual
Rev 2.11.1
NXP Semiconductors
|
This section describes the programming interface of the CAAM PKHA driver.
Data Structures | |
| struct | caam_pkha_ecc_point_t |
| PKHA ECC point structure. More... | |
Enumerations | |
| enum | caam_pkha_timing_t { kCAAM_PKHA_NoTimingEqualized = 0U, kCAAM_PKHA_TimingEqualized = 1U } |
| Use of timing equalized version of a PKHA function. More... | |
| enum | caam_pkha_f2m_t { kCAAM_PKHA_IntegerArith = 0U, kCAAM_PKHA_F2mArith = 1U } |
| Integer vs binary polynomial arithmetic selection. More... | |
| enum | caam_pkha_montgomery_form_t { kCAAM_PKHA_NormalValue = 0U, kCAAM_PKHA_MontgomeryFormat = 1U } |
| Montgomery or normal PKHA input format. More... | |
Functions | |
| status_t | CAAM_PKHA_NormalToMontgomery (CAAM_Type *base, caam_handle_t *handle, const uint8_t *N, size_t sizeN, uint8_t *A, size_t *sizeA, uint8_t *B, size_t *sizeB, uint8_t *R2, size_t *sizeR2, caam_pkha_timing_t equalTime, caam_pkha_f2m_t arithType) |
| Converts from integer to Montgomery format. More... | |
| status_t | CAAM_PKHA_MontgomeryToNormal (CAAM_Type *base, caam_handle_t *handle, const uint8_t *N, size_t sizeN, uint8_t *A, size_t *sizeA, uint8_t *B, size_t *sizeB, caam_pkha_timing_t equalTime, caam_pkha_f2m_t arithType) |
| Converts from Montgomery format to int. More... | |
| status_t | CAAM_PKHA_ModAdd (CAAM_Type *base, caam_handle_t *handle, const uint8_t *A, size_t sizeA, const uint8_t *B, size_t sizeB, const uint8_t *N, size_t sizeN, uint8_t *result, size_t *resultSize, caam_pkha_f2m_t arithType) |
| Performs modular addition - (A + B) mod N. More... | |
| status_t | CAAM_PKHA_ModSub1 (CAAM_Type *base, caam_handle_t *handle, const uint8_t *A, size_t sizeA, const uint8_t *B, size_t sizeB, const uint8_t *N, size_t sizeN, uint8_t *result, size_t *resultSize) |
| Performs modular subtraction - (A - B) mod N. More... | |
| status_t | CAAM_PKHA_ModSub2 (CAAM_Type *base, caam_handle_t *handle, const uint8_t *A, size_t sizeA, const uint8_t *B, size_t sizeB, const uint8_t *N, size_t sizeN, uint8_t *result, size_t *resultSize) |
| Performs modular subtraction - (B - A) mod N. More... | |
| status_t | CAAM_PKHA_ModMul (CAAM_Type *base, caam_handle_t *handle, const uint8_t *A, size_t sizeA, const uint8_t *B, size_t sizeB, const uint8_t *N, size_t sizeN, uint8_t *result, size_t *resultSize, caam_pkha_f2m_t arithType, caam_pkha_montgomery_form_t montIn, caam_pkha_montgomery_form_t montOut, caam_pkha_timing_t equalTime) |
| Performs modular multiplication - (A x B) mod N. More... | |
| status_t | CAAM_PKHA_ModExp (CAAM_Type *base, caam_handle_t *handle, const uint8_t *A, size_t sizeA, const uint8_t *N, size_t sizeN, const uint8_t *E, size_t sizeE, uint8_t *result, size_t *resultSize, caam_pkha_f2m_t arithType, caam_pkha_montgomery_form_t montIn, caam_pkha_timing_t equalTime) |
| Performs modular exponentiation - (A^E) mod N. More... | |
| status_t | CAAM_PKHA_ModRed (CAAM_Type *base, caam_handle_t *handle, const uint8_t *A, size_t sizeA, const uint8_t *N, size_t sizeN, uint8_t *result, size_t *resultSize, caam_pkha_f2m_t arithType) |
| Performs modular reduction - (A) mod N. More... | |
| status_t | CAAM_PKHA_ModInv (CAAM_Type *base, caam_handle_t *handle, const uint8_t *A, size_t sizeA, const uint8_t *N, size_t sizeN, uint8_t *result, size_t *resultSize, caam_pkha_f2m_t arithType) |
| Performs modular inversion - (A^-1) mod N. More... | |
| status_t | CAAM_PKHA_ModR2 (CAAM_Type *base, caam_handle_t *handle, const uint8_t *N, size_t sizeN, uint8_t *result, size_t *resultSize, caam_pkha_f2m_t arithType) |
| Computes integer Montgomery factor R^2 mod N. More... | |
| status_t | CAAM_PKHA_ModGcd (CAAM_Type *base, caam_handle_t *handle, const uint8_t *A, size_t sizeA, const uint8_t *N, size_t sizeN, uint8_t *result, size_t *resultSize, caam_pkha_f2m_t arithType) |
| Calculates the greatest common divisor - GCD (A, N). More... | |
| status_t | CAAM_PKHA_PrimalityTest (CAAM_Type *base, caam_handle_t *handle, const uint8_t *A, size_t sizeA, const uint8_t *B, size_t sizeB, const uint8_t *N, size_t sizeN, bool *res) |
| Executes Miller-Rabin primality test. More... | |
| status_t | CAAM_PKHA_ECC_PointAdd (CAAM_Type *base, caam_handle_t *handle, const caam_pkha_ecc_point_t *A, const caam_pkha_ecc_point_t *B, const uint8_t *N, const uint8_t *R2modN, const uint8_t *aCurveParam, const uint8_t *bCurveParam, size_t size, caam_pkha_f2m_t arithType, caam_pkha_ecc_point_t *result) |
| Adds elliptic curve points - A + B. More... | |
| status_t | CAAM_PKHA_ECC_PointDouble (CAAM_Type *base, caam_handle_t *handle, const caam_pkha_ecc_point_t *B, const uint8_t *N, const uint8_t *aCurveParam, const uint8_t *bCurveParam, size_t size, caam_pkha_f2m_t arithType, caam_pkha_ecc_point_t *result) |
| Doubles elliptic curve points - B + B. More... | |
| status_t | CAAM_PKHA_ECC_PointMul (CAAM_Type *base, caam_handle_t *handle, const caam_pkha_ecc_point_t *A, const uint8_t *E, size_t sizeE, const uint8_t *N, const uint8_t *R2modN, const uint8_t *aCurveParam, const uint8_t *bCurveParam, size_t size, caam_pkha_timing_t equalTime, caam_pkha_f2m_t arithType, caam_pkha_ecc_point_t *result) |
| Multiplies an elliptic curve point by a scalar - E x (A0, A1). More... | |
| struct caam_pkha_ecc_point_t |
| enum caam_pkha_timing_t |
| enum caam_pkha_f2m_t |
| status_t CAAM_PKHA_NormalToMontgomery | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | N, | ||
| size_t | sizeN, | ||
| uint8_t * | A, | ||
| size_t * | sizeA, | ||
| uint8_t * | B, | ||
| size_t * | sizeB, | ||
| uint8_t * | R2, | ||
| size_t * | sizeR2, | ||
| caam_pkha_timing_t | equalTime, | ||
| caam_pkha_f2m_t | arithType | ||
| ) |
This function computes R2 mod N and optionally converts A or B into Montgomery format of A or B.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| N | modulus | |
| sizeN | size of N in bytes | |
| [in,out] | A | The first input in non-Montgomery format. Output Montgomery format of the first input. |
| [in,out] | sizeA | pointer to size variable. On input it holds size of input A in bytes. On output it holds size of Montgomery format of A in bytes. |
| [in,out] | B | Second input in non-Montgomery format. Output Montgomery format of the second input. |
| [in,out] | sizeB | pointer to size variable. On input it holds size of input B in bytes. On output it holds size of Montgomery format of B in bytes. |
| [out] | R2 | Output Montgomery factor R2 mod N. |
| [out] | sizeR2 | pointer to size variable. On output it holds size of Montgomery factor R2 mod N in bytes. |
| equalTime | Run the function time equalized or no timing equalization. | |
| arithType | Type of arithmetic to perform (integer or F2m) |
| status_t CAAM_PKHA_MontgomeryToNormal | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | N, | ||
| size_t | sizeN, | ||
| uint8_t * | A, | ||
| size_t * | sizeA, | ||
| uint8_t * | B, | ||
| size_t * | sizeB, | ||
| caam_pkha_timing_t | equalTime, | ||
| caam_pkha_f2m_t | arithType | ||
| ) |
This function converts Montgomery format of A or B into int A or B.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| N | modulus. | |
| sizeN | size of N modulus in bytes. | |
| [in,out] | A | Input first number in Montgomery format. Output is non-Montgomery format. |
| [in,out] | sizeA | pointer to size variable. On input it holds size of the input A in bytes. On output it holds size of non-Montgomery A in bytes. |
| [in,out] | B | Input first number in Montgomery format. Output is non-Montgomery format. |
| [in,out] | sizeB | pointer to size variable. On input it holds size of the input B in bytes. On output it holds size of non-Montgomery B in bytes. |
| equalTime | Run the function time equalized or no timing equalization. | |
| arithType | Type of arithmetic to perform (integer or F2m) |
| status_t CAAM_PKHA_ModAdd | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | A, | ||
| size_t | sizeA, | ||
| const uint8_t * | B, | ||
| size_t | sizeB, | ||
| const uint8_t * | N, | ||
| size_t | sizeN, | ||
| uint8_t * | result, | ||
| size_t * | resultSize, | ||
| caam_pkha_f2m_t | arithType | ||
| ) |
This function performs modular addition of (A + B) mod N, with either integer or binary polynomial (F2m) inputs. In the F2m form, this function is equivalent to a bitwise XOR and it is functionally the same as subtraction.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| A | first addend (integer or binary polynomial) | |
| sizeA | Size of A in bytes | |
| B | second addend (integer or binary polynomial) | |
| sizeB | Size of B in bytes | |
| N | modulus. | |
| sizeN | Size of N in bytes. | |
| [out] | result | Output array to store result of operation |
| [out] | resultSize | Output size of operation in bytes |
| arithType | Type of arithmetic to perform (integer or F2m) |
| status_t CAAM_PKHA_ModSub1 | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | A, | ||
| size_t | sizeA, | ||
| const uint8_t * | B, | ||
| size_t | sizeB, | ||
| const uint8_t * | N, | ||
| size_t | sizeN, | ||
| uint8_t * | result, | ||
| size_t * | resultSize | ||
| ) |
This function performs modular subtraction of (A - B) mod N with integer inputs.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| A | first addend (integer or binary polynomial) | |
| sizeA | Size of A in bytes | |
| B | second addend (integer or binary polynomial) | |
| sizeB | Size of B in bytes | |
| N | modulus | |
| sizeN | Size of N in bytes | |
| [out] | result | Output array to store result of operation |
| [out] | resultSize | Output size of operation in bytes |
| status_t CAAM_PKHA_ModSub2 | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | A, | ||
| size_t | sizeA, | ||
| const uint8_t * | B, | ||
| size_t | sizeB, | ||
| const uint8_t * | N, | ||
| size_t | sizeN, | ||
| uint8_t * | result, | ||
| size_t * | resultSize | ||
| ) |
This function performs modular subtraction of (B - A) mod N, with integer inputs.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| A | first addend (integer or binary polynomial) | |
| sizeA | Size of A in bytes | |
| B | second addend (integer or binary polynomial) | |
| sizeB | Size of B in bytes | |
| N | modulus | |
| sizeN | Size of N in bytes | |
| [out] | result | Output array to store result of operation |
| [out] | resultSize | Output size of operation in bytes |
| status_t CAAM_PKHA_ModMul | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | A, | ||
| size_t | sizeA, | ||
| const uint8_t * | B, | ||
| size_t | sizeB, | ||
| const uint8_t * | N, | ||
| size_t | sizeN, | ||
| uint8_t * | result, | ||
| size_t * | resultSize, | ||
| caam_pkha_f2m_t | arithType, | ||
| caam_pkha_montgomery_form_t | montIn, | ||
| caam_pkha_montgomery_form_t | montOut, | ||
| caam_pkha_timing_t | equalTime | ||
| ) |
This function performs modular multiplication with either integer or binary polynomial (F2m) inputs. It can optionally specify whether inputs and/or outputs will be in Montgomery form or not.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| A | first addend (integer or binary polynomial) | |
| sizeA | Size of A in bytes | |
| B | second addend (integer or binary polynomial) | |
| sizeB | Size of B in bytes | |
| N | modulus. | |
| sizeN | Size of N in bytes | |
| [out] | result | Output array to store result of operation |
| [out] | resultSize | Output size of operation in bytes |
| arithType | Type of arithmetic to perform (integer or F2m) | |
| montIn | Format of inputs | |
| montOut | Format of output | |
| equalTime | Run the function time equalized or no timing equalization. This argument is ignored for F2m modular multiplication. |
| status_t CAAM_PKHA_ModExp | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | A, | ||
| size_t | sizeA, | ||
| const uint8_t * | N, | ||
| size_t | sizeN, | ||
| const uint8_t * | E, | ||
| size_t | sizeE, | ||
| uint8_t * | result, | ||
| size_t * | resultSize, | ||
| caam_pkha_f2m_t | arithType, | ||
| caam_pkha_montgomery_form_t | montIn, | ||
| caam_pkha_timing_t | equalTime | ||
| ) |
This function performs modular exponentiation with either integer or binary polynomial (F2m) inputs.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| A | first addend (integer or binary polynomial) | |
| sizeA | Size of A in bytes | |
| N | modulus | |
| sizeN | Size of N in bytes | |
| E | exponent | |
| sizeE | Size of E in bytes | |
| [out] | result | Output array to store result of operation |
| [out] | resultSize | Output size of operation in bytes |
| montIn | Format of A input (normal or Montgomery) | |
| arithType | Type of arithmetic to perform (integer or F2m) | |
| equalTime | Run the function time equalized or no timing equalization. |
| status_t CAAM_PKHA_ModRed | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | A, | ||
| size_t | sizeA, | ||
| const uint8_t * | N, | ||
| size_t | sizeN, | ||
| uint8_t * | result, | ||
| size_t * | resultSize, | ||
| caam_pkha_f2m_t | arithType | ||
| ) |
This function performs modular reduction with either integer or binary polynomial (F2m) inputs.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| A | first addend (integer or binary polynomial) | |
| sizeA | Size of A in bytes | |
| N | modulus | |
| sizeN | Size of N in bytes | |
| [out] | result | Output array to store result of operation |
| [out] | resultSize | Output size of operation in bytes |
| arithType | Type of arithmetic to perform (integer or F2m) |
| status_t CAAM_PKHA_ModInv | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | A, | ||
| size_t | sizeA, | ||
| const uint8_t * | N, | ||
| size_t | sizeN, | ||
| uint8_t * | result, | ||
| size_t * | resultSize, | ||
| caam_pkha_f2m_t | arithType | ||
| ) |
This function performs modular inversion with either integer or binary polynomial (F2m) inputs.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| A | first addend (integer or binary polynomial) | |
| sizeA | Size of A in bytes | |
| N | modulus | |
| sizeN | Size of N in bytes | |
| [out] | result | Output array to store result of operation |
| [out] | resultSize | Output size of operation in bytes |
| arithType | Type of arithmetic to perform (integer or F2m) |
| status_t CAAM_PKHA_ModR2 | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | N, | ||
| size_t | sizeN, | ||
| uint8_t * | result, | ||
| size_t * | resultSize, | ||
| caam_pkha_f2m_t | arithType | ||
| ) |
This function computes a constant to assist in converting operands into the Montgomery residue system representation.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| N | modulus | |
| sizeN | Size of N in bytes | |
| [out] | result | Output array to store result of operation |
| [out] | resultSize | Output size of operation in bytes |
| arithType | Type of arithmetic to perform (integer or F2m) |
| status_t CAAM_PKHA_ModGcd | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | A, | ||
| size_t | sizeA, | ||
| const uint8_t * | N, | ||
| size_t | sizeN, | ||
| uint8_t * | result, | ||
| size_t * | resultSize, | ||
| caam_pkha_f2m_t | arithType | ||
| ) |
This function calculates the greatest common divisor of two inputs with either integer or binary polynomial (F2m) inputs.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| A | first value (must be smaller than or equal to N) | |
| sizeA | Size of A in bytes | |
| N | second value (must be non-zero) | |
| sizeN | Size of N in bytes | |
| [out] | result | Output array to store result of operation |
| [out] | resultSize | Output size of operation in bytes |
| arithType | Type of arithmetic to perform (integer or F2m) |
| status_t CAAM_PKHA_PrimalityTest | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | A, | ||
| size_t | sizeA, | ||
| const uint8_t * | B, | ||
| size_t | sizeB, | ||
| const uint8_t * | N, | ||
| size_t | sizeN, | ||
| bool * | res | ||
| ) |
This function calculates whether or not a candidate prime number is likely to be a prime.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| A | initial random seed | |
| sizeA | Size of A in bytes | |
| B | number of trial runs | |
| sizeB | Size of B in bytes | |
| N | candidate prime integer | |
| sizeN | Size of N in bytes | |
| [out] | res | True if the value is likely prime or false otherwise |
| status_t CAAM_PKHA_ECC_PointAdd | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const caam_pkha_ecc_point_t * | A, | ||
| const caam_pkha_ecc_point_t * | B, | ||
| const uint8_t * | N, | ||
| const uint8_t * | R2modN, | ||
| const uint8_t * | aCurveParam, | ||
| const uint8_t * | bCurveParam, | ||
| size_t | size, | ||
| caam_pkha_f2m_t | arithType, | ||
| caam_pkha_ecc_point_t * | result | ||
| ) |
This function performs ECC point addition over a prime field (Fp) or binary field (F2m) using affine coordinates.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| A | Left-hand point | |
| B | Right-hand point | |
| N | Prime modulus of the field | |
| R2modN | NULL (the function computes R2modN internally) or pointer to pre-computed R2modN (obtained from CAAM_PKHA_ModR2() function). | |
| aCurveParam | A parameter from curve equation | |
| bCurveParam | B parameter from curve equation (constant) | |
| size | Size in bytes of curve points and parameters | |
| arithType | Type of arithmetic to perform (integer or F2m) | |
| [out] | result | Result point |
| status_t CAAM_PKHA_ECC_PointDouble | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const caam_pkha_ecc_point_t * | B, | ||
| const uint8_t * | N, | ||
| const uint8_t * | aCurveParam, | ||
| const uint8_t * | bCurveParam, | ||
| size_t | size, | ||
| caam_pkha_f2m_t | arithType, | ||
| caam_pkha_ecc_point_t * | result | ||
| ) |
This function performs ECC point doubling over a prime field (Fp) or binary field (F2m) using affine coordinates.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| B | Point to double | |
| N | Prime modulus of the field | |
| aCurveParam | A parameter from curve equation | |
| bCurveParam | B parameter from curve equation (constant) | |
| size | Size in bytes of curve points and parameters | |
| arithType | Type of arithmetic to perform (integer or F2m) | |
| [out] | result | Result point |
| status_t CAAM_PKHA_ECC_PointMul | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const caam_pkha_ecc_point_t * | A, | ||
| const uint8_t * | E, | ||
| size_t | sizeE, | ||
| const uint8_t * | N, | ||
| const uint8_t * | R2modN, | ||
| const uint8_t * | aCurveParam, | ||
| const uint8_t * | bCurveParam, | ||
| size_t | size, | ||
| caam_pkha_timing_t | equalTime, | ||
| caam_pkha_f2m_t | arithType, | ||
| caam_pkha_ecc_point_t * | result | ||
| ) |
This function performs ECC point multiplication to multiply an ECC point by a scalar integer multiplier over a prime field (Fp) or a binary field (F2m).
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| A | Point as multiplicand | |
| E | Scalar multiple | |
| sizeE | The size of E, in bytes | |
| N | Modulus, a prime number for the Fp field or Irreducible polynomial for F2m field. | |
| R2modN | NULL (the function computes R2modN internally) or pointer to pre-computed R2modN (obtained from CAAM_PKHA_ModR2() function). | |
| aCurveParam | A parameter from curve equation | |
| bCurveParam | B parameter from curve equation (C parameter for operation over F2m). | |
| size | Size in bytes of curve points and parameters | |
| equalTime | Run the function time equalized or no timing equalization. | |
| arithType | Type of arithmetic to perform (integer or F2m) | |
| [out] | result | Result point |