![]() |
MCUXpresso SDK API Reference Manual
Rev 2.11.1
NXP Semiconductors
|
This section describes the programming interface of the CAAM AES driver.
Macros | |
| #define | CAAM_AES_BLOCK_SIZE 16 |
| AES block size in bytes. | |
Functions | |
| status_t | CAAM_AES_EncryptEcb (CAAM_Type *base, caam_handle_t *handle, const uint8_t *plaintext, uint8_t *ciphertext, size_t size, const uint8_t *key, size_t keySize) |
| Encrypts AES using the ECB block mode. More... | |
| status_t | CAAM_AES_DecryptEcb (CAAM_Type *base, caam_handle_t *handle, const uint8_t *ciphertext, uint8_t *plaintext, size_t size, const uint8_t *key, size_t keySize) |
| Decrypts AES using ECB block mode. More... | |
| status_t | CAAM_AES_EncryptCbc (CAAM_Type *base, caam_handle_t *handle, const uint8_t *plaintext, uint8_t *ciphertext, size_t size, const uint8_t iv[CAAM_AES_BLOCK_SIZE], const uint8_t *key, size_t keySize) |
| Encrypts AES using CBC block mode. More... | |
| status_t | CAAM_AES_DecryptCbc (CAAM_Type *base, caam_handle_t *handle, const uint8_t *ciphertext, uint8_t *plaintext, size_t size, const uint8_t iv[CAAM_AES_BLOCK_SIZE], const uint8_t *key, size_t keySize) |
| Decrypts AES using CBC block mode. More... | |
| status_t | CAAM_AES_CryptCtr (CAAM_Type *base, caam_handle_t *handle, const uint8_t *input, uint8_t *output, size_t size, uint8_t counter[CAAM_AES_BLOCK_SIZE], const uint8_t *key, size_t keySize, uint8_t counterlast[CAAM_AES_BLOCK_SIZE], size_t *szLeft) |
| Encrypts or decrypts AES using CTR block mode. More... | |
| status_t | CAAM_AES_EncryptTagCcm (CAAM_Type *base, caam_handle_t *handle, const uint8_t *plaintext, uint8_t *ciphertext, size_t size, const uint8_t *iv, size_t ivSize, const uint8_t *aad, size_t aadSize, const uint8_t *key, size_t keySize, uint8_t *tag, size_t tagSize) |
| Encrypts AES and tags using CCM block mode. More... | |
| status_t | CAAM_AES_DecryptTagCcm (CAAM_Type *base, caam_handle_t *handle, const uint8_t *ciphertext, uint8_t *plaintext, size_t size, const uint8_t *iv, size_t ivSize, const uint8_t *aad, size_t aadSize, const uint8_t *key, size_t keySize, const uint8_t *tag, size_t tagSize) |
| Decrypts AES and authenticates using CCM block mode. More... | |
| status_t | CAAM_AES_EncryptTagGcm (CAAM_Type *base, caam_handle_t *handle, const uint8_t *plaintext, uint8_t *ciphertext, size_t size, const uint8_t *iv, size_t ivSize, const uint8_t *aad, size_t aadSize, const uint8_t *key, size_t keySize, uint8_t *tag, size_t tagSize) |
| Encrypts AES and tags using GCM block mode. More... | |
| status_t | CAAM_AES_DecryptTagGcm (CAAM_Type *base, caam_handle_t *handle, const uint8_t *ciphertext, uint8_t *plaintext, size_t size, const uint8_t *iv, size_t ivSize, const uint8_t *aad, size_t aadSize, const uint8_t *key, size_t keySize, const uint8_t *tag, size_t tagSize) |
| Decrypts AES and authenticates using GCM block mode. More... | |
| status_t CAAM_AES_EncryptEcb | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | plaintext, | ||
| uint8_t * | ciphertext, | ||
| size_t | size, | ||
| const uint8_t * | key, | ||
| size_t | keySize | ||
| ) |
Encrypts AES using the ECB block mode.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| plaintext | Input plain text to encrypt | |
| [out] | ciphertext | Output cipher text |
| size | Size of input and output data in bytes. Must be multiple of 16 bytes. | |
| key | Input key to use for encryption | |
| keySize | Size of the input key, in bytes. Must be 16, 24, or 32. |
| status_t CAAM_AES_DecryptEcb | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | ciphertext, | ||
| uint8_t * | plaintext, | ||
| size_t | size, | ||
| const uint8_t * | key, | ||
| size_t | keySize | ||
| ) |
Decrypts AES using ECB block mode.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| ciphertext | Input cipher text to decrypt | |
| [out] | plaintext | Output plain text |
| size | Size of input and output data in bytes. Must be multiple of 16 bytes. | |
| key | Input key. | |
| keySize | Size of the input key, in bytes. Must be 16, 24, or 32. |
| status_t CAAM_AES_EncryptCbc | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | plaintext, | ||
| uint8_t * | ciphertext, | ||
| size_t | size, | ||
| const uint8_t | iv[CAAM_AES_BLOCK_SIZE], | ||
| const uint8_t * | key, | ||
| size_t | keySize | ||
| ) |
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| plaintext | Input plain text to encrypt | |
| [out] | ciphertext | Output cipher text |
| size | Size of input and output data in bytes. Must be multiple of 16 bytes. | |
| iv | Input initial vector to combine with the first input block. | |
| key | Input key to use for encryption | |
| keySize | Size of the input key, in bytes. Must be 16, 24, or 32. |
| status_t CAAM_AES_DecryptCbc | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | ciphertext, | ||
| uint8_t * | plaintext, | ||
| size_t | size, | ||
| const uint8_t | iv[CAAM_AES_BLOCK_SIZE], | ||
| const uint8_t * | key, | ||
| size_t | keySize | ||
| ) |
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| ciphertext | Input cipher text to decrypt | |
| [out] | plaintext | Output plain text |
| size | Size of input and output data in bytes. Must be multiple of 16 bytes. | |
| iv | Input initial vector to combine with the first input block. | |
| key | Input key to use for decryption | |
| keySize | Size of the input key, in bytes. Must be 16, 24, or 32. |
| status_t CAAM_AES_CryptCtr | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | input, | ||
| uint8_t * | output, | ||
| size_t | size, | ||
| uint8_t | counter[CAAM_AES_BLOCK_SIZE], | ||
| const uint8_t * | key, | ||
| size_t | keySize, | ||
| uint8_t | counterlast[CAAM_AES_BLOCK_SIZE], | ||
| size_t * | szLeft | ||
| ) |
Encrypts or decrypts AES using CTR block mode. AES CTR mode uses only forward AES cipher and same algorithm for encryption and decryption. The only difference between encryption and decryption is that, for encryption, the input argument is plain text and the output argument is cipher text. For decryption, the input argument is cipher text and the output argument is plain text.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| input | Input data for CTR block mode | |
| [out] | output | Output data for CTR block mode |
| size | Size of input and output data in bytes | |
| [in,out] | counter | Input counter (updates on return) |
| key | Input key to use for forward AES cipher | |
| keySize | Size of the input key, in bytes. Must be 16, 24, or 32. | |
| [out] | counterlast | Output cipher of last counter, for chained CTR calls. NULL can be passed if chained calls are not used. |
| [out] | szLeft | Output number of bytes in left unused in counterlast block. NULL can be passed if chained calls are not used. |
| status_t CAAM_AES_EncryptTagCcm | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | plaintext, | ||
| uint8_t * | ciphertext, | ||
| size_t | size, | ||
| const uint8_t * | iv, | ||
| size_t | ivSize, | ||
| const uint8_t * | aad, | ||
| size_t | aadSize, | ||
| const uint8_t * | key, | ||
| size_t | keySize, | ||
| uint8_t * | tag, | ||
| size_t | tagSize | ||
| ) |
Encrypts AES and optionally tags using CCM block mode.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| plaintext | Input plain text to encrypt | |
| [out] | ciphertext | Output cipher text. |
| size | Size of input and output data in bytes. Zero means authentication only. | |
| iv | Nonce | |
| ivSize | Length of the Nonce in bytes. Must be 7, 8, 9, 10, 11, 12, or 13. | |
| aad | Input additional authentication data. Can be NULL if aadSize is zero. | |
| aadSize | Input size in bytes of AAD. Zero means data mode only (authentication skipped). | |
| key | Input key to use for encryption | |
| keySize | Size of the input key, in bytes. Must be 16, 24, or 32. | |
| [out] | tag | Generated output tag. Set to NULL to skip tag processing. |
| tagSize | Input size of the tag to generate, in bytes. Must be 4, 6, 8, 10, 12, 14, or 16. |
| status_t CAAM_AES_DecryptTagCcm | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | ciphertext, | ||
| uint8_t * | plaintext, | ||
| size_t | size, | ||
| const uint8_t * | iv, | ||
| size_t | ivSize, | ||
| const uint8_t * | aad, | ||
| size_t | aadSize, | ||
| const uint8_t * | key, | ||
| size_t | keySize, | ||
| const uint8_t * | tag, | ||
| size_t | tagSize | ||
| ) |
Decrypts AES and optionally authenticates using CCM block mode.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| ciphertext | Input cipher text to decrypt | |
| [out] | plaintext | Output plain text. |
| size | Size of input and output data in bytes. Zero means authentication data only. | |
| iv | Nonce | |
| ivSize | Length of the Nonce in bytes. Must be 7, 8, 9, 10, 11, 12, or 13. | |
| aad | Input additional authentication data. Can be NULL if aadSize is zero. | |
| aadSize | Input size in bytes of AAD. Zero means data mode only (authentication data skipped). | |
| key | Input key to use for decryption | |
| keySize | Size of the input key, in bytes. Must be 16, 24, or 32. | |
| tag | Received tag. Set to NULL to skip tag processing. | |
| tagSize | Input size of the received tag to compare with the computed tag, in bytes. Must be 4, 6, 8, 10, 12, 14, or 16. |
| status_t CAAM_AES_EncryptTagGcm | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | plaintext, | ||
| uint8_t * | ciphertext, | ||
| size_t | size, | ||
| const uint8_t * | iv, | ||
| size_t | ivSize, | ||
| const uint8_t * | aad, | ||
| size_t | aadSize, | ||
| const uint8_t * | key, | ||
| size_t | keySize, | ||
| uint8_t * | tag, | ||
| size_t | tagSize | ||
| ) |
Encrypts AES and optionally tags using GCM block mode. If plaintext is NULL, only the GHASH is calculated and output in the 'tag' field.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| plaintext | Input plain text to encrypt | |
| [out] | ciphertext | Output cipher text. |
| size | Size of input and output data in bytes | |
| iv | Input initial vector | |
| ivSize | Size of the IV | |
| aad | Input additional authentication data | |
| aadSize | Input size in bytes of AAD | |
| key | Input key to use for encryption | |
| keySize | Size of the input key, in bytes. Must be 16, 24, or 32. | |
| [out] | tag | Output hash tag. Set to NULL to skip tag processing. |
| tagSize | Input size of the tag to generate, in bytes. Must be 4,8,12,13,14,15 or 16. |
| status_t CAAM_AES_DecryptTagGcm | ( | CAAM_Type * | base, |
| caam_handle_t * | handle, | ||
| const uint8_t * | ciphertext, | ||
| uint8_t * | plaintext, | ||
| size_t | size, | ||
| const uint8_t * | iv, | ||
| size_t | ivSize, | ||
| const uint8_t * | aad, | ||
| size_t | aadSize, | ||
| const uint8_t * | key, | ||
| size_t | keySize, | ||
| const uint8_t * | tag, | ||
| size_t | tagSize | ||
| ) |
Decrypts AES and optionally authenticates using GCM block mode. If ciphertext is NULL, only the GHASH is calculated and compared with the received GHASH in 'tag' field.
| base | CAAM peripheral base address | |
| handle | Handle used for this request. Specifies jobRing. | |
| ciphertext | Input cipher text to decrypt | |
| [out] | plaintext | Output plain text. |
| size | Size of input and output data in bytes | |
| iv | Input initial vector | |
| ivSize | Size of the IV | |
| aad | Input additional authentication data | |
| aadSize | Input size in bytes of AAD | |
| key | Input key to use for encryption | |
| keySize | Size of the input key, in bytes. Must be 16, 24, or 32. | |
| tag | Input hash tag to compare. Set to NULL to skip tag processing. | |
| tagSize | Input size of the tag, in bytes. Must be 4, 8, 12, 13, 14, 15, or 16. |