MCUXpresso SDK API Reference Manual  Rev 2.12.1
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Spi_gpdma_driver

Overview

Files

file  fsl_spi_gpdma.h
 

Data Structures

struct  spi_gpdma_handle_t
 SPI GPDMA transfer handle, users should not touch the content of the handle. More...
 

Typedefs

typedef void(* spi_gpdma_callback_t )(SPI_Type *base, spi_gpdma_handle_t *handle, status_t status, void *userData)
 SPI GPDMA callback called at the end of transfer. More...
 

Driver version

#define FSL_SPI_GPDMA_DRIVER_VERSION   (MAKE_VERSION(2, 0, 1))
 SPI GPDMA driver version 2.0.1. More...
 

GPDMA Transactional

status_t SPI_MasterTransferCreateHandleGPDMA (SPI_Type *base, spi_gpdma_handle_t *handle, spi_gpdma_callback_t callback, void *userData, gpdma_handle_t *txHandle, gpdma_handle_t *rxHandle)
 Initialize the SPI master GPDMA handle. More...
 
status_t SPI_MasterTransferGPDMA (SPI_Type *base, spi_gpdma_handle_t *handle, spi_transfer_t *xfer)
 Perform a non-blocking SPI transfer using GPDMA. More...
 
void SPI_MasterTransferAbortGPDMA (SPI_Type *base, spi_gpdma_handle_t *handle)
 Abort a SPI transfer using GPDMA. More...
 

Data Structure Documentation

struct _spi_gpdma_handle

Data Fields

volatile bool txInProgress
 Send transfer finished.
 
volatile bool rxInProgress
 Receive transfer finished.
 
gpdma_handle_t * txHandle
 GPDMA handler for SPI send.
 
gpdma_handle_t * rxHandle
 GPDMA handler for SPI receive.
 
uint8_t bytesPerFrame
 Bytes in a frame for SPI transfer.
 
spi_gpdma_callback_t callback
 Callback for SPI GPDMA transfer.
 
void * userData
 User Data for SPI GPDMA callback.
 
uint32_t state
 Internal state of SPI GPDMA transfer.
 
size_t transferSize
 Bytes need to be transfer.
 

Macro Definition Documentation

#define FSL_SPI_GPDMA_DRIVER_VERSION   (MAKE_VERSION(2, 0, 1))

Typedef Documentation

typedef void(* spi_gpdma_callback_t)(SPI_Type *base, spi_gpdma_handle_t *handle, status_t status, void *userData)

Function Documentation

status_t SPI_MasterTransferCreateHandleGPDMA ( SPI_Type *  base,
spi_gpdma_handle_t *  handle,
spi_gpdma_callback_t  callback,
void *  userData,
gpdma_handle_t *  txHandle,
gpdma_handle_t *  rxHandle 
)

This function initializes the SPI master GPDMA handle which can be used for other SPI master transactional APIs. Usually, for a specified SPI instance, user need only call this API once to get the initialized handle.

Parameters
baseSPI peripheral base address.
handleSPI handle pointer.
callbackUser callback function called at the end of a transfer.
userDataUser data for callback.
txHandleGPDMA handle pointer for SPI Tx, the handle shall be static allocated by users.
rxHandleGPDMA handle pointer for SPI Rx, the handle shall be static allocated by users.
status_t SPI_MasterTransferGPDMA ( SPI_Type *  base,
spi_gpdma_handle_t *  handle,
spi_transfer_t *  xfer 
)
Note
This interface returned immediately after transfer initiates, users should call SPI_GetTransferStatus to poll the transfer status to check whether SPI transfer finished.
Parameters
baseSPI peripheral base address.
handleSPI GPDMA handle pointer.
xferPointer to gpdma transfer structure.
Return values
kStatus_SuccessSuccessfully start a transfer.
kStatus_InvalidArgumentInput argument is invalid.
kStatus_SPI_BusySPI is not idle, is running another transfer.
void SPI_MasterTransferAbortGPDMA ( SPI_Type *  base,
spi_gpdma_handle_t *  handle 
)
Parameters
baseSPI peripheral base address.
handleSPI GPDMA handle pointer.