![]() |
MCUXpresso SDK API Reference Manual
Rev 2.12.2
NXP Semiconductors
|
Data Structures | |
| struct | flexcan_edma_handle_t |
| FlexCAN eDMA handle. More... | |
Typedefs | |
| typedef void(* | flexcan_edma_transfer_callback_t )(CAN_Type *base, flexcan_edma_handle_t *handle, status_t status, void *userData) |
| FlexCAN transfer callback function. More... | |
Driver version | |
| #define | FSL_FLEXCAN_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 9, 2)) |
| FlexCAN EDMA driver version. More... | |
eDMA transactional | |
| void | FLEXCAN_TransferCreateHandleEDMA (CAN_Type *base, flexcan_edma_handle_t *handle, flexcan_edma_transfer_callback_t callback, void *userData, edma_handle_t *rxFifoEdmaHandle) |
| Initializes the FlexCAN handle, which is used in transactional functions. More... | |
| void | FLEXCAN_PrepareTransfConfiguration (CAN_Type *base, flexcan_fifo_transfer_t *pFifoXfer, edma_transfer_config_t *pEdmaConfig) |
| Prepares the eDMA transfer configuration for FLEXCAN Legacy RX FIFO. More... | |
| status_t | FLEXCAN_StartTransferDatafromRxFIFO (CAN_Type *base, flexcan_edma_handle_t *handle, edma_transfer_config_t *pEdmaConfig) |
| Start Transfer Data from the FLEXCAN Legacy Rx FIFO using eDMA. More... | |
| status_t | FLEXCAN_TransferReceiveFifoEDMA (CAN_Type *base, flexcan_edma_handle_t *handle, flexcan_fifo_transfer_t *pFifoXfer) |
| Receives the CAN Message from the Legacy Rx FIFO using eDMA. More... | |
| status_t | FLEXCAN_TransferGetReceiveFifoCountEMDA (CAN_Type *base, flexcan_edma_handle_t *handle, size_t *count) |
| Gets the Legacy Rx Fifo transfer status during a interrupt non-blocking receive. More... | |
| void | FLEXCAN_TransferAbortReceiveFifoEDMA (CAN_Type *base, flexcan_edma_handle_t *handle) |
| Aborts the receive Legacy/Enhanced Rx FIFO process which used eDMA. More... | |
| status_t | FLEXCAN_TransferReceiveEnhancedFifoEDMA (CAN_Type *base, flexcan_edma_handle_t *handle, flexcan_fifo_transfer_t *pFifoXfer) |
| Receives the CAN FD Message from the Enhanced Rx FIFO using eDMA. More... | |
| static status_t | FLEXCAN_TransferGetReceiveEnhancedFifoCountEMDA (CAN_Type *base, flexcan_edma_handle_t *handle, size_t *count) |
| Gets the Enhanced Rx Fifo transfer status during a interrupt non-blocking receive. More... | |
| struct _flexcan_edma_handle |
Data Fields | |
| flexcan_edma_transfer_callback_t | callback |
| Callback function. More... | |
| void * | userData |
| FlexCAN callback function parameter. More... | |
| edma_handle_t * | rxFifoEdmaHandle |
| The EDMA handler for Rx FIFO. More... | |
| volatile uint8_t | rxFifoState |
| Rx FIFO transfer state. More... | |
| size_t | frameNum |
| The number of messages that need to be received. More... | |
| flexcan_fd_frame_t * | framefd |
| Point to the buffer of CAN Message to be received from Enhanced Rx FIFO. More... | |
| flexcan_edma_transfer_callback_t flexcan_edma_handle_t::callback |
| void* flexcan_edma_handle_t::userData |
| edma_handle_t* flexcan_edma_handle_t::rxFifoEdmaHandle |
| volatile uint8_t flexcan_edma_handle_t::rxFifoState |
| size_t flexcan_edma_handle_t::frameNum |
| flexcan_fd_frame_t* flexcan_edma_handle_t::framefd |
| #define FSL_FLEXCAN_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 9, 2)) |
| typedef void(* flexcan_edma_transfer_callback_t)(CAN_Type *base, flexcan_edma_handle_t *handle, status_t status, void *userData) |
| void FLEXCAN_TransferCreateHandleEDMA | ( | CAN_Type * | base, |
| flexcan_edma_handle_t * | handle, | ||
| flexcan_edma_transfer_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | rxFifoEdmaHandle | ||
| ) |
| base | FlexCAN peripheral base address. |
| handle | Pointer to flexcan_edma_handle_t structure. |
| callback | The callback function. |
| userData | The parameter of the callback function. |
| rxFifoEdmaHandle | User-requested DMA handle for Rx FIFO DMA transfer. |
| void FLEXCAN_PrepareTransfConfiguration | ( | CAN_Type * | base, |
| flexcan_fifo_transfer_t * | pFifoXfer, | ||
| edma_transfer_config_t * | pEdmaConfig | ||
| ) |
This function prepares the eDMA transfer configuration structure according to FLEXCAN Legacy RX FIFO.
| base | FlexCAN peripheral base address. |
| pFifoXfer | FlexCAN Rx FIFO EDMA transfer structure, see flexcan_fifo_transfer_t. |
| pEdmaConfig | The user configuration structure of type edma_transfer_t. |
| status_t FLEXCAN_StartTransferDatafromRxFIFO | ( | CAN_Type * | base, |
| flexcan_edma_handle_t * | handle, | ||
| edma_transfer_config_t * | pEdmaConfig | ||
| ) |
This function to Update edma transfer confiugration and Start eDMA transfer
| base | FlexCAN peripheral base address. |
| handle | Pointer to flexcan_edma_handle_t structure. |
| pEdmaConfig | The user configuration structure of type edma_transfer_t. |
| kStatus_Success | if succeed, others failed. |
| kStatus_FLEXCAN_RxFifoBusy | Previous transfer ongoing. |
| status_t FLEXCAN_TransferReceiveFifoEDMA | ( | CAN_Type * | base, |
| flexcan_edma_handle_t * | handle, | ||
| flexcan_fifo_transfer_t * | pFifoXfer | ||
| ) |
This function receives the CAN Message using eDMA. This is a non-blocking function, which returns right away. After the CAN Message is received, the receive callback function is called.
| base | FlexCAN peripheral base address. |
| handle | Pointer to flexcan_edma_handle_t structure. |
| pFifoXfer | FlexCAN Rx FIFO EDMA transfer structure, see flexcan_fifo_transfer_t. |
| kStatus_Success | if succeed, others failed. |
| kStatus_FLEXCAN_RxFifoBusy | Previous transfer ongoing. |
| status_t FLEXCAN_TransferGetReceiveFifoCountEMDA | ( | CAN_Type * | base, |
| flexcan_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
| base | FlexCAN peripheral base address. |
| handle | FlexCAN handle pointer. |
| count | Number of CAN messages receive so far by the non-blocking transaction. |
| kStatus_InvalidArgument | count is Invalid. |
| kStatus_Success | Successfully return the count. |
| void FLEXCAN_TransferAbortReceiveFifoEDMA | ( | CAN_Type * | base, |
| flexcan_edma_handle_t * | handle | ||
| ) |
This function aborts the receive Legacy/Enhanced Rx FIFO process which used eDMA.
| base | FlexCAN peripheral base address. |
| handle | Pointer to flexcan_edma_handle_t structure. |
| status_t FLEXCAN_TransferReceiveEnhancedFifoEDMA | ( | CAN_Type * | base, |
| flexcan_edma_handle_t * | handle, | ||
| flexcan_fifo_transfer_t * | pFifoXfer | ||
| ) |
This function receives the CAN FD Message using eDMA. This is a non-blocking function, which returns right away. After the CAN Message is received, the receive callback function is called.
| base | FlexCAN peripheral base address. |
| handle | Pointer to flexcan_edma_handle_t structure. |
| pFifoXfer | FlexCAN Rx FIFO EDMA transfer structure, see flexcan_fifo_transfer_t. |
| kStatus_Success | if succeed, others failed. |
| kStatus_FLEXCAN_RxFifoBusy | Previous transfer ongoing. |
|
inlinestatic |
| base | FlexCAN peripheral base address. |
| handle | FlexCAN handle pointer. |
| count | Number of CAN messages receive so far by the non-blocking transaction. |
| kStatus_InvalidArgument | count is Invalid. |
| kStatus_Success | Successfully return the count. |