![]() |
MCUXpresso SDK API Reference Manual
Rev 2.12.2
NXP Semiconductors
|
Data Structures | |
| struct | led_pin_config_t |
| The pin config struct of LED. More... | |
| struct | led_rgb_config_t |
| The pin config struct of rgb LED. More... | |
| struct | led_monochrome_config_t |
| The pin config struct of monochrome LED. More... | |
| struct | led_config_t |
| The config struct of LED. More... | |
| struct | led_flash_config_t |
| The flash config struct of LED. More... | |
Macros | |
| #define | LED_DIMMING_ENABLEMENT (0U) |
| Definition to determine whether enable dimming. More... | |
| #define | LED_COLOR_WHEEL_ENABLEMENT (0U) |
| Definition to determine whether enable color wheel. More... | |
| #define | LED_USE_CONFIGURE_STRUCTURE (1U) |
| Definition to determine whether use confgure structure. More... | |
| #define | LED_HANDLE_SIZE ((16U * 3U) + 32U) |
| Definition of LED handle size. More... | |
| #define | LED_HANDLE_DEFINE(name) uint32_t name[((LED_HANDLE_SIZE + sizeof(uint32_t) - 1U) / sizeof(uint32_t))] |
| Defines the led handle. More... | |
| #define | LED_HANDLE_ARRAY_DEFINE(name, count) uint32_t name[count][((LED_HANDLE_SIZE + sizeof(uint32_t) - 1U) / sizeof(uint32_t))] |
| Defines the led handle array. More... | |
| #define | LED_TIMER_INTERVAL (100U) |
| Definition of LED timer interval,unit is ms. More... | |
| #define | LED_DIMMING_UPDATE_INTERVAL (100U) |
| Definition of LED dimming update interval,unit is ms. More... | |
| #define | LED_FLASH_CYCLE_FOREVER (0xFFFFFFFFU) |
| Definition of LED flash cycle forever. More... | |
| #define | LED_BLIP_INTERVAL (250U) |
| Definition of LED blip interval,unit is ms. More... | |
| #define | LED_MAKE_COLOR(r, g, b) ((led_color_t)((((led_color_t)b) << 16) | (((led_color_t)g) << 8) | ((led_color_t)r))) |
| Definition to set LED color. More... | |
Typedefs | |
| typedef void * | led_handle_t |
| The handle of LED. | |
| typedef uint32_t | led_color_t |
| The color struct of LED. | |
Enumerations | |
| enum | led_status_t { kStatus_LED_Success = kStatus_Success, kStatus_LED_Error = MAKE_STATUS(kStatusGroup_LED, 1), kStatus_LED_InvalidParameter = MAKE_STATUS(kStatusGroup_LED, 2) } |
| The status type of LED. More... | |
| enum | led_flash_type_t { kLED_FlashOneColor = 0x00U } |
| The flash type of LED. More... | |
| enum | _led_color { kLED_Black = LED_MAKE_COLOR(0, 0, 0), kLED_Red = LED_MAKE_COLOR(255, 0, 0), kLED_Green = LED_MAKE_COLOR(0, 255, 0), kLED_Yellow = LED_MAKE_COLOR(255, 255, 0), kLED_Blue = LED_MAKE_COLOR(0, 0, 255), kLED_Pink = LED_MAKE_COLOR(255, 0, 255), kLED_Aquamarine = LED_MAKE_COLOR(0, 255, 255), kLED_White = LED_MAKE_COLOR(255, 255, 255) } |
| The color type of LED. More... | |
| enum | led_type_t { kLED_TypeRgb = 0x01U, kLED_TypeMonochrome = 0x02U } |
| The type of LED. More... | |
Functions | |
| led_status_t | LED_Init (led_handle_t ledHandle, const led_config_t *ledConfig) |
| Initializes a LED with the LED handle and the user configuration structure. More... | |
| led_status_t | LED_Deinit (led_handle_t ledHandle) |
| Deinitializes a LED instance. More... | |
| led_status_t | LED_SetColor (led_handle_t ledHandle, led_color_t ledRgbColor) |
| Sets the LED color. More... | |
| led_status_t | LED_TurnOnOff (led_handle_t ledHandle, uint8_t turnOnOff) |
| Turns on or off the LED. More... | |
| led_status_t | LED_Blip (led_handle_t ledHandle) |
| Blips the LED. More... | |
| led_status_t | LED_Flash (led_handle_t ledHandle, led_flash_config_t *ledFlash) |
| Flashes the LED. More... | |
| led_status_t | LED_Dimming (led_handle_t ledHandle, uint16_t dimmingPeriod, uint8_t increasement) |
| Adjusts the brightness of the LED. More... | |
| led_status_t | LED_EnterLowpower (led_handle_t ledHandle) |
| Prepares to enter low power consumption. More... | |
| led_status_t | LED_ExitLowpower (led_handle_t ledHandle) |
| Restores from low power consumption. More... | |
| struct led_pin_config_t |
Data Fields | |
| uint8_t | dimmingEnable |
| dimming enable, 0 - disable, 1 - enable | |
| uint32_t | sourceClock |
| The clock source of the PWM module. | |
| uint8_t | instance |
| PWM instance of the pin. | |
| uint8_t | channel |
| PWM channel of the pin. | |
| uint8_t | pinStateDefault |
| The Pin voltage when LED is off (0 - low level, 1 - high level) | |
| struct led_rgb_config_t |
Data Fields | |
| led_pin_config_t | redPin |
| Red pin setting. | |
| led_pin_config_t | greenPin |
| Green pin setting. | |
| led_pin_config_t | bluePin |
| Blue pin setting. | |
| struct led_monochrome_config_t |
Data Fields | |
| led_pin_config_t | monochromePin |
| Monochrome pin setting. | |
| struct led_config_t |
| struct led_flash_config_t |
Data Fields | |
| uint32_t | times |
| Flash times, LED_FLASH_CYCLE_FOREVER for forever. | |
| uint16_t | period |
| Flash period, unit is ms. | |
| led_flash_type_t | flashType |
| Flash type, one color or color wheel. More... | |
| uint8_t | duty |
| Duty of the LED on for one period (duration = duty * period / 100). More... | |
| led_flash_type_t led_flash_config_t::flashType |
Refer to led_flash_type_t
| uint8_t led_flash_config_t::duty |
| #define LED_DIMMING_ENABLEMENT (0U) |
Enable or disable the dimming feature
| #define LED_COLOR_WHEEL_ENABLEMENT (0U) |
Enable or disable the color wheel feature
| #define LED_USE_CONFIGURE_STRUCTURE (1U) |
Enable or disable the confgure structure pointer
| #define LED_HANDLE_SIZE ((16U * 3U) + 32U) |
| #define LED_HANDLE_DEFINE | ( | name | ) | uint32_t name[((LED_HANDLE_SIZE + sizeof(uint32_t) - 1U) / sizeof(uint32_t))] |
This macro is used to define a 4 byte aligned led handle. Then use "(led_handle_t)name" to get the led handle.
The macro should be global and could be optional. You could also define led handle by yourself.
This is an example,
| name | The name string of the led handle. |
| #define LED_HANDLE_ARRAY_DEFINE | ( | name, | |
| count | |||
| ) | uint32_t name[count][((LED_HANDLE_SIZE + sizeof(uint32_t) - 1U) / sizeof(uint32_t))] |
This macro is used to define a 4 byte aligned led handle array. Then use "(led_handle_t)name[0]" to get the first led handle.
The macro should be global and could be optional. You could also define these led handle by yourself.
This is an example,
| name | The name string of the led handle array. |
| count | The amount of led handle. |
| #define LED_TIMER_INTERVAL (100U) |
| #define LED_DIMMING_UPDATE_INTERVAL (100U) |
| #define LED_FLASH_CYCLE_FOREVER (0xFFFFFFFFU) |
| #define LED_BLIP_INTERVAL (250U) |
| #define LED_MAKE_COLOR | ( | r, | |
| g, | |||
| b | |||
| ) | ((led_color_t)((((led_color_t)b) << 16) | (((led_color_t)g) << 8) | ((led_color_t)r))) |
| enum led_status_t |
| enum led_flash_type_t |
| enum _led_color |
| enum led_type_t |
| led_status_t LED_Init | ( | led_handle_t | ledHandle, |
| const led_config_t * | ledConfig | ||
| ) |
This function configures the LED with user-defined settings. The user can configure the configuration structure. The parameter ledHandle is a pointer to point to a memory space of size LED_HANDLE_SIZE allocated by the caller. The LED supports two types LED, RGB and monochrome. Please refer to led_type_t. These two types can be set by using led_config_t. The LED also supports LED dimming mode.
Example below shows how to use this API to configure the LED. For monochrome LED,
For rgb LED,
For dimming monochrome LED,
For multiple LEDs,
| ledHandle | Pointer to point to a memory space of size LED_HANDLE_SIZE allocated by the caller. The handle should be 4 byte aligned, because unaligned access doesn't be supported on some devices. You can define one handle in the following two ways: LED_HANDLE_DEFINE(ledHandle); or uint32_t ledHandle[((LED_HANDLE_SIZE + sizeof(uint32_t) - 1U) / sizeof(uint32_t))]; You can define multiple handles in the following way: LED_HANDLE_ARRAY_DEFINE(ledHandleArray, count); |
| ledConfig | Pointer to user-defined configuration structure. please note, if the LED_USE_CONFIGURE_STRUCTURE is set to 1, then user must use const buffer forledConfig, LED module will directly use the const buffer. |
| kStatus_LED_Error | An error occurred. |
| kStatus_LED_Success | LED initialization succeed. |
| led_status_t LED_Deinit | ( | led_handle_t | ledHandle | ) |
This function deinitializes the LED instance.
| ledHandle | LED handle pointer. |
| kStatus_LED_Success | LED de-initialization succeed. |
| led_status_t LED_SetColor | ( | led_handle_t | ledHandle, |
| led_color_t | ledRgbColor | ||
| ) |
This function sets the LED color. The function only supports the RGB LED. The default color is kLED_White. Please refer to LED_MAKE_COLOR(r,g,b).
| ledHandle | LED handle pointer. |
| ledRgbColor | LED color. |
| kStatus_LED_Error | An error occurred. |
| kStatus_LED_Success | Color setting succeed. |
| led_status_t LED_TurnOnOff | ( | led_handle_t | ledHandle, |
| uint8_t | turnOnOff | ||
| ) |
This function turns on or off the led.
| ledHandle | LED handle pointer. |
| turnOnOff | Setting value, 1 - turns on, 0 - turns off. |
| kStatus_LED_Error | An error occurred. |
| kStatus_LED_Success | Successfully turn on or off the LED. |
| led_status_t LED_Blip | ( | led_handle_t | ledHandle | ) |
This function blips the led.
| ledHandle | LED handle pointer. |
| kStatus_LED_Error | An error occurred. |
| kStatus_LED_Success | Successfully blip the LED. |
| led_status_t LED_Flash | ( | led_handle_t | ledHandle, |
| led_flash_config_t * | ledFlash | ||
| ) |
This function flashes the led. The flash configuration is passed by using led_flash_config_t.
| ledHandle | LED handle pointer. |
| ledFlash | LED flash configuration. |
| kStatus_LED_Error | An error occurred. |
| kStatus_LED_Success | Successfully flash the LED. |
| led_status_t LED_Dimming | ( | led_handle_t | ledHandle, |
| uint16_t | dimmingPeriod, | ||
| uint8_t | increasement | ||
| ) |
This function adjust the brightness of the LED.
| ledHandle | LED handle pointer. |
| dimmingPeriod | The duration of the dimming (unit is ms). |
| increasement | Brighten or dim (1 - brighten, 0 - dim). |
| kStatus_LED_Error | An error occurred. |
| kStatus_LED_Success | Successfully adjust the brightness of the LED. |
| led_status_t LED_EnterLowpower | ( | led_handle_t | ledHandle | ) |
This function is used to prepare to enter low power consumption.
| ledHandle | LED handle pointer. |
| kStatus_LED_Success | Successful operation. |
| led_status_t LED_ExitLowpower | ( | led_handle_t | ledHandle | ) |
This function is used to restore from low power consumption.
| ledHandle | LED handle pointer. |
| kStatus_LED_Success | Successful operation. |