![]() |
MCUXpresso SDK API Reference Manual
Rev 2.12.2
NXP Semiconductors
|
Macros | |
| #define | OSA_WAIT_FOREVER 0xFFFFFFFFU |
| Constant to pass as timeout value in order to wait indefinitely. More... | |
| #define | FSL_OSA_TIME_RANGE 0xFFFFFFFFU |
| OSA's time range in millisecond, OSA time wraps if exceeds this value. More... | |
| #define | OSA_DEFAULT_INT_HANDLER ((osa_int_handler_t)(&DefaultISR)) |
| The default interrupt handler installed in vector table. More... | |
Typedefs | |
| typedef TaskHandle_t | task_handler_t |
| Type for a task handler, returned by the OSA_TaskCreate function. More... | |
| typedef portSTACK_TYPE | task_stack_t |
| Type for a task stack. More... | |
| typedef void * | task_param_t |
| Type for task parameter. | |
| typedef EventBits_t | event_flags_t |
| Type for an event flags object. More... | |
Thread management | |
| #define | PRIORITY_OSA_TO_RTOS(osa_prio) ((UBaseType_t)configMAX_PRIORITIES - (osa_prio)-2U) |
| To provide unified task piority for upper layer, OSA layer makes conversion. | |
| #define | PRIORITY_RTOS_TO_OSA(rtos_prio) ((UBaseType_t)configMAX_PRIORITIES - (rtos_prio)-2U) |
Message queues | |
| #define | MSG_QUEUE_DECLARE(name, number, size) msg_queue_t *name = NULL |
| This macro statically reserves the memory required for the queue. More... | |
| #define OSA_WAIT_FOREVER 0xFFFFFFFFU |
| #define FSL_OSA_TIME_RANGE 0xFFFFFFFFU |
| #define OSA_DEFAULT_INT_HANDLER ((osa_int_handler_t)(&DefaultISR)) |
| #define MSG_QUEUE_DECLARE | ( | name, | |
| number, | |||
| size | |||
| ) | msg_queue_t *name = NULL |
| name | Identifier for the memory region. |
| number | Number of elements in the queue. |
| size | Size of every elements in words. |
| typedef TaskHandle_t task_handler_t |
| typedef portSTACK_TYPE task_stack_t |
| typedef EventBits_t event_flags_t |