![]() |
MCUXpresso SDK API Reference Manual
Rev 2.13.0
NXP Semiconductors
|
Data Structures | |
| struct | i2c_master_edma_handle_t |
| I2C master eDMA transfer structure. More... | |
Typedefs | |
| typedef void(* | i2c_master_edma_transfer_callback_t )(I2C_Type *base, i2c_master_edma_handle_t *handle, status_t status, void *userData) |
| I2C master eDMA transfer callback typedef. More... | |
Driver version | |
| #define | FSL_I2C_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 9)) |
| I2C EDMA driver version. More... | |
I2C Block eDMA Transfer Operation | |
| void | I2C_MasterCreateEDMAHandle (I2C_Type *base, i2c_master_edma_handle_t *handle, i2c_master_edma_transfer_callback_t callback, void *userData, edma_handle_t *edmaHandle) |
| Initializes the I2C handle which is used in transactional functions. More... | |
| status_t | I2C_MasterTransferEDMA (I2C_Type *base, i2c_master_edma_handle_t *handle, i2c_master_transfer_t *xfer) |
| Performs a master eDMA non-blocking transfer on the I2C bus. More... | |
| status_t | I2C_MasterTransferGetCountEDMA (I2C_Type *base, i2c_master_edma_handle_t *handle, size_t *count) |
| Gets a master transfer status during the eDMA non-blocking transfer. More... | |
| void | I2C_MasterTransferAbortEDMA (I2C_Type *base, i2c_master_edma_handle_t *handle) |
| Aborts a master eDMA non-blocking transfer early. More... | |
| struct _i2c_master_edma_handle |
Retry times for waiting flag.
I2C master eDMA handle typedef.
Data Fields | |
| i2c_master_transfer_t | transfer |
| I2C master transfer structure. More... | |
| size_t | transferSize |
| Total bytes to be transferred. More... | |
| uint8_t | nbytes |
| eDMA minor byte transfer count initially configured. More... | |
| uint8_t | state |
| I2C master transfer status. More... | |
| edma_handle_t * | dmaHandle |
| The eDMA handler used. More... | |
| i2c_master_edma_transfer_callback_t | completionCallback |
| A callback function called after the eDMA transfer is finished. More... | |
| void * | userData |
| A callback parameter passed to the callback function. More... | |
| i2c_master_transfer_t i2c_master_edma_handle_t::transfer |
| size_t i2c_master_edma_handle_t::transferSize |
| uint8_t i2c_master_edma_handle_t::nbytes |
| uint8_t i2c_master_edma_handle_t::state |
| edma_handle_t* i2c_master_edma_handle_t::dmaHandle |
| i2c_master_edma_transfer_callback_t i2c_master_edma_handle_t::completionCallback |
| void* i2c_master_edma_handle_t::userData |
| #define FSL_I2C_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 9)) |
| typedef void(* i2c_master_edma_transfer_callback_t)(I2C_Type *base, i2c_master_edma_handle_t *handle, status_t status, void *userData) |
| void I2C_MasterCreateEDMAHandle | ( | I2C_Type * | base, |
| i2c_master_edma_handle_t * | handle, | ||
| i2c_master_edma_transfer_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | edmaHandle | ||
| ) |
| base | I2C peripheral base address. |
| handle | A pointer to the i2c_master_edma_handle_t structure. |
| callback | A pointer to the user callback function. |
| userData | A user parameter passed to the callback function. |
| edmaHandle | eDMA handle pointer. |
| status_t I2C_MasterTransferEDMA | ( | I2C_Type * | base, |
| i2c_master_edma_handle_t * | handle, | ||
| i2c_master_transfer_t * | xfer | ||
| ) |
| base | I2C peripheral base address. |
| handle | A pointer to the i2c_master_edma_handle_t structure. |
| xfer | A pointer to the transfer structure of i2c_master_transfer_t. |
| kStatus_Success | Successfully completed the data transmission. |
| kStatus_I2C_Busy | A previous transmission is still not finished. |
| kStatus_I2C_Timeout | Transfer error, waits for a signal timeout. |
| kStatus_I2C_ArbitrationLost | Transfer error, arbitration lost. |
| kStataus_I2C_Nak | Transfer error, receive NAK during transfer. |
| status_t I2C_MasterTransferGetCountEDMA | ( | I2C_Type * | base, |
| i2c_master_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
| base | I2C peripheral base address. |
| handle | A pointer to the i2c_master_edma_handle_t structure. |
| count | A number of bytes transferred by the non-blocking transaction. |
| void I2C_MasterTransferAbortEDMA | ( | I2C_Type * | base, |
| i2c_master_edma_handle_t * | handle | ||
| ) |
| base | I2C peripheral base address. |
| handle | A pointer to the i2c_master_edma_handle_t structure. |