![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
Modules | |
| FGPIO Driver | |
| GPIO Driver | |
Data Structures | |
| struct | gpio_pin_config_t |
| The GPIO pin configuration structure. More... | |
Enumerations | |
| enum | gpio_pin_direction_t { kGPIO_DigitalInput = 0U, kGPIO_DigitalOutput = 1U } |
| GPIO direction definition. More... | |
| enum | gpio_interrupt_config_t { kGPIO_InterruptStatusFlagDisabled = 0x0U, kGPIO_DMARisingEdge = 0x1U, kGPIO_DMAFallingEdge = 0x2U, kGPIO_DMAEitherEdge = 0x3U, kGPIO_FlagRisingEdge = 0x05U, kGPIO_FlagFallingEdge = 0x06U, kGPIO_FlagEitherEdge = 0x07U, kGPIO_InterruptLogicZero = 0x8U, kGPIO_InterruptRisingEdge = 0x9U, kGPIO_InterruptFallingEdge = 0xAU, kGPIO_InterruptEitherEdge = 0xBU, kGPIO_InterruptLogicOne = 0xCU, kGPIO_ActiveHighTriggerOutputEnable = 0xDU, kGPIO_ActiveLowTriggerOutputEnable = 0xEU } |
| Configures the interrupt generation condition. More... | |
Driver version | |
| #define | FSL_GPIO_DRIVER_VERSION (MAKE_VERSION(2, 7, 3)) |
| GPIO driver version. More... | |
| struct gpio_pin_config_t |
Each pin can only be configured as either an output pin or an input pin at a time. If configured as an input pin, leave the outputConfig unused. Note that in some use cases, the corresponding port property should be configured in advance with the PORT_SetPinConfig().
Data Fields | |
| gpio_pin_direction_t | pinDirection |
| GPIO direction, input or output. | |
| uint8_t | outputLogic |
| Set a default output logic, which has no use in input. | |
| #define FSL_GPIO_DRIVER_VERSION (MAKE_VERSION(2, 7, 3)) |
| enum gpio_pin_direction_t |