![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
The MCUXpresso SDK provides APIs for MCUXpresso SDK devices' clock operation.
The clock driver supports:
Files | |
| file | fsl_clock.h |
Data Structures | |
| struct | firc_trim_config_t |
| firc trim configuration. More... | |
| struct | sirc_trim_config_t |
| sirc trim configuration. More... | |
| struct | vbat_osc_config_t |
| The structure of oscillator configuration. More... | |
| struct | pll_config_t |
| PLL configuration structure. More... | |
| struct | pll_setup_t |
| PLL0 setup structure This structure can be used to pre-build a PLL setup configuration at run-time and quickly set the PLL to the configuration. More... | |
Macros | |
| #define | FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL 0 |
| Configure whether driver controls clock. More... | |
| #define | CLOCK_USR_CFG_PLL_CONFIG_CACHE_COUNT 2U |
| User-defined the size of cache for CLOCK_PllGetConfig() function. More... | |
| #define | ROM_CLOCKS |
| Clock ip name array for ROM. More... | |
| #define | SRAM_CLOCKS |
| Clock ip name array for SRAM. More... | |
| #define | FMC_CLOCKS |
| Clock ip name array for FMC. More... | |
| #define | INPUTMUX_CLOCKS |
| Clock ip name array for INPUTMUX. More... | |
| #define | ETH_CLOCKS |
| Clock ip name array for ENET. More... | |
| #define | GPIO_CLOCKS |
| Clock ip name array for GPIO. More... | |
| #define | PINT_CLOCKS |
| Clock ip name array for PINT. More... | |
| #define | DMA_CLOCKS |
| Clock ip name array for DMA. More... | |
| #define | EDMA_CLOCKS |
| Clock gate name array for EDMA. More... | |
| #define | CRC_CLOCKS |
| Clock ip name array for CRC. More... | |
| #define | WWDT_CLOCKS |
| Clock ip name array for WWDT. More... | |
| #define | MAILBOX_CLOCKS |
| Clock ip name array for Mailbox. More... | |
| #define | LPADC_CLOCKS |
| Clock ip name array for LPADC. More... | |
| #define | MRT_CLOCKS |
| Clock ip name array for MRT. More... | |
| #define | OSTIMER_CLOCKS |
| Clock ip name array for OSTIMER. More... | |
| #define | SCT_CLOCKS |
| Clock ip name array for SCT0. More... | |
| #define | UTICK_CLOCKS |
| Clock ip name array for UTICK. More... | |
| #define | LP_FLEXCOMM_CLOCKS |
| Clock ip name array for LP_FLEXCOMM. More... | |
| #define | LPUART_CLOCKS |
| Clock ip name array for LPUART. More... | |
| #define | LPI2C_CLOCKS |
| Clock ip name array for LPI2C. More... | |
| #define | LPSPI_CLOCKS |
| Clock ip name array for LSPI. More... | |
| #define | CTIMER_CLOCKS |
| Clock ip name array for CTIMER. More... | |
| #define | FREQME_CLOCKS |
| Clock ip name array for FREQME. More... | |
| #define | POWERQUAD_CLOCKS |
| Clock ip name array for PowerQuad. More... | |
| #define | PLU_CLOCKS |
| Clock ip name array for PLU. More... | |
| #define | PUF_CLOCKS |
| Clock ip name array for PUF. More... | |
| #define | VREF_CLOCKS |
| Clock ip name array for VREF. More... | |
| #define | LPDAC_CLOCKS |
| Clock ip name array for LPDAC. More... | |
| #define | HPDAC_CLOCKS |
| Clock ip name array for HPDAC. More... | |
| #define | PWM_CLOCKS |
| Clock ip name array for PWM. More... | |
| #define | QDC_CLOCKS |
| Clock ip name array for QDC. More... | |
| #define | FLEXIO_CLOCKS |
| Clock ip name array for FLEXIO. More... | |
| #define | FLEXCAN_CLOCKS |
| Clock ip name array for FLEXCAN. More... | |
| #define | EMVSIM_CLOCKS |
| Clock ip name array for EMVSIM. More... | |
| #define | I3C_CLOCKS |
| Clock ip name array for I3C. | |
| #define | USDHC_CLOCKS |
| Clock ip name array for USDHC. More... | |
| #define | FLEXSPI_CLOCKS |
| Clock ip name array for FLEXSPI. | |
| #define | SAI_CLOCKS |
| Clock ip name array for SAI. More... | |
| #define | RTC_CLOCKS |
| Clock ip name array for RTC. More... | |
| #define | PDM_CLOCKS |
| Clock ip name array for PDM. More... | |
| #define | ERM_CLOCKS |
| Clock ip name array for ERM. More... | |
| #define | EIM_CLOCKS |
| Clock ip name array for EIM. More... | |
| #define | OPAMP_CLOCKS |
| Clock ip name array for OPAMP. More... | |
| #define | TSI_CLOCKS |
| Clock ip name array for TSI. More... | |
| #define | TRNG_CLOCKS |
| Clock ip name array for TRNG. More... | |
| #define | LPCMP_CLOCKS |
| Clock ip name array for LPCMP. More... | |
| #define | SINC_CLOCKS |
| Clock ip name array for SINC. | |
| #define | SEMA42_CLOCKS |
| Clock ip name array for SEMA42. | |
| #define | CLK_GATE_REG_OFFSET_SHIFT 8U |
| Clock gate name used for CLOCK_EnableClock/CLOCK_DisableClock. More... | |
| #define | BUS_CLK kCLOCK_BusClk |
| Peripherals clock source definition. More... | |
| #define | CLK_ATTACH_ID(mux, sel, pos) ((((uint32_t)(mux) << 0U) | (((uint32_t)(sel) + 1U) & 0xFU) << 12U) << ((uint32_t)(pos)*16U)) |
| Clock Mux Switches The encoding is as follows each connection identified is 32bits wide while 24bits are valuable starting from LSB upwards. More... | |
| #define | PLL_CONFIGFLAG_FORCENOFRACT (1U << 2U) |
| PLL configuration structure flags for 'flags' field These flags control how the PLL configuration function sets up the PLL setup structure. More... | |
Enumerations | |
| enum | clock_ip_name_t { kCLOCK_IpInvalid = 0U, kCLOCK_None = 0U, kCLOCK_Rom = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 1), kCLOCK_Sram1 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 2), kCLOCK_Sram2 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 3), kCLOCK_Sram3 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 4), kCLOCK_Sram4 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 5), kCLOCK_Sram5 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 6), kCLOCK_Sram6 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 7), kCLOCK_Sram7 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 8), kCLOCK_Fmu = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 9), kCLOCK_Fmc = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 10), kCLOCK_Flexspi = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 11), kCLOCK_InputMux0 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 12), kCLOCK_InputMux = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 12), kCLOCK_Port0 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 13), kCLOCK_Port1 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 14), kCLOCK_Port2 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 15), kCLOCK_Port3 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 16), kCLOCK_Port4 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 17), kCLOCK_Gpio0 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 19), kCLOCK_Gpio1 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 20), kCLOCK_Gpio2 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 21), kCLOCK_Gpio3 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 22), kCLOCK_Gpio4 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 23), kCLOCK_Pint = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 25), kCLOCK_Dma0 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 26), kCLOCK_Crc0 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 27), kCLOCK_Wwdt0 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 28), kCLOCK_Wwdt1 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 29), kCLOCK_Mailbox = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 31), kCLOCK_Mrt = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 0), kCLOCK_OsTimer = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 1), kCLOCK_Sct = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 2), kCLOCK_Adc0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 3), kCLOCK_Adc1 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 4), kCLOCK_Dac0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 5), kCLOCK_Rtc0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 6), kCLOCK_Evsim0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 8), kCLOCK_Evsim1 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 9), kCLOCK_Utick = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 10), kCLOCK_LPFlexComm0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 11), kCLOCK_LPFlexComm1 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 12), kCLOCK_LPFlexComm2 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 13), kCLOCK_LPFlexComm3 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 14), kCLOCK_LPFlexComm4 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 15), kCLOCK_LPFlexComm5 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 16), kCLOCK_LPFlexComm6 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 17), kCLOCK_LPFlexComm7 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 18), kCLOCK_LPFlexComm8 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 19), kCLOCK_LPFlexComm9 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 20), kCLOCK_LPUart0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 11), kCLOCK_LPUart1 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 12), kCLOCK_LPUart2 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 13), kCLOCK_LPUart3 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 14), kCLOCK_LPUart4 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 15), kCLOCK_LPUart5 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 16), kCLOCK_LPUart6 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 17), kCLOCK_LPUart7 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 18), kCLOCK_LPUart8 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 19), kCLOCK_LPUart9 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 20), kCLOCK_LPSpi0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 11), kCLOCK_LPSpi1 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 12), kCLOCK_LPSpi2 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 13), kCLOCK_LPSpi3 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 14), kCLOCK_LPSpi4 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 15), kCLOCK_LPSpi5 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 16), kCLOCK_LPSpi6 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 17), kCLOCK_LPSpi7 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 18), kCLOCK_LPSpi8 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 19), kCLOCK_LPSpi9 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 20), kCLOCK_LPI2c0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 11), kCLOCK_LPI2c1 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 12), kCLOCK_LPI2c2 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 13), kCLOCK_LPI2c3 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 14), kCLOCK_LPI2c4 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 15), kCLOCK_LPI2c5 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 16), kCLOCK_LPI2c6 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 17), kCLOCK_LPI2c7 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 18), kCLOCK_LPI2c8 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 19), kCLOCK_LPI2c9 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 20), kCLOCK_Micfil = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 21), kCLOCK_Timer2 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 22), kCLOCK_Usb0Ram = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 23), kCLOCK_Usb0FsDcd = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 24), kCLOCK_Usb0Fs = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 25), kCLOCK_Timer0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 26), kCLOCK_Timer1 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 27), kCLOCK_PkcRam = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 29), kCLOCK_Smartdma = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 31), kCLOCK_Espi = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 0), kCLOCK_Dma1 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 1), kCLOCK_Enet = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 2), kCLOCK_uSdhc = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 3), kCLOCK_Flexio = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 4), kCLOCK_Sai0 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 5), kCLOCK_Sai1 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 6), kCLOCK_Tro = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 7), kCLOCK_Freqme = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 8), kCLOCK_Trng = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 13), kCLOCK_Flexcan0 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 14), kCLOCK_Flexcan1 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 15), kCLOCK_UsbHs = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 16), kCLOCK_UsbHsPhy = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 17), kCLOCK_Css = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 18), kCLOCK_PowerQuad = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 19), kCLOCK_PluLut = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 20), kCLOCK_Timer3 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 21), kCLOCK_Timer4 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 22), kCLOCK_Puf = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 23), kCLOCK_Pkc = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 24), kCLOCK_Scg = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 26), kCLOCK_Gdet = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 29), kCLOCK_Sm3 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 30), kCLOCK_I3c0 = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 0), kCLOCK_I3c1 = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 1), kCLOCK_Sinc = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 2), kCLOCK_CoolFlux = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 3), kCLOCK_Qdc0 = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 4), kCLOCK_Qdc1 = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 5), kCLOCK_Pwm0 = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 6), kCLOCK_Pwm1 = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 7), kCLOCK_Evtg = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 8), kCLOCK_Dac1 = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 11), kCLOCK_Dac2 = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 12), kCLOCK_Opamp0 = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 13), kCLOCK_Opamp1 = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 14), kCLOCK_Opamp2 = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 15), kCLOCK_Cmp2 = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 18), kCLOCK_Vref = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 19), kCLOCK_CoolFluxApb = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 20), kCLOCK_Neutron = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 21), kCLOCK_Tsi = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 22), kCLOCK_Ewm = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 23), kCLOCK_Ewm0 = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 23), kCLOCK_Eim = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 24), kCLOCK_Erm = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 25), kCLOCK_Intm = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 26), kCLOCK_Sema42 = CLK_GATE_DEFINE(AHB_CLK_CTRL3, 27), kCLOCK_Pwm0_Sm0 = CLK_GATE_DEFINE(REG_PWM0SUBCTL, 0U), kCLOCK_Pwm0_Sm1 = CLK_GATE_DEFINE(REG_PWM0SUBCTL, 1U), kCLOCK_Pwm0_Sm2 = CLK_GATE_DEFINE(REG_PWM0SUBCTL, 2U), kCLOCK_Pwm0_Sm3 = CLK_GATE_DEFINE(REG_PWM0SUBCTL, 3U), kCLOCK_Pwm1_Sm0 = CLK_GATE_DEFINE(REG_PWM1SUBCTL, 0U), kCLOCK_Pwm1_Sm1 = CLK_GATE_DEFINE(REG_PWM1SUBCTL, 1U), kCLOCK_Pwm1_Sm2 = CLK_GATE_DEFINE(REG_PWM1SUBCTL, 2U), kCLOCK_Pwm1_Sm3 = CLK_GATE_DEFINE(REG_PWM1SUBCTL, 3U) } |
| Clock gate name used for CLOCK_EnableClock/CLOCK_DisableClock. More... | |
| enum | clock_name_t { kCLOCK_MainClk, kCLOCK_CoreSysClk, kCLOCK_BusClk, kCLOCK_SystickClk0, kCLOCK_SystickClk1, kCLOCK_ClockOut, kCLOCK_Fro12M, kCLOCK_Clk1M, kCLOCK_FroHf, kCLOCK_Clk48M, kCLOCK_Clk144M, kCLOCK_Clk16K0, kCLOCK_Clk16K1, kCLOCK_Clk16K2, kCLOCK_Clk16K3, kCLOCK_ExtClk, kCLOCK_Osc32K0, kCLOCK_Osc32K1, kCLOCK_Osc32K2, kCLOCK_Osc32K3, kCLOCK_Pll0Out, kCLOCK_Pll1Out, kCLOCK_UsbPllOut, kCLOCK_LpOsc } |
| Clock name used to get clock frequency. More... | |
| enum | clock_attach_id_t { kCLK_IN_to_MAIN_CLK = MUX_A(CM_SCGRCCRSCSCLKSEL, 1), kFRO12M_to_MAIN_CLK = MUX_A(CM_SCGRCCRSCSCLKSEL, 2), kFRO_HF_to_MAIN_CLK = MUX_A(CM_SCGRCCRSCSCLKSEL, 3), kXTAL32K2_to_MAIN_CLK = MUX_A(CM_SCGRCCRSCSCLKSEL, 4), kPLL0_to_MAIN_CLK = MUX_A(CM_SCGRCCRSCSCLKSEL, 5), kPLL1_to_MAIN_CLK = MUX_A(CM_SCGRCCRSCSCLKSEL, 6), kUSB_PLL_to_MAIN_CLK = MUX_A(CM_SCGRCCRSCSCLKSEL, 7), kNONE_to_MAIN_CLK = MUX_A(CM_SCGRCCRSCSCLKSEL, 15), kSYSTICK_DIV0_to_SYSTICK0 = MUX_A(CM_SYSTICKCLKSEL0, 0), kCLK_1M_to_SYSTICK0 = MUX_A(CM_SYSTICKCLKSEL0, 1), kLPOSC_to_SYSTICK0 = MUX_A(CM_SYSTICKCLKSEL0, 2), kNONE_to_SYSTICK0 = MUX_A(CM_SYSTICKCLKSEL0, 7), kSYSTICK_DIV1_to_SYSTICK1 = MUX_A(CM_SYSTICKCLKSEL1, 0), kCLK_1M_to_SYSTICK1 = MUX_A(CM_SYSTICKCLKSEL1, 1), kLPOSC_to_SYSTICK1 = MUX_A(CM_SYSTICKCLKSEL1, 2), kNONE_to_SYSTICK1 = MUX_A(CM_SYSTICKCLKSEL1, 7), kTRACE_DIV_to_TRACE = MUX_A(CM_TRACECLKSEL, 0), kCLK_1M_to_TRACE = MUX_A(CM_TRACECLKSEL, 1), kLPOSC_to_TRACE = MUX_A(CM_TRACECLKSEL, 2), kNONE_to_TRACE = MUX_A(CM_TRACECLKSEL, 7), kCLK_1M_to_CTIMER0 = MUX_A(CM_CTIMERCLKSEL0, 0), kPLL0_to_CTIMER0 = MUX_A(CM_CTIMERCLKSEL0, 1), kPLL1_CLK0_to_CTIMER0 = MUX_A(CM_CTIMERCLKSEL0, 2), kFRO_HF_to_CTIMER0 = MUX_A(CM_CTIMERCLKSEL0, 3), kFRO12M_to_CTIMER0 = MUX_A(CM_CTIMERCLKSEL0, 4), kSAI0_MCLK_IN_to_CTIMER0 = MUX_A(CM_CTIMERCLKSEL0, 5), kLPOSC_to_CTIMER0 = MUX_A(CM_CTIMERCLKSEL0, 6), kSAI1_MCLK_IN_to_CTIMER0 = MUX_A(CM_CTIMERCLKSEL0, 8), kSAI0_TX_BCLK_to_CTIMER0 = MUX_A(CM_CTIMERCLKSEL0, 9), kSAI0_RX_BCLK_to_CTIMER0 = MUX_A(CM_CTIMERCLKSEL0, 10), kSAI1_TX_BCLK_to_CTIMER0 = MUX_A(CM_CTIMERCLKSEL0, 11), kSAI1_RX_BCLK_to_CTIMER0 = MUX_A(CM_CTIMERCLKSEL0, 12), kNONE_to_CTIMER0 = MUX_A(CM_CTIMERCLKSEL0, 15), kCLK_1M_to_CTIMER1 = MUX_A(CM_CTIMERCLKSEL1, 0), kPLL0_to_CTIMER1 = MUX_A(CM_CTIMERCLKSEL1, 1), kPLL1_CLK0_to_CTIMER1 = MUX_A(CM_CTIMERCLKSEL1, 2), kFRO_HF_to_CTIMER1 = MUX_A(CM_CTIMERCLKSEL1, 3), kFRO12M_to_CTIMER1 = MUX_A(CM_CTIMERCLKSEL1, 4), kSAI0_MCLK_IN_to_CTIMER1 = MUX_A(CM_CTIMERCLKSEL1, 5), kLPOSC_to_CTIMER1 = MUX_A(CM_CTIMERCLKSEL1, 6), kSAI1_MCLK_IN_to_CTIMER1 = MUX_A(CM_CTIMERCLKSEL1, 8), kSAI0_TX_BCLK_to_CTIMER1 = MUX_A(CM_CTIMERCLKSEL1, 9), kSAI0_RX_BCLK_to_CTIMER1 = MUX_A(CM_CTIMERCLKSEL1, 10), kSAI1_TX_BCLK_to_CTIMER1 = MUX_A(CM_CTIMERCLKSEL1, 11), kSAI1_RX_BCLK_to_CTIMER1 = MUX_A(CM_CTIMERCLKSEL1, 12), kNONE_to_CTIMER1 = MUX_A(CM_CTIMERCLKSEL1, 15), kCLK_1M_to_CTIMER2 = MUX_A(CM_CTIMERCLKSEL2, 0), kPLL0_to_CTIMER2 = MUX_A(CM_CTIMERCLKSEL2, 1), kPLL1_CLK0_to_CTIMER2 = MUX_A(CM_CTIMERCLKSEL2, 2), kFRO_HF_to_CTIMER2 = MUX_A(CM_CTIMERCLKSEL2, 3), kFRO12M_to_CTIMER2 = MUX_A(CM_CTIMERCLKSEL2, 4), kSAI0_MCLK_IN_to_CTIMER2 = MUX_A(CM_CTIMERCLKSEL2, 5), kLPOSC_to_CTIMER2 = MUX_A(CM_CTIMERCLKSEL2, 6), kSAI1_MCLK_IN_to_CTIMER2 = MUX_A(CM_CTIMERCLKSEL2, 8), kSAI0_TX_BCLK_to_CTIMER2 = MUX_A(CM_CTIMERCLKSEL2, 9), kSAI0_RX_BCLK_to_CTIMER2 = MUX_A(CM_CTIMERCLKSEL2, 10), kSAI1_TX_BCLK_to_CTIMER2 = MUX_A(CM_CTIMERCLKSEL2, 11), kSAI1_RX_BCLK_to_CTIMER2 = MUX_A(CM_CTIMERCLKSEL2, 12), kNONE_to_CTIMER2 = MUX_A(CM_CTIMERCLKSEL2, 15), kCLK_1M_to_CTIMER3 = MUX_A(CM_CTIMERCLKSEL3, 0), kPLL0_to_CTIMER3 = MUX_A(CM_CTIMERCLKSEL3, 1), kPLL1_CLK0_to_CTIMER3 = MUX_A(CM_CTIMERCLKSEL3, 2), kFRO_HF_to_CTIMER3 = MUX_A(CM_CTIMERCLKSEL3, 3), kFRO12M_to_CTIMER3 = MUX_A(CM_CTIMERCLKSEL3, 4), kSAI0_MCLK_IN_to_CTIMER3 = MUX_A(CM_CTIMERCLKSEL3, 5), kLPOSC_to_CTIMER3 = MUX_A(CM_CTIMERCLKSEL3, 6), kSAI1_MCLK_IN_to_CTIMER3 = MUX_A(CM_CTIMERCLKSEL3, 8), kSAI0_TX_BCLK_to_CTIMER3 = MUX_A(CM_CTIMERCLKSEL3, 9), kSAI0_RX_BCLK_to_CTIMER3 = MUX_A(CM_CTIMERCLKSEL3, 10), kSAI1_TX_BCLK_to_CTIMER3 = MUX_A(CM_CTIMERCLKSEL3, 11), kSAI1_RX_BCLK_to_CTIMER3 = MUX_A(CM_CTIMERCLKSEL3, 12), kNONE_to_CTIMER3 = MUX_A(CM_CTIMERCLKSEL3, 15), kCLK_1M_to_CTIMER4 = MUX_A(CM_CTIMERCLKSEL4, 0), kPLL0_to_CTIMER4 = MUX_A(CM_CTIMERCLKSEL4, 1), kPLL1_CLK0_to_CTIMER4 = MUX_A(CM_CTIMERCLKSEL4, 2), kFRO_HF_to_CTIMER4 = MUX_A(CM_CTIMERCLKSEL4, 3), kFRO12M_to_CTIMER4 = MUX_A(CM_CTIMERCLKSEL4, 4), kSAI0_MCLK_IN_to_CTIMER4 = MUX_A(CM_CTIMERCLKSEL4, 5), kLPOSC_to_CTIMER4 = MUX_A(CM_CTIMERCLKSEL4, 6), kSAI1_MCLK_IN_to_CTIMER4 = MUX_A(CM_CTIMERCLKSEL4, 8), kSAI0_TX_BCLK_to_CTIMER4 = MUX_A(CM_CTIMERCLKSEL4, 9), kSAI0_RX_BCLK_to_CTIMER4 = MUX_A(CM_CTIMERCLKSEL4, 10), kSAI1_TX_BCLK_to_CTIMER4 = MUX_A(CM_CTIMERCLKSEL4, 11), kSAI1_RX_BCLK_to_CTIMER4 = MUX_A(CM_CTIMERCLKSEL4, 12), kNONE_to_CTIMER4 = MUX_A(CM_CTIMERCLKSEL4, 15), kMAIN_CLK_to_CLKOUT = MUX_A(CM_CLKOUTCLKSEL, 0), kPLL0_to_CLKOUT = MUX_A(CM_CLKOUTCLKSEL, 1), kCLK_IN_to_CLKOUT = MUX_A(CM_CLKOUTCLKSEL, 2), kFRO_HF_to_CLKOUT = MUX_A(CM_CLKOUTCLKSEL, 3), kFRO12M_to_CLKOUT = MUX_A(CM_CLKOUTCLKSEL, 4), kPLL1_CLK0_to_CLKOUT = MUX_A(CM_CLKOUTCLKSEL, 5), kLPOSC_to_CLKOUT = MUX_A(CM_CLKOUTCLKSEL, 6), kUSB_PLL_to_CLKOUT = MUX_A(CM_CLKOUTCLKSEL, 7), kNONE_to_CLKOUT = MUX_A(CM_CLKOUTCLKSEL, 15), kPLL0_to_ADC0 = MUX_A(CM_ADC0CLKSEL, 1), kFRO_HF_to_ADC0 = MUX_A(CM_ADC0CLKSEL, 2), kFRO12M_to_ADC0 = MUX_A(CM_ADC0CLKSEL, 3), kCLK_IN_to_ADC0 = MUX_A(CM_ADC0CLKSEL, 4), kPLL1_CLK0_to_ADC0 = MUX_A(CM_ADC0CLKSEL, 5), kUSB_PLL_to_ADC0 = MUX_A(CM_ADC0CLKSEL, 6), kNONE_to_ADC0 = MUX_A(CM_ADC0CLKSEL, 7), kPLL0_to_USB0 = MUX_A(CM_USB0CLKSEL, 1), kCLK_48M_to_USB0 = MUX_A(CM_USB0CLKSEL, 3), kCLK_IN_to_USB0 = MUX_A(CM_USB0CLKSEL, 4), kPLL1_CLK0_to_USB0 = MUX_A(CM_USB0CLKSEL, 5), kUSB_PLL_to_USB0 = MUX_A(CM_USB0CLKSEL, 6), kNONE_to_USB0 = MUX_A(CM_USB0CLKSEL, 7), kPLL_DIV_to_FLEXCOMM0 = MUX_A(CM_FCCLKSEL0, 1), kFRO12M_to_FLEXCOMM0 = MUX_A(CM_FCCLKSEL0, 2), kFRO_HF_DIV_to_FLEXCOMM0 = MUX_A(CM_FCCLKSEL0, 3), kCLK_1M_to_FLEXCOMM0 = MUX_A(CM_FCCLKSEL0, 4), kUSB_PLL_to_FLEXCOMM0 = MUX_A(CM_FCCLKSEL0, 5), kLPOSC_to_FLEXCOMM0 = MUX_A(CM_FCCLKSEL0, 6), kNONE_to_FLEXCOMM0 = MUX_A(CM_FCCLKSEL0, 7), kPLL_DIV_to_FLEXCOMM1 = MUX_A(CM_FCCLKSEL1, 1), kFRO12M_to_FLEXCOMM1 = MUX_A(CM_FCCLKSEL1, 2), kFRO_HF_DIV_to_FLEXCOMM1 = MUX_A(CM_FCCLKSEL1, 3), kCLK_1M_to_FLEXCOMM1 = MUX_A(CM_FCCLKSEL1, 4), kUSB_PLL_to_FLEXCOMM1 = MUX_A(CM_FCCLKSEL1, 5), kLPOSC_to_FLEXCOMM1 = MUX_A(CM_FCCLKSEL1, 6), kNONE_to_FLEXCOMM1 = MUX_A(CM_FCCLKSEL1, 7), kPLL_DIV_to_FLEXCOMM2 = MUX_A(CM_FCCLKSEL2, 1), kFRO12M_to_FLEXCOMM2 = MUX_A(CM_FCCLKSEL2, 2), kFRO_HF_DIV_to_FLEXCOMM2 = MUX_A(CM_FCCLKSEL2, 3), kCLK_1M_to_FLEXCOMM2 = MUX_A(CM_FCCLKSEL2, 4), kUSB_PLL_to_FLEXCOMM2 = MUX_A(CM_FCCLKSEL2, 5), kLPOSC_to_FLEXCOMM2 = MUX_A(CM_FCCLKSEL2, 6), kNONE_to_FLEXCOMM2 = MUX_A(CM_FCCLKSEL2, 7), kPLL_DIV_to_FLEXCOMM3 = MUX_A(CM_FCCLKSEL3, 1), kFRO12M_to_FLEXCOMM3 = MUX_A(CM_FCCLKSEL3, 2), kFRO_HF_DIV_to_FLEXCOMM3 = MUX_A(CM_FCCLKSEL3, 3), kCLK_1M_to_FLEXCOMM3 = MUX_A(CM_FCCLKSEL3, 4), kUSB_PLL_to_FLEXCOMM3 = MUX_A(CM_FCCLKSEL3, 5), kLPOSC_to_FLEXCOMM3 = MUX_A(CM_FCCLKSEL3, 6), kNONE_to_FLEXCOMM3 = MUX_A(CM_FCCLKSEL3, 7), kPLL_DIV_to_FLEXCOMM4 = MUX_A(CM_FCCLKSEL4, 1), kFRO12M_to_FLEXCOMM4 = MUX_A(CM_FCCLKSEL4, 2), kFRO_HF_DIV_to_FLEXCOMM4 = MUX_A(CM_FCCLKSEL4, 3), kCLK_1M_to_FLEXCOMM4 = MUX_A(CM_FCCLKSEL4, 4), kUSB_PLL_to_FLEXCOMM4 = MUX_A(CM_FCCLKSEL4, 5), kLPOSC_to_FLEXCOMM4 = MUX_A(CM_FCCLKSEL4, 6), kNONE_to_FLEXCOMM4 = MUX_A(CM_FCCLKSEL4, 7), kPLL_DIV_to_FLEXCOMM5 = MUX_A(CM_FCCLKSEL5, 1), kFRO12M_to_FLEXCOMM5 = MUX_A(CM_FCCLKSEL5, 2), kFRO_HF_DIV_to_FLEXCOMM5 = MUX_A(CM_FCCLKSEL5, 3), kCLK_1M_to_FLEXCOMM5 = MUX_A(CM_FCCLKSEL5, 4), kUSB_PLL_to_FLEXCOMM5 = MUX_A(CM_FCCLKSEL5, 5), kLPOSC_to_FLEXCOMM5 = MUX_A(CM_FCCLKSEL5, 6), kNONE_to_FLEXCOMM5 = MUX_A(CM_FCCLKSEL5, 7), kPLL_DIV_to_FLEXCOMM6 = MUX_A(CM_FCCLKSEL6, 1), kFRO12M_to_FLEXCOMM6 = MUX_A(CM_FCCLKSEL6, 2), kFRO_HF_DIV_to_FLEXCOMM6 = MUX_A(CM_FCCLKSEL6, 3), kCLK_1M_to_FLEXCOMM6 = MUX_A(CM_FCCLKSEL6, 4), kUSB_PLL_to_FLEXCOMM6 = MUX_A(CM_FCCLKSEL6, 5), kLPOSC_to_FLEXCOMM6 = MUX_A(CM_FCCLKSEL6, 6), kNONE_to_FLEXCOMM6 = MUX_A(CM_FCCLKSEL6, 7), kPLL_DIV_to_FLEXCOMM7 = MUX_A(CM_FCCLKSEL7, 1), kFRO12M_to_FLEXCOMM7 = MUX_A(CM_FCCLKSEL7, 2), kFRO_HF_DIV_to_FLEXCOMM7 = MUX_A(CM_FCCLKSEL7, 3), kCLK_1M_to_FLEXCOMM7 = MUX_A(CM_FCCLKSEL7, 4), kUSB_PLL_to_FLEXCOMM7 = MUX_A(CM_FCCLKSEL7, 5), kLPOSC_to_FLEXCOMM7 = MUX_A(CM_FCCLKSEL7, 6), kNONE_to_FLEXCOMM7 = MUX_A(CM_FCCLKSEL7, 7), kPLL_DIV_to_FLEXCOMM8 = MUX_A(CM_FCCLKSEL8, 1), kFRO12M_to_FLEXCOMM8 = MUX_A(CM_FCCLKSEL8, 2), kFRO_HF_DIV_to_FLEXCOMM8 = MUX_A(CM_FCCLKSEL8, 3), kCLK_1M_to_FLEXCOMM8 = MUX_A(CM_FCCLKSEL8, 4), kUSB_PLL_to_FLEXCOMM8 = MUX_A(CM_FCCLKSEL8, 5), kLPOSC_to_FLEXCOMM8 = MUX_A(CM_FCCLKSEL8, 6), kNONE_to_FLEXCOMM8 = MUX_A(CM_FCCLKSEL8, 7), kPLL_DIV_to_FLEXCOMM9 = MUX_A(CM_FCCLKSEL9, 1), kFRO12M_to_FLEXCOMM9 = MUX_A(CM_FCCLKSEL9, 2), kFRO_HF_DIV_to_FLEXCOMM9 = MUX_A(CM_FCCLKSEL9, 3), kCLK_1M_to_FLEXCOMM9 = MUX_A(CM_FCCLKSEL9, 4), kUSB_PLL_to_FLEXCOMM9 = MUX_A(CM_FCCLKSEL9, 5), kLPOSC_to_FLEXCOMM9 = MUX_A(CM_FCCLKSEL9, 6), kNONE_to_FLEXCOMM9 = MUX_A(CM_FCCLKSEL9, 7), kPLL0_to_SCT = MUX_A(CM_SCTCLKSEL, 1), kCLK_IN_to_SCT = MUX_A(CM_SCTCLKSEL, 2), kFRO_HF_to_SCT = MUX_A(CM_SCTCLKSEL, 3), kPLL1_CLK0_to_SCT = MUX_A(CM_SCTCLKSEL, 4), kSAI0_MCLK_IN_to_SCT = MUX_A(CM_SCTCLKSEL, 5), kUSB_PLL_to_SCT = MUX_A(CM_SCTCLKSEL, 6), kSAI1_MCLK_IN_to_SCT = MUX_A(CM_SCTCLKSEL, 8), kNONE_to_SCT = MUX_A(CM_SCTCLKSEL, 15), kCLK_IN_to_TSI = MUX_A(CM_TSICLKSEL, 2), kFRO12M_to_TSI = MUX_A(CM_TSICLKSEL, 4), kNONE_to_TSI = MUX_A(CM_TSICLKSEL, 7), kPLL0_to_SINCFILT = MUX_A(CM_SINCFILTCLKSEL, 1), kCLK_IN_to_SINCFILT = MUX_A(CM_SINCFILTCLKSEL, 2), kFRO_HF_to_SINCFILT = MUX_A(CM_SINCFILTCLKSEL, 3), kFRO12M_to_SINCFILT = MUX_A(CM_SINCFILTCLKSEL, 4), kPLL1_CLK0_to_SINCFILT = MUX_A(CM_SINCFILTCLKSEL, 5), kUSB_PLL_to_SINCFILT = MUX_A(CM_SINCFILTCLKSEL, 6), kNONE_to_SINCFILT = MUX_A(CM_SINCFILTCLKSEL, 7), kPLL0_to_ADC1 = MUX_A(CM_ADC1CLKSEL, 1), kFRO_HF_to_ADC1 = MUX_A(CM_ADC1CLKSEL, 2), kFRO12M_to_ADC1 = MUX_A(CM_ADC1CLKSEL, 3), kCLK_IN_to_ADC1 = MUX_A(CM_ADC1CLKSEL, 4), kPLL1_CLK0_to_ADC1 = MUX_A(CM_ADC1CLKSEL, 5), kUSB_PLL_to_ADC1 = MUX_A(CM_ADC1CLKSEL, 6), kNONE_to_ADC1 = MUX_A(CM_ADC1CLKSEL, 7), kPLL0_to_DAC0 = MUX_A(CM_DAC0CLKSEL, 1), kCLK_IN_to_DAC0 = MUX_A(CM_DAC0CLKSEL, 2), kFRO_HF_to_DAC0 = MUX_A(CM_DAC0CLKSEL, 3), kFRO12M_to_DAC0 = MUX_A(CM_DAC0CLKSEL, 4), kPLL1_CLK0_to_DAC0 = MUX_A(CM_DAC0CLKSEL, 5), kNONE_to_DAC0 = MUX_A(CM_DAC0CLKSEL, 7), kPLL0_to_DAC1 = MUX_A(CM_DAC1CLKSEL, 1), kCLK_IN_to_DAC1 = MUX_A(CM_DAC1CLKSEL, 2), kFRO_HF_to_DAC1 = MUX_A(CM_DAC1CLKSEL, 3), kFRO12M_to_DAC1 = MUX_A(CM_DAC1CLKSEL, 4), kPLL1_CLK0_to_DAC1 = MUX_A(CM_DAC1CLKSEL, 5), kNONE_to_DAC1 = MUX_A(CM_DAC1CLKSEL, 7), kPLL0_to_DAC2 = MUX_A(CM_DAC2CLKSEL, 1), kCLK_IN_to_DAC2 = MUX_A(CM_DAC2CLKSEL, 2), kFRO_HF_to_DAC2 = MUX_A(CM_DAC2CLKSEL, 3), kFRO12M_to_DAC2 = MUX_A(CM_DAC2CLKSEL, 4), kPLL1_CLK0_to_DAC2 = MUX_A(CM_DAC2CLKSEL, 5), kNONE_to_DAC2 = MUX_A(CM_DAC2CLKSEL, 7), kPLL0_to_FLEXSPI = MUX_A(CM_FLEXSPICLKSEL, 1), kFRO_HF_to_FLEXSPI = MUX_A(CM_FLEXSPICLKSEL, 3), kPLL1_to_FLEXSPI = MUX_A(CM_FLEXSPICLKSEL, 5), kUSB_PLL_to_FLEXSPI = MUX_A(CM_FLEXSPICLKSEL, 6), kNONE_to_FLEXSPI = MUX_A(CM_FLEXSPICLKSEL, 15), kPLL0_to_PLLCLKDIV = MUX_A(CM_PLLCLKDIVSEL, 0), kPLL1_CLK0_to_PLLCLKDIV = MUX_A(CM_PLLCLKDIVSEL, 1), kNONE_to_PLLCLKDIV = MUX_A(CM_PLLCLKDIVSEL, 1), kPLL0_to_I3C0FCLK = MUX_A(CM_I3C0FCLKSEL, 1), kCLK_IN_to_I3C0FCLK = MUX_A(CM_I3C0FCLKSEL, 2), kFRO_HF_to_I3C0FCLK = MUX_A(CM_I3C0FCLKSEL, 3), kPLL1_CLK0_to_I3C0FCLK = MUX_A(CM_I3C0FCLKSEL, 5), kUSB_PLL_to_I3C0FCLK = MUX_A(CM_I3C0FCLKSEL, 6), kNONE_to_I3C0FCLK = MUX_A(CM_I3C0FCLKSEL, 7), kI3C0FCLK_to_I3C0FCLKSTC = MUX_A(CM_I3C0FCLKSTCSEL, 0), kCLK_1M_to_I3C0FCLKSTC = MUX_A(CM_I3C0FCLKSTCSEL, 1), kNONE_to_I3C0FCLKSTC = MUX_A(CM_I3C0FCLKSTCSEL, 7), kCLK_1M_to_I3C0FCLKS = MUX_A(CM_I3C0FCLKSSEL, 0), kNONE_to_I3C0FCLKS = MUX_A(CM_I3C0FCLKSSEL, 7), kFRO12M_to_MICFILF = MUX_A(CM_MICFILFCLKSEL, 0), kPLL0_to_MICFILF = MUX_A(CM_MICFILFCLKSEL, 1), kCLK_IN_to_MICFILF = MUX_A(CM_MICFILFCLKSEL, 2), kFRO_HF_to_MICFILF = MUX_A(CM_MICFILFCLKSEL, 3), kPLL1_CLK0_to_MICFILF = MUX_A(CM_MICFILFCLKSEL, 4), kSAI0_MCLK_IN_to_MICFILF = MUX_A(CM_MICFILFCLKSEL, 5), kUSB_PLL_to_MICFILF = MUX_A(CM_MICFILFCLKSEL, 6), kSAI1_MCLK_IN_to_MICFILF = MUX_A(CM_MICFILFCLKSEL, 8), kNONE_to_MICFILF = MUX_A(CM_MICFILFCLKSEL, 15), kPLL0_to_ESPI = MUX_A(CM_ESPICLKSEL, 1), kCLK_48M_to_ESPI = MUX_A(CM_ESPICLKSEL, 3), kPLL1_CLK0_to_ESPI = MUX_A(CM_ESPICLKSEL, 5), kUSB_PLL_to_ESPI = MUX_A(CM_ESPICLKSEL, 6), kNONE_to_ESPI = MUX_A(CM_ESPICLKSEL, 7), kPLL0_to_USDHC = MUX_A(CM_USDHCCLKSEL, 1), kCLK_IN_to_USDHC = MUX_A(CM_USDHCCLKSEL, 2), kFRO_HF_to_USDHC = MUX_A(CM_USDHCCLKSEL, 3), kFRO12M_to_USDHC = MUX_A(CM_USDHCCLKSEL, 4), kPLL1_CLK1_to_USDHC = MUX_A(CM_USDHCCLKSEL, 5), kUSB_PLL_to_USDHC = MUX_A(CM_USDHCCLKSEL, 6), kNONE_to_USDHC = MUX_A(CM_USDHCCLKSEL, 7), kPLL0_to_FLEXIO = MUX_A(CM_FLEXIOCLKSEL, 1), kCLK_IN_to_FLEXIO = MUX_A(CM_FLEXIOCLKSEL, 2), kFRO_HF_to_FLEXIO = MUX_A(CM_FLEXIOCLKSEL, 3), kFRO12M_to_FLEXIO = MUX_A(CM_FLEXIOCLKSEL, 4), kPLL1_CLK0_to_FLEXIO = MUX_A(CM_FLEXIOCLKSEL, 5), kUSB_PLL_to_FLEXIO = MUX_A(CM_FLEXIOCLKSEL, 6), kNONE_to_FLEXIO = MUX_A(CM_FLEXIOCLKSEL, 7), kPLL0_to_FLEXCAN0 = MUX_A(CM_FLEXCAN0CLKSEL, 1), kCLK_IN_to_FLEXCAN0 = MUX_A(CM_FLEXCAN0CLKSEL, 2), kFRO_HF_to_FLEXCAN0 = MUX_A(CM_FLEXCAN0CLKSEL, 3), kPLL1_CLK0_to_FLEXCAN0 = MUX_A(CM_FLEXCAN0CLKSEL, 5), kUSB_PLL_to_FLEXCAN0 = MUX_A(CM_FLEXCAN0CLKSEL, 6), kNONE_to_FLEXCAN0 = MUX_A(CM_FLEXCAN0CLKSEL, 7), kPLL0_to_FLEXCAN1 = MUX_A(CM_FLEXCAN1CLKSEL, 1), kCLK_IN_to_FLEXCAN1 = MUX_A(CM_FLEXCAN1CLKSEL, 2), kFRO_HF_to_FLEXCAN1 = MUX_A(CM_FLEXCAN1CLKSEL, 3), kPLL1_CLK0_to_FLEXCAN1 = MUX_A(CM_FLEXCAN1CLKSEL, 5), kUSB_PLL_to_FLEXCAN1 = MUX_A(CM_FLEXCAN1CLKSEL, 6), kNONE_to_FLEXCAN1 = MUX_A(CM_FLEXCAN1CLKSEL, 7), kNONE_to_ENETRMII = MUX_A(CM_ENETRMIICLKSEL, 0), kPLL0_to_ENETRMII = MUX_A(CM_ENETRMIICLKSEL, 1), kCLK_IN_to_ENETRMII = MUX_A(CM_ENETRMIICLKSEL, 2), kPLL1_CLK0_to_ENETRMII = MUX_A(CM_ENETRMIICLKSEL, 5), kPLL0_to_ENETPTPREF = MUX_A(CM_ENETPTPREFCLKSEL, 1), kCLK_IN_to_ENETPTPREF = MUX_A(CM_ENETPTPREFCLKSEL, 2), kENET0_TX_CLK_to_ENETPTPREF = MUX_A(CM_ENETPTPREFCLKSEL, 4), kPLL1_CLK1_to_ENETPTPREF = MUX_A(CM_ENETPTPREFCLKSEL, 5), kNONE_to_ENETPTPREF = MUX_A(CM_ENETPTPREFCLKSEL, 7), kCLK_16K2_to_EWM0 = MUX_A(CM_EWM0CLKSEL, 0), kXTAL32K2_to_EWM0 = MUX_A(CM_EWM0CLKSEL, 1), kCLK_16K2_to_WDT1 = MUX_A(CM_WDT1CLKSEL, 0), kFRO_HF_DIV_to_WDT1 = MUX_A(CM_WDT1CLKSEL, 1), kCLK_1M_to_WDT1 = MUX_A(CM_WDT1CLKSEL, 2), kCLK_1M_2_to_WDT1 = MUX_A(CM_WDT1CLKSEL, 3), kCLK_16K2_to_OSTIMER = MUX_A(CM_OSTIMERCLKSEL, 0), kXTAL32K2_to_OSTIMER = MUX_A(CM_OSTIMERCLKSEL, 1), kCLK_1M_to_OSTIMER = MUX_A(CM_OSTIMERCLKSEL, 2), kNONE_to_OSTIMER = MUX_A(CM_OSTIMERCLKSEL, 3), kPLL0_to_CMP0F = MUX_A(CM_CMP0FCLKSEL, 1), kFRO_HF_to_CMP0F = MUX_A(CM_CMP0FCLKSEL, 2), kFRO12M_to_CMP0F = MUX_A(CM_CMP0FCLKSEL, 3), kCLK_IN_to_CMP0F = MUX_A(CM_CMP0FCLKSEL, 4), kPLL1_CLK0_to_CMP0F = MUX_A(CM_CMP0FCLKSEL, 5), kUSB_PLL_to_CMP0F = MUX_A(CM_CMP0FCLKSEL, 6), kNONE_to_CMP0F = MUX_A(CM_CMP0FCLKSEL, 7), kPLL0_to_CMP0RR = MUX_A(CM_CMP0RRCLKSEL, 1), kFRO_HF_to_CMP0RR = MUX_A(CM_CMP0RRCLKSEL, 2), kFRO12M_to_CMP0RR = MUX_A(CM_CMP0RRCLKSEL, 3), kCLK_IN_to_CMP0RR = MUX_A(CM_CMP0RRCLKSEL, 4), kPLL1_CLK0_to_CMP0RR = MUX_A(CM_CMP0RRCLKSEL, 5), kUSB_PLL_to_CMP0RR = MUX_A(CM_CMP0RRCLKSEL, 6), kNONE_to_CMP0RR = MUX_A(CM_CMP0RRCLKSEL, 7), kPLL0_to_CMP1F = MUX_A(CM_CMP1FCLKSEL, 1), kFRO_HF_to_CMP1F = MUX_A(CM_CMP1FCLKSEL, 2), kFRO12M_to_CMP1F = MUX_A(CM_CMP1FCLKSEL, 3), kCLK_IN_to_CMP1F = MUX_A(CM_CMP1FCLKSEL, 4), kPLL1_CLK0_to_CMP1F = MUX_A(CM_CMP1FCLKSEL, 5), kUSB_PLL_to_CMP1F = MUX_A(CM_CMP1FCLKSEL, 6), kNONE_to_CMP1F = MUX_A(CM_CMP1FCLKSEL, 7), kPLL0_to_CMP1RR = MUX_A(CM_CMP1RRCLKSEL, 1), kFRO_HF_to_CMP1RR = MUX_A(CM_CMP1RRCLKSEL, 2), kFRO12M_to_CMP1RR = MUX_A(CM_CMP1RRCLKSEL, 3), kCLK_IN_to_CMP1RR = MUX_A(CM_CMP1RRCLKSEL, 4), kPLL1_CLK0_to_CMP1RR = MUX_A(CM_CMP1RRCLKSEL, 5), kUSB_PLL_to_CMP1RR = MUX_A(CM_CMP1RRCLKSEL, 6), kNONE_to_CMP1RR = MUX_A(CM_CMP1RRCLKSEL, 7), kPLL0_to_CMP2F = MUX_A(CM_CMP2FCLKSEL, 1), kFRO_HF_to_CMP2F = MUX_A(CM_CMP2FCLKSEL, 2), kFRO12M_to_CMP2F = MUX_A(CM_CMP2FCLKSEL, 3), kCLK_IN_to_CMP2F = MUX_A(CM_CMP2FCLKSEL, 4), kPLL1_CLK0_to_CMP2F = MUX_A(CM_CMP2FCLKSEL, 5), kUSB_PLL_to_CMP2F = MUX_A(CM_CMP2FCLKSEL, 6), kNONE_to_CMP2F = MUX_A(CM_CMP2FCLKSEL, 7), kPLL0_to_CMP2RR = MUX_A(CM_CMP2RRCLKSEL, 1), kFRO_HF_to_CMP2RR = MUX_A(CM_CMP2RRCLKSEL, 2), kFRO12M_to_CMP2RR = MUX_A(CM_CMP2RRCLKSEL, 3), kCLK_IN_to_CMP2RR = MUX_A(CM_CMP2RRCLKSEL, 4), kPLL1_CLK0_to_CMP2RR = MUX_A(CM_CMP2RRCLKSEL, 5), kUSB_PLL_to_CMP2RR = MUX_A(CM_CMP2RRCLKSEL, 6), kNONE_to_CMP2RR = MUX_A(CM_CMP2RRCLKSEL, 7), kPLL0_to_SAI0 = MUX_A(CM_SAI0CLKSEL, 1), kCLK_IN_to_SAI0 = MUX_A(CM_SAI0CLKSEL, 2), kFRO_HF_to_SAI0 = MUX_A(CM_SAI0CLKSEL, 3), kPLL1_CLK0_to_SAI0 = MUX_A(CM_SAI0CLKSEL, 4), kUSB_PLL_to_SAI0 = MUX_A(CM_SAI0CLKSEL, 6), kNONE_to_SAI0 = MUX_A(CM_SAI0CLKSEL, 7), kPLL0_to_SAI1 = MUX_A(CM_SAI1CLKSEL, 1), kCLK_IN_to_SAI1 = MUX_A(CM_SAI1CLKSEL, 2), kFRO_HF_to_SAI1 = MUX_A(CM_SAI1CLKSEL, 3), kPLL1_CLK0_to_SAI1 = MUX_A(CM_SAI1CLKSEL, 4), kUSB_PLL_to_SAI1 = MUX_A(CM_SAI1CLKSEL, 6), kNONE_to_SAI1 = MUX_A(CM_SAI1CLKSEL, 7), kPLL0_to_EMVSIM0 = MUX_A(CM_EMVSIM0CLKSEL, 1), kCLK_IN_to_EMVSIM0 = MUX_A(CM_EMVSIM0CLKSEL, 2), kFRO_HF_to_EMVSIM0 = MUX_A(CM_EMVSIM0CLKSEL, 3), kFRO12M_to_EMVSIM0 = MUX_A(CM_EMVSIM0CLKSEL, 4), kPLL1_CLK0_to_EMVSIM0 = MUX_A(CM_EMVSIM0CLKSEL, 5), kNONE_to_EMVSIM0 = MUX_A(CM_EMVSIM0CLKSEL, 7), kPLL0_to_EMVSIM1 = MUX_A(CM_EMVSIM1CLKSEL, 1), kCLK_IN_to_EMVSIM1 = MUX_A(CM_EMVSIM1CLKSEL, 2), kFRO_HF_to_EMVSIM1 = MUX_A(CM_EMVSIM1CLKSEL, 3), kFRO12M_to_EMVSIM1 = MUX_A(CM_EMVSIM1CLKSEL, 4), kPLL1_CLK0_to_EMVSIM1 = MUX_A(CM_EMVSIM1CLKSEL, 5), kNONE_to_EMVSIM1 = MUX_A(CM_EMVSIM1CLKSEL, 7), kPLL0_to_I3C1FCLK = MUX_A(CM_I3C1FCLKSEL, 1), kCLK_IN_to_I3C1FCLK = MUX_A(CM_I3C1FCLKSEL, 2), kFRO_HF_to_I3C1FCLK = MUX_A(CM_I3C1FCLKSEL, 3), kPLL1_CLK0_to_I3C1FCLK = MUX_A(CM_I3C1FCLKSEL, 5), kUSB_PLL_to_I3C1FCLK = MUX_A(CM_I3C1FCLKSEL, 6), kNONE_to_I3C1FCLK = MUX_A(CM_I3C1FCLKSEL, 7), kI3C1FCLK_to_I3C1FCLKSTC = MUX_A(CM_I3C1FCLKSTCSEL, 0), kCLK_1M_to_I3C1FCLKSTC = MUX_A(CM_I3C1FCLKSTCSEL, 1), kNONE_to_I3C1FCLKSTC = MUX_A(CM_I3C1FCLKSTCSEL, 7), kCLK_1M_to_I3C1FCLKS = MUX_A(CM_I3C1FCLKSSEL, 0), kNONE_to_I3C1FCLKS = MUX_A(CM_I3C1FCLKSSEL, 7), kNONE_to_NONE = (int)0x80000000U } |
| The enumerator of clock attach Id. More... | |
| enum | clock_div_name_t { kCLOCK_DivSystickClk0 = 0, kCLOCK_DivSystickClk1 = ((0x304 - 0x300) / 4), kCLOCK_DivTraceClk = ((0x308 - 0x300) / 4), kCLOCK_DivSlowClk = ((0x378 - 0x300) / 4), kCLOCK_DivTsiClk = ((0x37C - 0x300) / 4), kCLOCK_DivAhbClk = ((0x380 - 0x300) / 4), kCLOCK_DivClkOut = ((0x384 - 0x300) / 4), kCLOCK_DivFrohfClk = ((0x388 - 0x300) / 4), kCLOCK_DivWdt0Clk = ((0x38C - 0x300) / 4), kCLOCK_DivAdc0Clk = ((0x394 - 0x300) / 4), kCLOCK_DivUsb0Clk = ((0x398 - 0x300) / 4), kCLOCK_DivSctClk = ((0x3B4 - 0x300) / 4), kCLOCK_DivPllClk = ((0x3C4 - 0x300) / 4), kCLOCK_DivCtimer0Clk = ((0x3D0 - 0x300) / 4), kCLOCK_DivCtimer1Clk = ((0x3D4 - 0x300) / 4), kCLOCK_DivCtimer2Clk = ((0x3D8 - 0x300) / 4), kCLOCK_DivCtimer3Clk = ((0x3DC - 0x300) / 4), kCLOCK_DivCtimer4Clk = ((0x3E0 - 0x300) / 4), kCLOCK_DivPLL1Clk0 = ((0x3E4 - 0x300) / 4), kCLOCK_DivPLL1Clk1 = ((0x3E8 - 0x300) / 4), kCLOCK_DivAdc1Clk = ((0x468 - 0x300) / 4), kCLOCK_DivDac0Clk = ((0x494 - 0x300) / 4), kCLOCK_DivDac1Clk = ((0x49C - 0x300) / 4), kCLOCK_DivDac2Clk = ((0x4A4 - 0x300) / 4), kCLOCK_DivFlexspiClk = ((0x4AC - 0x300) / 4), kCLOCK_DivI3c0FClkStc = ((0x538 - 0x300) / 4), kCLOCK_DivI3c0FClkS = ((0x53C - 0x300) / 4), kCLOCK_DivI3c0FClk = ((0x540 - 0x300) / 4), kCLOCK_DivMicfilFClk = ((0x54C - 0x300) / 4), kCLOCK_DivEspiClk = ((0x554 - 0x300) / 4), kCLOCK_DivUSdhcClk = ((0x55C - 0x300) / 4), kCLOCK_DivFlexioClk = ((0x564 - 0x300) / 4), kCLOCK_DivFlexcan0Clk = ((0x5A4 - 0x300) / 4), kCLOCK_DivFlexcan1Clk = ((0x5AC - 0x300) / 4), kCLOCK_DivEnetrmiiClk = ((0x5B4 - 0x300) / 4), kCLOCK_DivEnetptprefClk = ((0x5BC - 0x300) / 4), kCLOCK_DivWdt1Clk = ((0x5DC - 0x300) / 4), kCLOCK_DivCmp0FClk = ((0x5F4 - 0x300) / 4), kCLOCK_DivCmp0rrClk = ((0x5FC - 0x300) / 4), kCLOCK_DivCmp1FClk = ((0x604 - 0x300) / 4), kCLOCK_DivCmp1rrClk = ((0x60C - 0x300) / 4), kCLOCK_DivCmp2FClk = ((0x614 - 0x300) / 4), kCLOCK_DivCmp2rrClk = ((0x61C - 0x300) / 4), kCLOCK_DivFlexcom0Clk = ((0x850 - 0x300) / 4), kCLOCK_DivFlexcom1Clk = ((0x854 - 0x300) / 4), kCLOCK_DivFlexcom2Clk = ((0x858 - 0x300) / 4), kCLOCK_DivFlexcom3Clk = ((0x85C - 0x300) / 4), kCLOCK_DivFlexcom4Clk = ((0x860 - 0x300) / 4), kCLOCK_DivFlexcom5Clk = ((0x864 - 0x300) / 4), kCLOCK_DivFlexcom6Clk = ((0x868 - 0x300) / 4), kCLOCK_DivFlexcom7Clk = ((0x86C - 0x300) / 4), kCLOCK_DivFlexcom8Clk = ((0x870 - 0x300) / 4), kCLOCK_DivFlexcom9Clk = ((0x874 - 0x300) / 4), kCLOCK_DivSai0Clk = ((0x888 - 0x300) / 4), kCLOCK_DivSai1Clk = ((0x88C - 0x300) / 4), kCLOCK_DivEmvsim0Clk = ((0x898 - 0x300) / 4), kCLOCK_DivEmvsim1Clk = ((0x89C - 0x300) / 4), kCLOCK_DivI3c1FClkStc = ((0xB38 - 0x300) / 4), kCLOCK_DivI3c1FClkS = ((0xB3C - 0x300) / 4), kCLOCK_DivI3c1FClk = ((0xB40 - 0x300) / 4) } |
| Clock dividers. More... | |
| enum | osc32k_clk_gate_id_t { kCLOCK_Osc32kToVbat = 0x1, kCLOCK_Osc32kToVsys = 0x2, kCLOCK_Osc32kToWake = 0x4, kCLOCK_Osc32kToMain = 0x8, kCLOCK_Osc32kToAll = 0xF } |
| OSC32K clock gate. More... | |
| enum | clk16k_clk_gate_id_t { kCLOCK_Clk16KToVbat = 0x1, kCLOCK_Clk16KToVsys = 0x2, kCLOCK_Clk16KToWake = 0x4, kCLOCK_Clk16KToMain = 0x8, kCLOCK_Clk16KToAll = 0xF } |
| CLK16K clock gate. More... | |
| enum | clock_ctrl_enable_t { kCLOCK_PLU_DEGLITCH_CLK_ENA, kCLOCK_FRO1MHZ_CLK_ENA, kCLOCK_CLKIN_ENA, kCLOCK_FRO_HF_ENA, kCLOCK_FRO12MHZ_ENA = SYSCON_CLOCK_CTRL_FRO12MHZ_ENA_MASK, kCLOCK_FRO1MHZ_ENA, kCLOCK_CLKIN_ENA_FM_USBH_LPT } |
| system clocks enable controls More... | |
| enum | clock_usb_phy_src_t { kCLOCK_Usbphy480M = 0 } |
| Source of the USB HS PHY. More... | |
| enum | _scg_status { kStatus_SCG_Busy = MAKE_STATUS(kStatusGroup_SCG, 1), kStatus_SCG_InvalidSrc = MAKE_STATUS(kStatusGroup_SCG, 2) } |
| SCG status return codes. More... | |
| enum | firc_trim_mode_t { kSCG_FircTrimNonUpdate = SCG_FIRCCSR_FIRCTREN_MASK, kSCG_FircTrimUpdate = SCG_FIRCCSR_FIRCTREN_MASK | SCG_FIRCCSR_FIRCTRUP_MASK } |
| firc trim mode. More... | |
| enum | firc_trim_src_t { kSCG_FircTrimSrcUsb0 = 0U, kSCG_FircTrimSrcSysOsc = 2U, kSCG_FircTrimSrcRtcOsc = 3U } |
| firc trim source. More... | |
| enum | sirc_trim_mode_t { kSCG_SircTrimNonUpdate = SCG_SIRCCSR_SIRCTREN_MASK, kSCG_SircTrimUpdate = SCG_SIRCCSR_SIRCTREN_MASK | SCG_SIRCCSR_SIRCTRUP_MASK } |
| sirc trim mode. More... | |
| enum | sirc_trim_src_t { kSCG_SircTrimSrcSysOsc = 2U, kSCG_SircTrimSrcRtcOsc = 3U } |
| sirc trim source. More... | |
| enum | scg_sosc_monitor_mode_t { kSCG_SysOscMonitorDisable = 0U, kSCG_SysOscMonitorInt = SCG_SOSCCSR_SOSCCM_MASK, kSCG_SysOscMonitorReset } |
| SCG system OSC monitor mode. More... | |
| enum | scg_rosc_monitor_mode_t { kSCG_RoscMonitorDisable = 0U, kSCG_RoscMonitorInt = SCG_ROSCCSR_ROSCCM_MASK, kSCG_RoscMonitorReset } |
| SCG ROSC monitor mode. More... | |
| enum | scg_upll_monitor_mode_t { kSCG_UpllMonitorDisable = 0U, kSCG_UpllMonitorInt = SCG_UPLLCSR_UPLLCM_MASK, kSCG_UpllMonitorReset } |
| SCG UPLL monitor mode. More... | |
| enum | scg_pll0_monitor_mode_t { kSCG_Pll0MonitorDisable = 0U, kSCG_Pll0MonitorInt = SCG_APLLCSR_APLLCM_MASK, kSCG_Pll0MonitorReset } |
| SCG PLL0 monitor mode. More... | |
| enum | scg_pll1_monitor_mode_t { kSCG_Pll1MonitorDisable = 0U, kSCG_Pll1MonitorInt = SCG_SPLLCSR_SPLLCM_MASK, kSCG_Pll1MonitorReset } |
| SCG PLL1 monitor mode. More... | |
| enum | vbat_osc_xtal_cap_t { kVBAT_OscXtal0pFCap = 0x0U, kVBAT_OscXtal2pFCap = 0x1U, kVBAT_OscXtal4pFCap = 0x2U, kVBAT_OscXtal6pFCap = 0x3U, kVBAT_OscXtal8pFCap = 0x4U, kVBAT_OscXtal10pFCap = 0x5U, kVBAT_OscXtal12pFCap = 0x6U, kVBAT_OscXtal14pFCap = 0x7U, kVBAT_OscXtal16pFCap = 0x8U, kVBAT_OscXtal18pFCap = 0x9U, kVBAT_OscXtal20pFCap = 0xAU, kVBAT_OscXtal22pFCap = 0xBU, kVBAT_OscXtal24pFCap = 0xCU, kVBAT_OscXtal26pFCap = 0xDU, kVBAT_OscXtal28pFCap = 0xEU, kVBAT_OscXtal30pFCap = 0xFU } |
| The enumerator of internal capacitance of OSC's XTAL pin. More... | |
| enum | vbat_osc_extal_cap_t { kVBAT_OscExtal0pFCap = 0x0U, kVBAT_OscExtal2pFCap = 0x1U, kVBAT_OscExtal4pFCap = 0x2U, kVBAT_OscExtal6pFCap = 0x3U, kVBAT_OscExtal8pFCap = 0x4U, kVBAT_OscExtal10pFCap = 0x5U, kVBAT_OscExtal12pFCap = 0x6U, kVBAT_OscExtal14pFCap = 0x7U, kVBAT_OscExtal16pFCap = 0x8U, kVBAT_OscExtal18pFCap = 0x9U, kVBAT_OscExtal20pFCap = 0xAU, kVBAT_OscExtal22pFCap = 0xBU, kVBAT_OscExtal24pFCap = 0xCU, kVBAT_OscExtal26pFCap = 0xDU, kVBAT_OscExtal28pFCap = 0xEU, kVBAT_OscExtal30pFCap = 0xFU } |
| The enumerator of internal capacitance of OSC's EXTAL pin. More... | |
| enum | vbat_osc_coarse_adjustment_value_t |
| The enumerator of osc amplifier gain fine adjustment. More... | |
| enum | run_mode_t { kMD_Mode, kSD_Mode, kOD_Mode } |
| The active run mode (voltage level). More... | |
| enum | pll_clk_src_t { kPll_ClkSrcSysOsc = (0 << 25), kPll_ClkSrcFirc = (1 << 25), kPll_ClkSrcRosc = (2 << 25) } |
| PLL clock source. More... | |
| enum | ss_progmodfm_t { kSS_MF_512 = (0 << 2), kSS_MF_384 = (1 << 2), kSS_MF_256 = (2 << 2), kSS_MF_128 = (3 << 2), kSS_MF_64 = (4 << 2), kSS_MF_32 = (5 << 2), kSS_MF_24 = (6 << 2), kSS_MF_16 = (7 << 2) } |
| PLL Spread Spectrum (SS) Programmable modulation frequency See (MF) field in the PLL0SSCG1 register in the UM. More... | |
| enum | ss_progmoddp_t { kSS_MR_K0 = (0 << 5), kSS_MR_K1 = (1 << 5), kSS_MR_K1_5 = (2 << 5), kSS_MR_K2 = (3 << 5), kSS_MR_K3 = (4 << 5), kSS_MR_K4 = (5 << 5), kSS_MR_K6 = (6 << 5), kSS_MR_K8 = (7 << 5) } |
| PLL Spread Spectrum (SS) Programmable frequency modulation depth See (MR) field in the PLL0SSCG1 register in the UM. More... | |
| enum | ss_modwvctrl_t { kSS_MC_NOC = (0 << 8), kSS_MC_RECC = (2 << 8), kSS_MC_MAXC = (3 << 8) } |
| PLL Spread Spectrum (SS) Modulation waveform control See (MC) field in the PLL0SSCG1 register in the UM. More... | |
| enum | pll_error_t { kStatus_PLL_Success = MAKE_STATUS(kStatusGroup_Generic, 0), kStatus_PLL_OutputTooLow = MAKE_STATUS(kStatusGroup_Generic, 1), kStatus_PLL_OutputTooHigh = MAKE_STATUS(kStatusGroup_Generic, 2), kStatus_PLL_OutputError = MAKE_STATUS(kStatusGroup_Generic, 3), kStatus_PLL_InputTooLow = MAKE_STATUS(kStatusGroup_Generic, 4), kStatus_PLL_InputTooHigh = MAKE_STATUS(kStatusGroup_Generic, 5), kStatus_PLL_OutsideIntLimit = MAKE_STATUS(kStatusGroup_Generic, 6), kStatus_PLL_CCOTooLow = MAKE_STATUS(kStatusGroup_Generic, 7), kStatus_PLL_CCOTooHigh = MAKE_STATUS(kStatusGroup_Generic, 8) } |
| PLL status definitions. More... | |
Functions | |
| static void | CLOCK_EnableClock (clock_ip_name_t clk) |
| Enable the clock for specific IP. More... | |
| static void | CLOCK_DisableClock (clock_ip_name_t clk) |
| Disable the clock for specific IP. More... | |
| status_t | CLOCK_SetupFROHFClocking (uint32_t iFreq) |
| Initialize the Core clock to given frequency (48 or 144 MHz). This function turns on FIRC and select the given frequency as the source of fro_hf. More... | |
| status_t | CLOCK_SetupExtClocking (uint32_t iFreq) |
| Initialize the external osc clock to given frequency. More... | |
| status_t | CLOCK_SetupExtRefClocking (uint32_t iFreq) |
| Initialize the external reference clock to given frequency. More... | |
| status_t | CLOCK_SetupOsc32KClocking (uint32_t id) |
| Initialize the XTAL32/EXTAL32 input clock to given frequency. More... | |
| status_t | CLOCK_SetupClk16KClocking (uint32_t id) |
| Initialize the FRO16K input clock to given frequency. More... | |
| status_t | CLOCK_FROHFTrimConfig (firc_trim_config_t config) |
| Setup FROHF trim. More... | |
| status_t | CLOCK_FRO12MTrimConfig (sirc_trim_config_t config) |
| Setup FRO 12M trim. More... | |
| void | CLOCK_SetSysOscMonitorMode (scg_sosc_monitor_mode_t mode) |
| Sets the system OSC monitor mode. More... | |
| void | CLOCK_SetRoscMonitorMode (scg_rosc_monitor_mode_t mode) |
| Sets the ROSC monitor mode. More... | |
| void | CLOCK_SetUpllMonitorMode (scg_upll_monitor_mode_t mode) |
| Sets the UPLL monitor mode. More... | |
| void | CLOCK_SetPll0MonitorMode (scg_pll0_monitor_mode_t mode) |
| Sets the PLL0 monitor mode. More... | |
| void | CLOCK_SetPll1MonitorMode (scg_pll1_monitor_mode_t mode) |
| Sets the PLL1 monitor mode. More... | |
| void | VBAT_SetOscConfig (VBAT_Type *base, const vbat_osc_config_t *config) |
| Config 32k Crystal Oscillator. More... | |
| status_t | CLOCK_SetFLASHAccessCyclesForFreq (uint32_t system_freq_hz, run_mode_t mode) |
| Set the additional number of wait-states added to account for the ratio of system clock period to flash access time during full speed power mode. More... | |
| void | CLOCK_AttachClk (clock_attach_id_t connection) |
| Configure the clock selection muxes. More... | |
| clock_attach_id_t | CLOCK_GetClockAttachId (clock_attach_id_t attachId) |
| Get the actual clock attach id. This fuction uses the offset in input attach id, then it reads the actual source value in the register and combine the offset to obtain an actual attach id. More... | |
| void | CLOCK_SetClkDiv (clock_div_name_t div_name, uint32_t divided_by_value) |
| Setup peripheral clock dividers. More... | |
| uint32_t | CLOCK_GetClkDiv (clock_div_name_t div_name) |
| Get peripheral clock dividers. More... | |
| void | CLOCK_HaltClkDiv (clock_div_name_t div_name) |
| Halt peripheral clock dividers. More... | |
| void | CLOCK_SetupClockCtrl (uint32_t mask) |
| system clocks enable controls. More... | |
| uint32_t | CLOCK_GetFreq (clock_name_t clockName) |
| Return Frequency of selected clock. More... | |
| uint32_t | CLOCK_GetMainClkFreq (void) |
| Return Frequency of main. More... | |
| uint32_t | CLOCK_GetCoreSysClkFreq (void) |
| Return Frequency of core. More... | |
| uint32_t | CLOCK_GetCTimerClkFreq (uint32_t id) |
| Return Frequency of CTimer functional Clock. More... | |
| uint32_t | CLOCK_GetAdcClkFreq (uint32_t id) |
| Return Frequency of Adc Clock. More... | |
| uint32_t | CLOCK_GetUsb0ClkFreq (void) |
| Return Frequency of Usb Clock. More... | |
| uint32_t | CLOCK_GetLPFlexCommClkFreq (uint32_t id) |
| Return Frequency of LPFlexComm Clock. More... | |
| uint32_t | CLOCK_GetSctClkFreq (void) |
| Return Frequency of SCTimer Clock. More... | |
| uint32_t | CLOCK_GetTsiClkFreq (void) |
| Return Frequency of TSI Clock. More... | |
| uint32_t | CLOCK_GetSincFilterClkFreq (void) |
| Return Frequency of SINC FILTER Clock. More... | |
| uint32_t | CLOCK_GetDacClkFreq (uint32_t id) |
| Return Frequency of DAC Clock. More... | |
| uint32_t | CLOCK_GetFlexspiClkFreq (void) |
| Return Frequency of FlexSPI. More... | |
| uint32_t | CLOCK_GetPll0OutFreq (void) |
| Return Frequency of PLL. More... | |
| uint32_t | CLOCK_GetPll1OutFreq (void) |
| Return Frequency of USB PLL. More... | |
| uint32_t | CLOCK_GetPllClkDivFreq (void) |
| Return Frequency of PLLCLKDIV. More... | |
| uint32_t | CLOCK_GetI3cClkFreq (uint32_t id) |
| Return Frequency of I3C function Clock. More... | |
| uint32_t | CLOCK_GetI3cSTCClkFreq (uint32_t id) |
| Return Frequency of I3C function slow TC Clock. More... | |
| uint32_t | CLOCK_GetI3cSClkFreq (uint32_t id) |
| Return Frequency of I3C function slow Clock. More... | |
| uint32_t | CLOCK_GetMicfilClkFreq (void) |
| Return Frequency of MICFIL Clock. More... | |
| uint32_t | CLOCK_GetUsdhcClkFreq (void) |
| Return Frequency of uSDHC. More... | |
| uint32_t | CLOCK_GetFlexioClkFreq (void) |
| Return Frequency of FLEXIO. More... | |
| uint32_t | CLOCK_GetFlexcanClkFreq (uint32_t id) |
| Return Frequency of FLEXCAN. More... | |
| uint32_t | CLOCK_GetEnetRmiiClkFreq (void) |
| Return Frequency of Ethernet RMII Clock. More... | |
| uint32_t | CLOCK_GetEnetPtpRefClkFreq (void) |
| Return Frequency of Ethernet PTP REF Clock. More... | |
| void | CLOCK_SetupEnetTxClk (uint32_t iFreq) |
| Initialize the ENET TX CLK to given frequency. More... | |
| uint32_t | CLOCK_GetEnetTxClkFreq (void) |
| Return Frequency of ENET TX CLK. More... | |
| uint32_t | CLOCK_GetEwm0ClkFreq (void) |
| Return Frequency of EWM0 Clock. More... | |
| uint32_t | CLOCK_GetWdtClkFreq (uint32_t id) |
| Return Frequency of Watchdog. More... | |
| uint32_t | CLOCK_GetOstimerClkFreq (void) |
| Return Frequency of OSTIMER. More... | |
| uint32_t | CLOCK_GetCmpFClkFreq (uint32_t id) |
| Return Frequency of CMP Function Clock. More... | |
| uint32_t | CLOCK_GetCmpRRClkFreq (uint32_t id) |
| Return Frequency of CMP Round Robin Clock. More... | |
| uint32_t | CLOCK_GetSaiClkFreq (uint32_t id) |
| Return Frequency of SAI Clock. More... | |
| void | CLOCK_SetupSaiMclk (uint32_t id, uint32_t iFreq) |
| Initialize the SAI MCLK to given frequency. More... | |
| void | CLOCK_SetupSaiTxBclk (uint32_t id, uint32_t iFreq) |
| Initialize the SAI TX BCLK to given frequency. More... | |
| void | CLOCK_SetupSaiRxBclk (uint32_t id, uint32_t iFreq) |
| Initialize the SAI RX BCLK to given frequency. More... | |
| uint32_t | CLOCK_GetSaiMclkFreq (uint32_t id) |
| Return Frequency of SAI MCLK. More... | |
| uint32_t | CLOCK_GetSaiTxBclkFreq (uint32_t id) |
| Return Frequency of SAI TX BCLK. More... | |
| uint32_t | CLOCK_GetSaiRxBclkFreq (uint32_t id) |
| Return Frequency of SAI RX BCLK. More... | |
| uint32_t | CLOCK_GetEmvsimClkFreq (uint32_t id) |
| Return Frequency of EMVSIM Clock. More... | |
| uint32_t | CLOCK_GetPLL0InClockRate (void) |
| Return PLL0 input clock rate. More... | |
| uint32_t | CLOCK_GetPLL1InClockRate (void) |
| Return PLL1 input clock rate. More... | |
| uint32_t | CLOCK_GetExtUpllFreq (void) |
| Gets the external UPLL frequency. More... | |
| void | CLOCK_SetExtUpllFreq (uint32_t freq) |
| Sets the external UPLL frequency. More... | |
| __STATIC_INLINE bool | CLOCK_IsPLL0Locked (void) |
| Check if PLL is locked or not. More... | |
| __STATIC_INLINE bool | CLOCK_IsPLL1Locked (void) |
| Check if PLL1 is locked or not. More... | |
| uint32_t | CLOCK_GetPLLOutFromSetup (pll_setup_t *pSetup) |
| Return PLL0 output clock rate from setup structure. More... | |
| pll_error_t | CLOCK_SetupPLLData (pll_config_t *pControl, pll_setup_t *pSetup) |
| Set PLL output based on the passed PLL setup data. More... | |
| pll_error_t | CLOCK_SetPLL0Freq (const pll_setup_t *pSetup) |
| Set PLL output from PLL setup structure (precise frequency) More... | |
| pll_error_t | CLOCK_SetPLL1Freq (const pll_setup_t *pSetup) |
| Set PLL output from PLL setup structure (precise frequency) More... | |
| void | CLOCK_EnableOstimer32kClock (void) |
| Enable the OSTIMER 32k clock. More... | |
| bool | CLOCK_EnableUsbfsClock (void) |
| brief Enable USB FS clock. More... | |
| bool | CLOCK_EnableUsbhsPhyPllClock (clock_usb_phy_src_t src, uint32_t freq) |
| brief Enable USB HS PHY PLL clock. More... | |
| void | CLOCK_DisableUsbhsPhyPllClock (void) |
| brief Disable USB HS PHY PLL clock. More... | |
| bool | CLOCK_EnableUsbhsClock (void) |
| brief Enable USB HS clock. More... | |
| status_t | CLOCK_FIRCAutoTrimWithSOF (void) |
| FIRC Auto Trim With SOF. More... | |
Driver version | |
| #define | FSL_CLOCK_DRIVER_VERSION (MAKE_VERSION(1, 0, 1)) |
| CLOCK driver version 1.0.1. More... | |
| struct firc_trim_config_t |
Data Fields | |
| firc_trim_mode_t | trimMode |
| Trim mode. More... | |
| firc_trim_src_t | trimSrc |
| Trim source. More... | |
| uint16_t | trimDiv |
| Divider of SOSC. More... | |
| uint8_t | trimCoar |
| Trim coarse value; Irrelevant if trimMode is kSCG_TrimUpdate. More... | |
| uint8_t | trimFine |
| Trim fine value; Irrelevant if trimMode is kSCG_TrimUpdate. More... | |
| firc_trim_mode_t firc_trim_config_t::trimMode |
| firc_trim_src_t firc_trim_config_t::trimSrc |
| uint16_t firc_trim_config_t::trimDiv |
| uint8_t firc_trim_config_t::trimCoar |
| uint8_t firc_trim_config_t::trimFine |
| struct sirc_trim_config_t |
Data Fields | |
| sirc_trim_mode_t | trimMode |
| Trim mode. More... | |
| sirc_trim_src_t | trimSrc |
| Trim source. More... | |
| uint16_t | trimDiv |
| Divider of SOSC. More... | |
| uint8_t | cltrim |
| Trim coarse value; Irrelevant if trimMode is kSCG_TrimUpdate. More... | |
| uint8_t | ccotrim |
| Trim fine value; Irrelevant if trimMode is kSCG_TrimUpdate. More... | |
| sirc_trim_mode_t sirc_trim_config_t::trimMode |
| sirc_trim_src_t sirc_trim_config_t::trimSrc |
| uint16_t sirc_trim_config_t::trimDiv |
| uint8_t sirc_trim_config_t::cltrim |
| uint8_t sirc_trim_config_t::ccotrim |
| struct vbat_osc_config_t |
Data Fields | |
| bool | enableInternalCapBank |
| enable/disable the internal capacitance bank. More... | |
| bool | enableCrystalOscillatorBypass |
| enable/disable the crystal oscillator bypass. More... | |
| vbat_osc_xtal_cap_t | xtalCap |
| The internal capacitance for the OSC XTAL pin from the capacitor bank, only useful when the internal capacitance bank is enabled. More... | |
| vbat_osc_extal_cap_t | extalCap |
| The internal capacitance for the OSC EXTAL pin from the capacitor bank, only useful when the internal capacitance bank is enabled. More... | |
| vbat_osc_coarse_adjustment_value_t | coarseAdjustment |
| 32kHz crystal oscillator amplifier coarse adjustment value. More... | |
| bool vbat_osc_config_t::enableInternalCapBank |
| bool vbat_osc_config_t::enableCrystalOscillatorBypass |
| vbat_osc_xtal_cap_t vbat_osc_config_t::xtalCap |
| vbat_osc_extal_cap_t vbat_osc_config_t::extalCap |
| vbat_osc_coarse_adjustment_value_t vbat_osc_config_t::coarseAdjustment |
| struct pll_config_t |
This structure can be used to configure the settings for a PLL setup structure. Fill in the desired configuration for the PLL and call the PLL setup function to fill in a PLL setup structure.
Data Fields | |
| uint32_t | desiredRate |
| Desired PLL rate in Hz. | |
| uint32_t | inputSource |
| PLL input source. | |
| uint32_t | flags |
| PLL configuration flags, Or'ed value of PLL_CONFIGFLAG_* definitions. | |
| ss_progmodfm_t | ss_mf |
| SS Programmable modulation frequency, only applicable when not using PLL_CONFIGFLAG_FORCENOFRACT flag. | |
| ss_progmoddp_t | ss_mr |
| SS Programmable frequency modulation depth, only applicable when not using PLL_CONFIGFLAG_FORCENOFRACT flag. | |
| ss_modwvctrl_t | ss_mc |
| SS Modulation waveform control, only applicable when not using PLL_CONFIGFLAG_FORCENOFRACT flag. | |
| bool | mfDither |
| false for fixed modulation frequency or true for dithering, only applicable when not using PLL_CONFIGFLAG_FORCENOFRACT flag | |
| struct pll_setup_t |
It can be populated with the PLL setup function. If powering up or waiting for PLL lock, the PLL input clock source should be configured prior to PLL setup.
Data Fields | |
| uint32_t | pllctrl |
| PLL Control register APLLCTRL. | |
| uint32_t | pllndiv |
| PLL N Divider register APLLNDIV. | |
| uint32_t | pllpdiv |
| PLL P Divider register APLLPDIV. | |
| uint32_t | pllmdiv |
| PLL M Divider register APLLMDIV. | |
| uint32_t | pllsscg [2] |
| PLL Spread Spectrum Control registers APLLSSCG. | |
| uint32_t | pllRate |
| Acutal PLL rate. | |
| #define FSL_CLOCK_DRIVER_VERSION (MAKE_VERSION(1, 0, 1)) |
| #define FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL 0 |
When set to 0, peripheral drivers will enable clock in initialize function and disable clock in de-initialize function. When set to 1, peripheral driver will not control the clock, application could control the clock out of the driver.
| #define CLOCK_USR_CFG_PLL_CONFIG_CACHE_COUNT 2U |
Once define this MACRO to be non-zero value, CLOCK_PllGetConfig() function would cache the recent calulation and accelerate the execution to get the right settings.
| #define ROM_CLOCKS |
| #define SRAM_CLOCKS |
| #define FMC_CLOCKS |
| #define INPUTMUX_CLOCKS |
| #define ETH_CLOCKS |
| #define GPIO_CLOCKS |
| #define PINT_CLOCKS |
| #define DMA_CLOCKS |
| #define EDMA_CLOCKS |
| #define CRC_CLOCKS |
| #define WWDT_CLOCKS |
| #define MAILBOX_CLOCKS |
| #define LPADC_CLOCKS |
| #define MRT_CLOCKS |
| #define OSTIMER_CLOCKS |
| #define SCT_CLOCKS |
| #define UTICK_CLOCKS |
| #define LP_FLEXCOMM_CLOCKS |
| #define LPUART_CLOCKS |
| #define LPI2C_CLOCKS |
| #define LPSPI_CLOCKS |
| #define CTIMER_CLOCKS |
| #define FREQME_CLOCKS |
| #define POWERQUAD_CLOCKS |
| #define PLU_CLOCKS |
| #define PUF_CLOCKS |
| #define VREF_CLOCKS |
| #define LPDAC_CLOCKS |
| #define HPDAC_CLOCKS |
| #define PWM_CLOCKS |
| #define QDC_CLOCKS |
| #define FLEXIO_CLOCKS |
| #define FLEXCAN_CLOCKS |
| #define EMVSIM_CLOCKS |
| #define USDHC_CLOCKS |
| #define SAI_CLOCKS |
| #define RTC_CLOCKS |
| #define PDM_CLOCKS |
| #define ERM_CLOCKS |
| #define EIM_CLOCKS |
| #define OPAMP_CLOCKS |
| #define TSI_CLOCKS |
| #define TRNG_CLOCKS |
| #define LPCMP_CLOCKS |
| #define CLK_GATE_REG_OFFSET_SHIFT 8U |
| #define BUS_CLK kCLOCK_BusClk |
| #define CLK_ATTACH_ID | ( | mux, | |
| sel, | |||
| pos | |||
| ) | ((((uint32_t)(mux) << 0U) | (((uint32_t)(sel) + 1U) & 0xFU) << 12U) << ((uint32_t)(pos)*16U)) |
[4 bits for choice, 0 means invalid choice] [8 bits mux ID]*
| #define PLL_CONFIGFLAG_FORCENOFRACT (1U << 2U) |
When the PLL_CONFIGFLAG_FORCENOFRACT flag is selected, the PLL hardware for the automatic bandwidth selection, Spread Spectrum (SS) support, and fractional M-divider are not used.
Force non-fractional output mode, PLL output will not use the fractional, automatic bandwidth, or SS hardware
| enum clock_ip_name_t |
| enum clock_name_t |
| enum clock_attach_id_t |
| enum clock_div_name_t |
| enum osc32k_clk_gate_id_t |
| enum clk16k_clk_gate_id_t |
| enum clock_ctrl_enable_t |
| enum clock_usb_phy_src_t |
| enum _scg_status |
| enum firc_trim_mode_t |
| enum firc_trim_src_t |
| enum sirc_trim_mode_t |
| enum sirc_trim_src_t |
| enum vbat_osc_xtal_cap_t |
| enum vbat_osc_extal_cap_t |
Changes the oscillator amplitude by modifying the automatic gain control (AGC).
| enum run_mode_t |
| enum pll_clk_src_t |
| enum ss_progmodfm_t |
| enum ss_progmoddp_t |
| enum ss_modwvctrl_t |
| enum pll_error_t |
|
inlinestatic |
| clk | : Clock to be enabled. |
|
inlinestatic |
| clk | : Clock to be Disabled. |
| status_t CLOCK_SetupFROHFClocking | ( | uint32_t | iFreq | ) |
| iFreq | : Desired frequency (must be one of CLK_FRO_44MHZ or CLK_FRO_144MHZ) |
| status_t CLOCK_SetupExtClocking | ( | uint32_t | iFreq | ) |
| iFreq | : Desired frequency (must be equal to exact rate in Hz) |
| status_t CLOCK_SetupExtRefClocking | ( | uint32_t | iFreq | ) |
| iFreq | : Desired frequency (must be equal to exact rate in Hz) |
| status_t CLOCK_SetupOsc32KClocking | ( | uint32_t | id | ) |
| id | : OSC 32 kHz output clock to specified modules, it should use osc32k_clk_gate_id_t value |
| status_t CLOCK_SetupClk16KClocking | ( | uint32_t | id | ) |
| id | : FRO 16 kHz output clock to specified modules, it should use clk16k_clk_gate_id_t value |
| status_t CLOCK_FROHFTrimConfig | ( | firc_trim_config_t | config | ) |
| config | : FROHF trim value |
| status_t CLOCK_FRO12MTrimConfig | ( | sirc_trim_config_t | config | ) |
| config | : FRO 12M trim value |
| void CLOCK_SetSysOscMonitorMode | ( | scg_sosc_monitor_mode_t | mode | ) |
This function sets the system OSC monitor mode. The mode can be disabled, it can generate an interrupt when the error is disabled, or reset when the error is detected.
| mode | Monitor mode to set. |
| void CLOCK_SetRoscMonitorMode | ( | scg_rosc_monitor_mode_t | mode | ) |
This function sets the ROSC monitor mode. The mode can be disabled, it can generate an interrupt when the error is disabled, or reset when the error is detected.
| mode | Monitor mode to set. |
| void CLOCK_SetUpllMonitorMode | ( | scg_upll_monitor_mode_t | mode | ) |
This function sets the UPLL monitor mode. The mode can be disabled, it can generate an interrupt when the error is disabled, or reset when the error is detected.
| mode | Monitor mode to set. |
| void CLOCK_SetPll0MonitorMode | ( | scg_pll0_monitor_mode_t | mode | ) |
This function sets the PLL0 monitor mode. The mode can be disabled, it can generate an interrupt when the error is disabled, or reset when the error is detected.
| mode | Monitor mode to set. |
| void CLOCK_SetPll1MonitorMode | ( | scg_pll1_monitor_mode_t | mode | ) |
This function sets the PLL1 monitor mode. The mode can be disabled, it can generate an interrupt when the error is disabled, or reset when the error is detected.
| mode | Monitor mode to set. |
| void VBAT_SetOscConfig | ( | VBAT_Type * | base, |
| const vbat_osc_config_t * | config | ||
| ) |
| base | VBAT peripheral base address. |
| config | The pointer to the structure vbat_osc_config_t. |
| status_t CLOCK_SetFLASHAccessCyclesForFreq | ( | uint32_t | system_freq_hz, |
| run_mode_t | mode | ||
| ) |
| system_freq_hz | : Input frequency |
| mode | : Active run mode (voltage level). |
| void CLOCK_AttachClk | ( | clock_attach_id_t | connection | ) |
| connection | : Clock to be configured. |
| clock_attach_id_t CLOCK_GetClockAttachId | ( | clock_attach_id_t | attachId | ) |
| attachId | : Clock attach id to get. |
| void CLOCK_SetClkDiv | ( | clock_div_name_t | div_name, |
| uint32_t | divided_by_value | ||
| ) |
| div_name | : Clock divider name |
| divided_by_value,: | Value to be divided |
| uint32_t CLOCK_GetClkDiv | ( | clock_div_name_t | div_name | ) |
| div_name | : Clock divider name |
| void CLOCK_HaltClkDiv | ( | clock_div_name_t | div_name | ) |
| div_name | : Clock divider name |
| void CLOCK_SetupClockCtrl | ( | uint32_t | mask | ) |
| mask | : system clocks enable value, it should use clock_ctrl_enable_t value |
| uint32_t CLOCK_GetFreq | ( | clock_name_t | clockName | ) |
| uint32_t CLOCK_GetMainClkFreq | ( | void | ) |
| uint32_t CLOCK_GetCoreSysClkFreq | ( | void | ) |
| uint32_t CLOCK_GetCTimerClkFreq | ( | uint32_t | id | ) |
| uint32_t CLOCK_GetAdcClkFreq | ( | uint32_t | id | ) |
| uint32_t CLOCK_GetUsb0ClkFreq | ( | void | ) |
| uint32_t CLOCK_GetLPFlexCommClkFreq | ( | uint32_t | id | ) |
| uint32_t CLOCK_GetSctClkFreq | ( | void | ) |
| uint32_t CLOCK_GetTsiClkFreq | ( | void | ) |
| uint32_t CLOCK_GetSincFilterClkFreq | ( | void | ) |
| uint32_t CLOCK_GetDacClkFreq | ( | uint32_t | id | ) |
| uint32_t CLOCK_GetFlexspiClkFreq | ( | void | ) |
| uint32_t CLOCK_GetPll0OutFreq | ( | void | ) |
| uint32_t CLOCK_GetPll1OutFreq | ( | void | ) |
| uint32_t CLOCK_GetPllClkDivFreq | ( | void | ) |
| uint32_t CLOCK_GetI3cClkFreq | ( | uint32_t | id | ) |
| uint32_t CLOCK_GetI3cSTCClkFreq | ( | uint32_t | id | ) |
| uint32_t CLOCK_GetI3cSClkFreq | ( | uint32_t | id | ) |
| uint32_t CLOCK_GetMicfilClkFreq | ( | void | ) |
| uint32_t CLOCK_GetUsdhcClkFreq | ( | void | ) |
| uint32_t CLOCK_GetFlexioClkFreq | ( | void | ) |
| uint32_t CLOCK_GetFlexcanClkFreq | ( | uint32_t | id | ) |
| uint32_t CLOCK_GetEnetRmiiClkFreq | ( | void | ) |
| uint32_t CLOCK_GetEnetPtpRefClkFreq | ( | void | ) |
| void CLOCK_SetupEnetTxClk | ( | uint32_t | iFreq | ) |
| iFreq | : Desired frequency |
| uint32_t CLOCK_GetEnetTxClkFreq | ( | void | ) |
| uint32_t CLOCK_GetEwm0ClkFreq | ( | void | ) |
| uint32_t CLOCK_GetWdtClkFreq | ( | uint32_t | id | ) |
| uint32_t CLOCK_GetOstimerClkFreq | ( | void | ) |
| uint32_t CLOCK_GetCmpFClkFreq | ( | uint32_t | id | ) |
| uint32_t CLOCK_GetCmpRRClkFreq | ( | uint32_t | id | ) |
| uint32_t CLOCK_GetSaiClkFreq | ( | uint32_t | id | ) |
| void CLOCK_SetupSaiMclk | ( | uint32_t | id, |
| uint32_t | iFreq | ||
| ) |
| iFreq | : Desired frequency |
| void CLOCK_SetupSaiTxBclk | ( | uint32_t | id, |
| uint32_t | iFreq | ||
| ) |
| iFreq | : Desired frequency |
| void CLOCK_SetupSaiRxBclk | ( | uint32_t | id, |
| uint32_t | iFreq | ||
| ) |
| iFreq | : Desired frequency |
| uint32_t CLOCK_GetSaiMclkFreq | ( | uint32_t | id | ) |
| uint32_t CLOCK_GetSaiTxBclkFreq | ( | uint32_t | id | ) |
| uint32_t CLOCK_GetSaiRxBclkFreq | ( | uint32_t | id | ) |
| uint32_t CLOCK_GetEmvsimClkFreq | ( | uint32_t | id | ) |
| uint32_t CLOCK_GetPLL0InClockRate | ( | void | ) |
| uint32_t CLOCK_GetPLL1InClockRate | ( | void | ) |
| uint32_t CLOCK_GetExtUpllFreq | ( | void | ) |
| void CLOCK_SetExtUpllFreq | ( | uint32_t | freq | ) |
| The | frequency of external UPLL. |
| __STATIC_INLINE bool CLOCK_IsPLL0Locked | ( | void | ) |
| __STATIC_INLINE bool CLOCK_IsPLL1Locked | ( | void | ) |
| uint32_t CLOCK_GetPLLOutFromSetup | ( | pll_setup_t * | pSetup | ) |
| pSetup | : Pointer to a PLL setup structure |
| pll_error_t CLOCK_SetupPLLData | ( | pll_config_t * | pControl, |
| pll_setup_t * | pSetup | ||
| ) |
| pControl | : Pointer to populated PLL control structure to generate setup with |
| pSetup | : Pointer to PLL setup structure to be filled |
| pll_error_t CLOCK_SetPLL0Freq | ( | const pll_setup_t * | pSetup | ) |
| pSetup | : Pointer to populated PLL setup structure |
| pll_error_t CLOCK_SetPLL1Freq | ( | const pll_setup_t * | pSetup | ) |
| pSetup | : Pointer to populated PLL setup structure |
| void CLOCK_EnableOstimer32kClock | ( | void | ) |
| bool CLOCK_EnableUsbfsClock | ( | void | ) |
Enable USB Full Speed clock.
| bool CLOCK_EnableUsbhsPhyPllClock | ( | clock_usb_phy_src_t | src, |
| uint32_t | freq | ||
| ) |
This function enables the internal 480MHz USB PHY PLL clock.
param src USB HS PHY PLL clock source. param freq The frequency specified by src. retval true The clock is set successfully. retval false The clock source is invalid to get proper USB HS clock.
| void CLOCK_DisableUsbhsPhyPllClock | ( | void | ) |
This function disables USB HS PHY PLL clock.
| bool CLOCK_EnableUsbhsClock | ( | void | ) |
retval true The clock is set successfully. retval false The clock source is invalid to get proper USB HS clock.
| status_t CLOCK_FIRCAutoTrimWithSOF | ( | void | ) |