![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev 2.16.000
    
   NXP Semiconductors 
   | 
 
Data Structures | |
| struct | i2c_master_dma_handle_t | 
| I2C master dma transfer structure.  More... | |
Macros | |
| #define | I2C_MAX_DMA_TRANSFER_COUNT 1024 | 
| Maximum lenght of single DMA transfer (determined by capability of the DMA engine)  | |
Typedefs | |
| typedef void(* | i2c_master_dma_transfer_callback_t )(I2C_Type *base, i2c_master_dma_handle_t *handle, status_t status, void *userData) | 
| I2C master dma transfer callback typedef.  More... | |
| typedef void(* | flexcomm_i2c_dma_master_irq_handler_t )(I2C_Type *base, i2c_master_dma_handle_t *handle) | 
| Typedef for master dma handler.  More... | |
Driver version | |
| #define | FSL_I2C_DMA_DRIVER_VERSION (MAKE_VERSION(2, 3, 1)) | 
| I2C DMA driver version.  More... | |
I2C Block DMA Transfer Operation | |
| void | I2C_MasterTransferCreateHandleDMA (I2C_Type *base, i2c_master_dma_handle_t *handle, i2c_master_dma_transfer_callback_t callback, void *userData, dma_handle_t *dmaHandle) | 
| Init the I2C handle which is used in transactional functions.  More... | |
| status_t | I2C_MasterTransferDMA (I2C_Type *base, i2c_master_dma_handle_t *handle, i2c_master_transfer_t *xfer) | 
| Performs a master dma non-blocking transfer on the I2C bus.  More... | |
| status_t | I2C_MasterTransferGetCountDMA (I2C_Type *base, i2c_master_dma_handle_t *handle, size_t *count) | 
| Get master transfer status during a dma non-blocking transfer.  More... | |
| void | I2C_MasterTransferAbortDMA (I2C_Type *base, i2c_master_dma_handle_t *handle) | 
| Abort a master dma non-blocking transfer in a early time.  More... | |
| struct _i2c_master_dma_handle | 
I2C master dma handle typedef.
Data Fields | |
| uint8_t | state | 
| Transfer state machine current state.  More... | |
| uint32_t | transferCount | 
| Indicates progress of the transfer.  | |
| uint32_t | remainingBytesDMA | 
| Remaining byte count to be transferred using DMA.  More... | |
| uint8_t * | buf | 
| Buffer pointer for current state.  More... | |
| bool | checkAddrNack | 
| Whether to check the nack signal is detected during addressing.  More... | |
| dma_handle_t * | dmaHandle | 
| The DMA handler used.  More... | |
| i2c_master_transfer_t | transfer | 
| Copy of the current transfer info.  More... | |
| i2c_master_dma_transfer_callback_t | completionCallback | 
| Callback function called after dma transfer finished.  More... | |
| void * | userData | 
| Callback parameter passed to callback function.  More... | |
| uint8_t i2c_master_dma_handle_t::state | 
| uint32_t i2c_master_dma_handle_t::remainingBytesDMA | 
| uint8_t* i2c_master_dma_handle_t::buf | 
| bool i2c_master_dma_handle_t::checkAddrNack | 
| dma_handle_t* i2c_master_dma_handle_t::dmaHandle | 
| i2c_master_transfer_t i2c_master_dma_handle_t::transfer | 
| i2c_master_dma_transfer_callback_t i2c_master_dma_handle_t::completionCallback | 
| void* i2c_master_dma_handle_t::userData | 
| #define FSL_I2C_DMA_DRIVER_VERSION (MAKE_VERSION(2, 3, 1)) | 
| typedef void(* i2c_master_dma_transfer_callback_t)(I2C_Type *base, i2c_master_dma_handle_t *handle, status_t status, void *userData) | 
| typedef void(* flexcomm_i2c_dma_master_irq_handler_t)(I2C_Type *base, i2c_master_dma_handle_t *handle) | 
| void I2C_MasterTransferCreateHandleDMA | ( | I2C_Type * | base, | 
| i2c_master_dma_handle_t * | handle, | ||
| i2c_master_dma_transfer_callback_t | callback, | ||
| void * | userData, | ||
| dma_handle_t * | dmaHandle | ||
| ) | 
| base | I2C peripheral base address | 
| handle | pointer to i2c_master_dma_handle_t structure | 
| callback | pointer to user callback function | 
| userData | user param passed to the callback function | 
| dmaHandle | DMA handle pointer | 
| status_t I2C_MasterTransferDMA | ( | I2C_Type * | base, | 
| i2c_master_dma_handle_t * | handle, | ||
| i2c_master_transfer_t * | xfer | ||
| ) | 
| base | I2C peripheral base address | 
| handle | pointer to i2c_master_dma_handle_t structure | 
| xfer | pointer to transfer structure of i2c_master_transfer_t | 
| kStatus_Success | Sucessully complete the data transmission. | 
| kStatus_I2C_Busy | Previous transmission still not finished. | 
| kStatus_I2C_Timeout | Transfer error, wait signal timeout. | 
| kStatus_I2C_ArbitrationLost | Transfer error, arbitration lost. | 
| kStataus_I2C_Nak | Transfer error, receive Nak during transfer. | 
| status_t I2C_MasterTransferGetCountDMA | ( | I2C_Type * | base, | 
| i2c_master_dma_handle_t * | handle, | ||
| size_t * | count | ||
| ) | 
| base | I2C peripheral base address | 
| handle | pointer to i2c_master_dma_handle_t structure | 
| count | Number of bytes transferred so far by the non-blocking transaction. | 
| void I2C_MasterTransferAbortDMA | ( | I2C_Type * | base, | 
| i2c_master_dma_handle_t * | handle | ||
| ) | 
| base | I2C peripheral base address | 
| handle | pointer to i2c_master_dma_handle_t structure |