MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

The MMCCARD driver provide card initialization/read/write/erase interface.

MMC CARD Operation

error log support

Not support yet

User configuable

Board dependency

Typical use case

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/sdmmc_examples/

Data Structures

struct  mmc_usr_param_t
 card user parameter More...
 
struct  mmc_card_t
 mmc card state More...
 

Macros

#define FSL_MMC_DRIVER_VERSION   (MAKE_VERSION(2U, 4U, 1U)) /*2.4.1*/
 Middleware mmc version. More...
 

Typedefs

typedef void(* mmc_io_strength_t )(uint32_t busFreq)
 card io strength control
 

Enumerations

enum  {
  kMMC_SupportHighSpeed26MHZFlag = (1U << 0U),
  kMMC_SupportHighSpeed52MHZFlag = (1U << 1U),
  kMMC_SupportHighSpeedDDR52MHZ180V300VFlag = (1 << 2U),
  kMMC_SupportHighSpeedDDR52MHZ120VFlag = (1 << 3U),
  kMMC_SupportHS200200MHZ180VFlag = (1 << 4U),
  kMMC_SupportHS200200MHZ120VFlag = (1 << 5U),
  kMMC_SupportHS400DDR200MHZ180VFlag = (1 << 6U),
  kMMC_SupportHS400DDR200MHZ120VFlag = (1 << 7U),
  kMMC_SupportHighCapacityFlag = (1U << 8U),
  kMMC_SupportAlternateBootFlag = (1U << 9U),
  kMMC_SupportDDRBootFlag = (1U << 10U),
  kMMC_SupportHighSpeedBootFlag = (1U << 11U),
  kMMC_SupportEnhanceHS400StrobeFlag = (1U << 12U)
}
 MMC card flags. More...
 

MMCCARD Function

status_t MMC_Init (mmc_card_t *card)
 Initializes the MMC card and host. More...
 
void MMC_Deinit (mmc_card_t *card)
 Deinitializes the card and host. More...
 
status_t MMC_CardInit (mmc_card_t *card)
 intialize the card. More...
 
void MMC_CardDeinit (mmc_card_t *card)
 Deinitializes the card. More...
 
status_t MMC_HostInit (mmc_card_t *card)
 initialize the host. More...
 
void MMC_HostDeinit (mmc_card_t *card)
 Deinitializes the host. More...
 
void MMC_HostReset (SDMMCHOST_CONFIG *host)
 reset the host. More...
 
void MMC_PowerOnCard (SDMMCHOST_TYPE *base, const sdmmchost_pwr_card_t *pwr)
 power on card. More...
 
void MMC_PowerOffCard (SDMMCHOST_TYPE *base, const sdmmchost_pwr_card_t *pwr)
 power off card. More...
 
void MMC_SetCardPower (mmc_card_t *card, bool enable)
 set card power. More...
 
bool MMC_CheckReadOnly (mmc_card_t *card)
 Checks if the card is read-only. More...
 
status_t MMC_ReadBlocks (mmc_card_t *card, uint8_t *buffer, uint32_t startBlock, uint32_t blockCount)
 Reads data blocks from the card. More...
 
status_t MMC_WriteBlocks (mmc_card_t *card, const uint8_t *buffer, uint32_t startBlock, uint32_t blockCount)
 Writes data blocks to the card. More...
 
status_t MMC_EraseGroups (mmc_card_t *card, uint32_t startGroup, uint32_t endGroup)
 Erases groups of the card. More...
 
status_t MMC_SelectPartition (mmc_card_t *card, mmc_access_partition_t partitionNumber)
 Selects the partition to access. More...
 
status_t MMC_SetBootConfig (mmc_card_t *card, const mmc_boot_config_t *config)
 Configures the boot activity of the card. More...
 
status_t MMC_StartBoot (mmc_card_t *card, const mmc_boot_config_t *mmcConfig, uint8_t *buffer, sdmmchost_boot_config_t *hostConfig)
 MMC card start boot. More...
 
status_t MMC_SetBootConfigWP (mmc_card_t *card, uint8_t wp)
 MMC card set boot configuration write protect. More...
 
status_t MMC_ReadBootData (mmc_card_t *card, uint8_t *buffer, sdmmchost_boot_config_t *hostConfig)
 MMC card continous read boot data. More...
 
status_t MMC_StopBoot (mmc_card_t *card, uint32_t bootMode)
 MMC card stop boot mode. More...
 
status_t MMC_SetBootPartitionWP (mmc_card_t *card, mmc_boot_partition_wp_t bootPartitionWP)
 MMC card set boot partition write protect. More...
 
status_t MMC_EnableCacheControl (mmc_card_t *card, bool enable)
 MMC card cache control function. More...
 
status_t MMC_FlushCache (mmc_card_t *card)
 MMC card cache flush function. More...
 

Data Structure Documentation

struct mmc_usr_param_t

Data Fields

mmc_io_strength_t ioStrength
 swicth sd io strength
 
uint32_t maxFreq
 board support maximum frequency
 
uint32_t capability
 board capability flag
 
struct mmc_card_t

Define the card structure including the necessary fields to identify and describe the card.

Data Fields

sdmmchost_t * host
 Host information.
 
mmc_usr_param_t usrParam
 user parameter
 
bool isHostReady
 Use this flag to indicate if need host re-init or not.
 
bool noInteralAlign
 use this flag to disable sdmmc align. More...
 
uint32_t busClock_Hz
 MMC bus clock united in Hz.
 
uint32_t relativeAddress
 Relative address of the card.
 
bool enablePreDefinedBlockCount
 Enable PRE-DEFINED block count when read/write.
 
uint32_t flags
 Capability flag in _mmc_card_flag.
 
uint8_t internalBuffer [FSL_SDMMC_CARD_INTERNAL_BUFFER_SIZE]
 raw buffer used for mmc driver internal
 
uint32_t ocr
 Raw OCR content.
 
mmc_cid_t cid
 CID.
 
mmc_csd_t csd
 CSD.
 
mmc_extended_csd_t extendedCsd
 Extended CSD.
 
uint32_t blockSize
 Card block size.
 
uint32_t userPartitionBlocks
 Card total block number in user partition.
 
uint32_t bootPartitionBlocks
 Boot partition size united as block size.
 
uint32_t eraseGroupBlocks
 Erase group size united as block size.
 
mmc_access_partition_t currentPartition
 Current access partition.
 
mmc_voltage_window_t hostVoltageWindowVCCQ
 application must set this value according to board specific
 
mmc_voltage_window_t hostVoltageWindowVCC
 application must set this value according to board specific
 
mmc_high_speed_timing_t busTiming
 indicate the current work timing mode
 
mmc_data_bus_width_t busWidth
 indicate the current work bus width
 

Field Documentation

bool mmc_card_t::noInteralAlign

If disable, sdmmc will not make sure the data buffer address is word align, otherwise all the transfer are align to low level driver

Macro Definition Documentation

#define FSL_MMC_DRIVER_VERSION   (MAKE_VERSION(2U, 4U, 1U)) /*2.4.1*/

Enumeration Type Documentation

anonymous enum

Enumerator
kMMC_SupportHighSpeed26MHZFlag 

Support high speed 26MHZ.

kMMC_SupportHighSpeed52MHZFlag 

Support high speed 52MHZ.

kMMC_SupportHighSpeedDDR52MHZ180V300VFlag 

ddr 52MHZ 1.8V or 3.0V

kMMC_SupportHighSpeedDDR52MHZ120VFlag 

DDR 52MHZ 1.2V.

kMMC_SupportHS200200MHZ180VFlag 

HS200 ,200MHZ,1.8V.

kMMC_SupportHS200200MHZ120VFlag 

HS200, 200MHZ, 1.2V.

kMMC_SupportHS400DDR200MHZ180VFlag 

HS400, DDR, 200MHZ,1.8V.

kMMC_SupportHS400DDR200MHZ120VFlag 

HS400, DDR, 200MHZ,1.2V.

kMMC_SupportHighCapacityFlag 

Support high capacity.

kMMC_SupportAlternateBootFlag 

Support alternate boot.

kMMC_SupportDDRBootFlag 

support DDR boot flag

kMMC_SupportHighSpeedBootFlag 

support high speed boot flag

kMMC_SupportEnhanceHS400StrobeFlag 

support enhance HS400 strobe

Function Documentation

status_t MMC_Init ( mmc_card_t *  card)
Parameters
cardCard descriptor.
Return values
kStatus_SDMMC_HostNotReadyhost is not ready.
kStatus_SDMMC_GoIdleFailedGo idle failed.
kStatus_SDMMC_HandShakeOperationConditionFailedSend operation condition failed.
kStatus_SDMMC_AllSendCidFailedSend CID failed.
kStatus_SDMMC_SetRelativeAddressFailedSet relative address failed.
kStatus_SDMMC_SendCsdFailedSend CSD failed.
kStatus_SDMMC_CardNotSupportCard not support.
kStatus_SDMMC_SelectCardFailedSend SELECT_CARD command failed.
kStatus_SDMMC_SendExtendedCsdFailedSend EXT_CSD failed.
kStatus_SDMMC_SetDataBusWidthFailedSet bus width failed.
kStatus_SDMMC_SwitchBusTimingFailedSwitch high speed failed.
kStatus_SDMMC_SetCardBlockSizeFailedSet card block size failed.
kStatus_SDMMC_SetPowerClassFailset card power class failed.
kStatus_SuccessOperate successfully.
void MMC_Deinit ( mmc_card_t *  card)
Parameters
cardCard descriptor.
status_t MMC_CardInit ( mmc_card_t *  card)
Parameters
cardCard descriptor.
Return values
kStatus_SDMMC_HostNotReadyhost is not ready.
kStatus_SDMMC_GoIdleFailedGo idle failed.
kStatus_SDMMC_HandShakeOperationConditionFailedSend operation condition failed.
kStatus_SDMMC_AllSendCidFailedSend CID failed.
kStatus_SDMMC_SetRelativeAddressFailedSet relative address failed.
kStatus_SDMMC_SendCsdFailedSend CSD failed.
kStatus_SDMMC_CardNotSupportCard not support.
kStatus_SDMMC_SelectCardFailedSend SELECT_CARD command failed.
kStatus_SDMMC_SendExtendedCsdFailedSend EXT_CSD failed.
kStatus_SDMMC_SetDataBusWidthFailedSet bus width failed.
kStatus_SDMMC_SwitchBusTimingFailedSwitch high speed failed.
kStatus_SDMMC_SetCardBlockSizeFailedSet card block size failed.
kStatus_SDMMC_SetPowerClassFailset card power class failed.
kStatus_SuccessOperate successfully.
void MMC_CardDeinit ( mmc_card_t *  card)
Parameters
cardCard descriptor.
status_t MMC_HostInit ( mmc_card_t *  card)

This function deinitializes the specific host.

Parameters
cardCard descriptor.
void MMC_HostDeinit ( mmc_card_t *  card)

This function deinitializes the host.

Parameters
cardCard descriptor.
void MMC_HostReset ( SDMMCHOST_CONFIG *  host)

This function reset the specific host.

Parameters
hosthost descriptor.
void MMC_PowerOnCard ( SDMMCHOST_TYPE *  base,
const sdmmchost_pwr_card_t *  pwr 
)

The power on operation depend on host or the user define power on function.

Deprecated:
Do not use this function. It has been superceded by MMC_SetCardPower.
Parameters
basehost base address.
pwruser define power control configuration
void MMC_PowerOffCard ( SDMMCHOST_TYPE *  base,
const sdmmchost_pwr_card_t *  pwr 
)

The power off operation depend on host or the user define power on function.

Deprecated:
Do not use this function. It has been superceded by MMC_SetCardPower.
Parameters
basehost base address.
pwruser define power control configuration
void MMC_SetCardPower ( mmc_card_t *  card,
bool  enable 
)
Parameters
cardcard descriptor.
enabletrue is power on, false is power off.
bool MMC_CheckReadOnly ( mmc_card_t *  card)
Parameters
cardCard descriptor.
Return values
trueCard is read only.
falseCard isn't read only.
status_t MMC_ReadBlocks ( mmc_card_t *  card,
uint8_t *  buffer,
uint32_t  startBlock,
uint32_t  blockCount 
)
Parameters
cardCard descriptor.
bufferThe buffer to save data.
startBlockThe start block index.
blockCountThe number of blocks to read.
Return values
kStatus_InvalidArgumentInvalid argument.
kStatus_SDMMC_CardNotSupportCard not support.
kStatus_SDMMC_SetBlockCountFailedSet block count failed.
kStatus_SDMMC_TransferFailedTransfer failed.
kStatus_SDMMC_StopTransmissionFailedStop transmission failed.
kStatus_SuccessOperate successfully.
status_t MMC_WriteBlocks ( mmc_card_t *  card,
const uint8_t *  buffer,
uint32_t  startBlock,
uint32_t  blockCount 
)
Parameters
cardCard descriptor.
bufferThe buffer to save data blocks.
startBlockStart block number to write.
blockCountBlock count.
Return values
kStatus_InvalidArgumentInvalid argument.
kStatus_SDMMC_NotSupportYetNot support now.
kStatus_SDMMC_SetBlockCountFailedSet block count failed.
kStatus_SDMMC_WaitWriteCompleteFailedSend status failed.
kStatus_SDMMC_TransferFailedTransfer failed.
kStatus_SDMMC_StopTransmissionFailedStop transmission failed.
kStatus_SuccessOperate successfully.
status_t MMC_EraseGroups ( mmc_card_t *  card,
uint32_t  startGroup,
uint32_t  endGroup 
)

Erase group is the smallest erase unit in MMC card. The erase range is [startGroup, endGroup].

Parameters
cardCard descriptor.
startGroupStart group number.
endGroupEnd group number.
Return values
kStatus_InvalidArgumentInvalid argument.
kStatus_SDMMC_WaitWriteCompleteFailedSend status failed.
kStatus_SDMMC_TransferFailedTransfer failed.
kStatus_SuccessOperate successfully.
status_t MMC_SelectPartition ( mmc_card_t *  card,
mmc_access_partition_t  partitionNumber 
)
Parameters
cardCard descriptor.
partitionNumberThe partition number.
Return values
kStatus_SDMMC_ConfigureExtendedCsdFailedConfigure EXT_CSD failed.
kStatus_SuccessOperate successfully.
status_t MMC_SetBootConfig ( mmc_card_t *  card,
const mmc_boot_config_t *  config 
)
Parameters
cardCard descriptor.
configBoot configuration structure.
Return values
kStatus_SDMMC_NotSupportYetNot support now.
kStatus_SDMMC_ConfigureExtendedCsdFailedConfigure EXT_CSD failed.
kStatus_SDMMC_ConfigureBootFailedConfigure boot failed.
kStatus_SuccessOperate successfully.
status_t MMC_StartBoot ( mmc_card_t *  card,
const mmc_boot_config_t *  mmcConfig,
uint8_t *  buffer,
sdmmchost_boot_config_t *  hostConfig 
)
Parameters
cardCard descriptor.
mmcConfigmmc Boot configuration structure.
bufferaddress to recieve data.
hostConfighost boot configurations.
Return values
kStatus_Failfail.
kStatus_SDMMC_TransferFailedtransfer fail.
kStatus_SDMMC_GoIdleFailedreset card fail.
kStatus_SuccessOperate successfully.
status_t MMC_SetBootConfigWP ( mmc_card_t *  card,
uint8_t  wp 
)
Parameters
cardCard descriptor.
wpwrite protect value.
status_t MMC_ReadBootData ( mmc_card_t *  card,
uint8_t *  buffer,
sdmmchost_boot_config_t *  hostConfig 
)
Parameters
cardCard descriptor.
bufferbuffer address.
hostConfighost boot configurations.
status_t MMC_StopBoot ( mmc_card_t *  card,
uint32_t  bootMode 
)
Parameters
cardCard descriptor.
bootModeboot mode.
status_t MMC_SetBootPartitionWP ( mmc_card_t *  card,
mmc_boot_partition_wp_t  bootPartitionWP 
)
Parameters
cardCard descriptor.
bootPartitionWPboot partition write protect value.
status_t MMC_EnableCacheControl ( mmc_card_t *  card,
bool  enable 
)

The mmc device's cache is enabled by the driver by default. The cache should in typical case reduce the access time (compared to an access to the main nonvolatile storage) for both write and read.

Parameters
cardCard descriptor.
enabletrue is enable the cache, false is disable the cache.
status_t MMC_FlushCache ( mmc_card_t *  card)

A Flush operation refers to the requirement, from the host to the device, to write the cached data to the nonvolatile memory. Prior to a flush, the device may autonomously write data to the nonvolatile memory, but after the flush operation all data in the volatile area must be written to nonvolatile memory There is no requirement for flush due to switching between the partitions. (Note: This also implies that the cache data shall not be lost when switching between partitions). Cached data may be lost in SLEEP state, so host should flush the cache before placing the device into SLEEP state.

Parameters
cardCard descriptor.