GDB server information
One of the functions of LinkServer is to launch and manage the GDB server instances.
./LinkServer gdbserver --help command provides details about the gdbserver command.
A GDB server instance means a crt_emu_cm_redlink utility process started with the appropriate arguments.
The crt_emu_cm_redlink tool can be found in the binaries folder. One of its functions is to process GDB remote protocol requests. Also, it is possible to pass textual GDB commands to it through GDB client and receive textual results via monitor command.
Note
crt_emu_cm_redlink is not intended for use as a standalone tool. If needed, use the crt_emu_cm_redlink --help command to list the supported arguments.
The LinkServer GDB server functions are targeted for debugging applications running on Cortex-M cores. It can be used with standalone GDB clients or with GDB clients integrated within an IDE. The GDB client is a component of the GNU Arm Toolchain.
The IDE automatically sends the GDB commands to initialize a debug session, while a standalone GDB client requires them to be provided manually.
The monitor commands are implementation-specific.
The LinkServer GDB server supports the following monitor commands:
monitor help
This command displays details about the supported monitor commands and their syntax.
Example:
(gdb) monitor help
capabilities -- display capabilities string
catch [set=, | clear=] [event-list | all]
-- set or clear event-catches
counter [watch=0x1234 | clear | set=0x0]
-- watch/clear/set/reset/show cycle counter
flash_load_option [mass_at_0 | no_mass_at_0 | mass_not_0 | no_mass_not_0 | check_0 | no_check_0 | default]
-- set erase rules for load into flash.
help [command] -- show info on all or a specific monitor command
info [,all | ,emu | ,periph ] -- display target information
kill_server -- causes the GDB server to quit when GDB client does
ondisconnect [nochange | stop | cont | run_cont]
-- behavior on disconnect/quit
register_display [* | -| core[-extra|-all] | <name>[!][/] ]
* -- display all peripheral names
- -- display all peripheral details
core -- display main core registers
core-extra -- display additional core registers
core-all -- display main+additional registers
<name>[!][/] -- display peripheral, reg, or field
register_modify [$]<name>=<value> -- update peripheral or register
reset -- issue a processor connection reset
semihosting [ena | dis] -- enable or disable semihosting
stdout [buffered | unbuffered] -- buffer or unbuffer stdout
(gdb)
When given the name of another monitor command, it prints help for that command. Example:
(gdb) monitor help semihosting
Semihosting allows a target application to access host services
such as files, and notably stdio (printf). It does this in a
very non-realtime way (breakpoints). It also requires software
breakpoints on some systems. The default depends on whether
software breakpoints are builtin to the processor.
(gdb)
monitor capabilities
Displays capabilities using upper/lower case letters.
Example:
(gdb) monitor capabilities
CRTv00.1/Apfe/MB08W04C1S/rt/Lf
(gdb)
monitor catch
Usage: catch [set=, | clear=] [event-list | all]
Set, Clear, or Display event catches.
When used without any arguments, it displays all catchable events by name, and current state. Otherwise, you can set or clear one or more by a comma-separated list (or all).
Example:
(gdb) monitor catch set=reset
monitor counter
Usage: counter [watch=0x1234 | clear | set=0x0]
Catch or Clear, (re)Set, or show the state of the cycle counter.
Watch sets the value to match. When the cycle counter reaches that number, it stops the execution.
Clear removes the watch.
Set is used to set a new counter value, which is reset on load. Note: the ‘FPS’ register shows the current counter number as a relative value (from last execution start).
Example:
(gdb) monitor counter watch=0x100
monitor flash_load_option
Usage: flash_load_option [mass_at_0 | no_mass_at_0 | mass_not_0 | no_mass_not_0 | check_0 | no_check_0 | default]
Set erase rules for load into flash.
Choose one of:
mass_at_0,
no_mass_at_0, or
default (mass_at_0).
Choose one of:
mass_not_0,
no_mass_not_0, or
default (no_mass_not_0).
Choose one of:
check_0,
no_check_0, or
default.
Default depends on the target processor. check_0 means to check reset vector when not loading at 0.
monitor info
Usage: info [,all | ,emu | ,periph]
Show information on the target and/or emulator.
The output of this command is different, depending on whether the GDB server was started with -mi or not (MI is used by Eclipse). If started with -mi the output is XML, else normal text.
The
,allqualifier causes all information to be displayed (same as no qualifier).The
,periphqualifier only shows the peripheral information.The
,emuqualifier only shows the emulator defaults.
monitor kill_server
Causes the GDB server to quit when GDB does.
Example:
(gdb) monitor kill_server
Server will now quit when GDB does
monitor ondisconnect
Usage: ondisconnect [nochange | stop | cont | run_cont]
When disconnecting from the target (ending a debug session), it is possible to choose what state the target is left in.
The default is the same as when disconnecting. It is possible always to have it stop, always to have it continue, and to run (reset) and continue.
Example:
(gdb) monitor ondisconnect
Current on disconnect action is: cont
(gdb) monitor ondisconnect stop
(gdb) monitor ondisconnect
Current on disconnect action is: stop
(gdb) monitor ondisconnect cont
(gdb) monitor ondisconnect
Current on disconnect action is: cont
(gdb)
monitor reset
Issues a specific reset, based on the target and image type. The reset method (hard/system/core/soft/romstall/reset script) depends on the target reset configuration and/or the image type (flash/RAM).
Example:
(gdb) monitor reset
Processor connection reset
(gdb)
monitor register_display
Usage: register_display [ core | core-extra | core-all | <register-name>[!][/] ]
Display information about either peripherals or registers.
Command use - register_display core | core-extra | core-all
Display a set of registers as a set of register categories. Each category is preceded with the name of the category.
Different sets of registers are displayed depending on the argument:
core- the main set of processor registerscore-extra- an additional set of registers of interest (currently it seems to provide the same registers ascore)core-all- both thecoreandcore-extraregisters together
Register category names (for example: ‘Core Registers’, ‘IntMask’, ‘FP Registers’) optionally appear in square brackets on a separate line. If the category name is preceded with ‘+’ or ‘-’, it indicates that the following registers are enabled (+) or disabled (-). For example, if the ‘IntMask’ category is listed as ‘+IntMask’ the following interrupt registers are enabled, otherwise interrupts have been disabled. The ‘’ category (which appears as ‘[]’) introduces a set of pseudoregisters the GDB server constructs.
The subsequent lines provide a description of a given register:
[+|-|!] [{<gdbname>}] <name> = <value> [: <valuedescription>]
These lines optionally begin with a ‘+’, ‘-’ or ‘!’ character
no character - register is readable and writeable
‘+’ - register is write only
‘-’ - register is read-only
‘!’ - not really a register at all, a pseudo register
It may then optionally include the register name as used in GDB, shown in braces.
Next comes the register name defined in the GDB server, followed by an ‘=’ sign.
The value that follows is normally presented as a hexadecimal number. If it cannot be read, it could appear as ‘<error>’, or if it logically has no associated value it appears as ‘disabled’.
If followed by a colon (:), the remainder text on the line provides further information about the value for the user.
For example, register_display core can produce this output:
(gdb) mon register_display core
[Core Registers]
{r0}R0=0x000003E8
{r1}R1=0x00400000
{r2}R2=0x2000001C
{r3}R3=0x2000001C
{r4}R4=0x000001D4
{r5}R5=0x00000000
{r6}R6=0x00000000
{r7}R7=0x2002FFE8
{r8}R8=0x00000000
{r9}R9=0x00000000
{r10}R10=0x00000000
{r11}R11=0x00000000
{r12}R12=0x00000000
{sp}SP=0x2002FFE8
{lr}LR=0x0000098B
{pc}PC=0x00000942
{cpsr}xPSR=0x21000000
!Flags=0x21000000:nzCvq
!EPSR=0x21000000:none
!IPSR=0x21000000:0 (Base)
!MSP=0x2002FFE8
PSP=0x00000000
CONTROL=0x0
[+IntMask]
BasePri=0x00
PriMask=0x00
FaultMask=0x00
[]
!Cycle=0x00000111
-CycleDelta=0x1409B6E0
!VECTPC=<error>
!CFSR=0x00000000
!Faults=none
!MMAR=ignore
!BFAR=ignore
[]
[+FP Registers]
{fpscr}FPSCR=0x00000000
{fpccr}FPCCR=0xC0000000
{fpcar}FPCAR=0x00000000
{fpdscr}FPDSCR=0x00000000
{mvfr0}MVFR0=0x10110021
{mvfr1}MVFR1=0x11000011
{s0}S0=0x00000000
{s1}S1=0x00000000
{s2}S2=0x00000000
{s3}S3=0x00000000
{s4}S4=0x00000000
{s5}S5=0x00000000
{s6}S6=0x00000000
{s7}S7=0x00000000
{s8}S8=0x00000000
{s9}S9=0x00000000
{s10}S10=0x00000000
{s11}S11=0x00000000
{s12}S12=0x00000000
{s13}S13=0x00000000
{s14}S14=0x00000000
{s15}S15=0x00000000
{s16}S16=0x00000000
{s17}S17=0x00000000
{s18}S18=0x00000000
{s19}S19=0x00000000
{s20}S20=0x00000000
{s21}S21=0x00000000
{s22}S22=0x00000000
{s23}S23=0x00000000
{s24}S24=0x00000000
{s25}S25=0x00000000
{s26}S26=0x00000000
{s27}S27=0x00000000
{s28}S28=0x00000000
{s29}S29=0x00000000
{s30}S30=0x00000000
{s31}S31=0x00000000
{d0}D0=0x0000000000000000
{d1}D1=0x0000000000000000
{d2}D2=0x0000000000000000
{d3}D3=0x0000000000000000
{d4}D4=0x0000000000000000
{d5}D5=0x0000000000000000
{d6}D6=0x0000000000000000
{d7}D7=0x0000000000000000
{d8}D8=0x0000000000000000
{d9}D9=0x0000000000000000
{d10}D10=0x0000000000000000
{d11}D11=0x0000000000000000
{d12}D12=0x0000000000000000
{d13}D13=0x0000000000000000
{d14}D14=0x0000000000000000
{d15}D15=0x0000000000000000
Command use - register_display <name>[!][/]
The name provided can be a core register name.
Currently it also accepts:
the name of a peripheral
the name of a register within any peripheral (the first with a register of that name is chosen)
<peripheral>.<register>- the name of a peripheral and a register within it<peripheral>.<register>.<field>- the name of a field within a register within a peripheral<register>.<field>- the name of a field within any peripheral (the first with a register of that name is chosen).
The usage for displaying peripheral information is deprecated and planned for removal.
The names do not need to match the case of the names listed in register_display core (which are typically uppercase).
These commands display details of a given register.
Two letters can follow the name of the register or peripheral to be displayed:
! - means that both volatile and nonvolatile registers are read
/ - means that the field contents is also displayed
Lines showing the register contents are either:
[?] <name> [=|:] <value>
These lines optionally begin with a ‘?’ which is present if the register is volatile (for example, its value could change upon reading).
An equal sign (=) follows the name normally, but it is replaced with a colon (:) for read-only register.
The value is displayed as ‘?’ if the register is volatile and volatile reads have not been requested. If the value could not be read, it is displayed as ‘error’. Otherwise, it appears in decimal, hexadecimal, or as the corresponding enumeration name.
Lines showing field contents contain ‘!’ before the register name and are on lines immediately following the display of the parent register. These details are presented on lines with the syntax [?]!<name>=<value>.
In this case, the value is provided either as a hexadecimal value or as a text string interpreting its meaning, intended for a user. As with the register content an initial ‘?’ is used to indicate that the value of the field is volatile.
Example core register from register_display r1
r1=0x00000000
monitor register_modify
Usage: register_modify [$]<name>=<value>
Write a value to the given register.
The name provided can be a core register name.
A dollar sign ($) can precede the register name but it is ignored.
Currently it also accepts:
the name of a register within any peripheral (the first with a register of that name is chosen)
<peripheral>.<register>- the name of a peripheral and a register within it
The usage for modifying peripheral register is deprecated and planned for removal.
monitor semihosting
Usage: monitor semihosting [ena | dis]
With no argument reports whether semihosting is enabled or disabled. Otherwise
ena- enables semihostingdis- disables semihosting
When semihosting is disabled, the semihosting BKPT instructions executed on the target are ignored (by continuing execution on the target). Otherwise, the accompanying I/O request is decoded and acted upon.
Example:
(gdb) monitor semihosting
Semihosting enabled.
(gdb) monitor semihosting ena
Semihosting enabled.
(gdb) monitor semihosting dis
Semihosting disabled.
(gdb)
monitor stdout
Usage: stdout [buffered | unbuffered]
If semihosted I/O is in use, this command controls whether the target semihosted output is buffered or not. If no argument is provided, the command reports whether the semihosted output is buffered or not. Otherwise:
buffered- the output is bufferedunbuffered- the output is unbuffered
When unbuffered, each write from the host is written directly to the semihosted output channel. When buffered, data is first accumulated in a buffer and then written to the semihosted output channel every few microseconds (if data is available).