Miscellaneous configurations
The LinkServer debug support for a particular board or device is based on the information included in the corresponding JSON files. A JSON file can include multiple entries.
For example, the support for several legacy devices is included in preinstalled_devices.json.
Device specific configuration
Besides the device identification information, the device configuration includes properties related to cores and memory regions (especially the flash regions and the associated flash drivers).
Debug specific configuration
The debug properties that can be configured for a device are listed below:
core-options:<core-name>:cachelib: a specific cache library used by LinkServer to manage memory accesses during the debug sessions (--cachelib <lib>.somiscellaneous option for LinkServer GDB server)connect-reset: reset method on initial connection (system,core,default)flash-driver-reset: reset method before running the RAM-loaded flash driver (system,core,soft)reset: reset method used to start the image loaded (system,core,soft)preattach-script: a pre attach script used for attach sessionspreconnect-script: a pre connect script used for debug sessionsconnect-script: a connect script used for debug sessionsreset-script: a reset script used for debug sessionsmasserase-script: a mass-erase script used for resurrecting some devicesbootromstall: BootROM stall addressromstalldelay: BootROM stall delay in millisecondsno-flash-hashing: disable flash hashing (enabled by default)no-packed: Debug Access Port (DAP) does not support packed transfersdapstride: DAP stride mode (auto,standard,long,short)apindex-limit: DAP AP index limitprotocol: debug protocol (swd,jtag)wirespeed: the wire speed in Hzswo: has SWO supportbootconfigs: boot configurations (name:<data>pairs) aimed to be used with MCU-Link on-board probes.<data>is a string of 4 characters (‘x’, ‘1’ or ‘0’) describing how each ISP_CTRL[3…0] pin is handled
Cache library (core-options:<core-name>:cachelib)
For applications that enable caching, the LinkServer GDB server must use an appropriate cachelib for cache management. Otherwise, the memory write operations from the debugger could not be visible to the core (for example, setting software breakpoints).
The cache libraries currently supported are:
libahb_lpcac.so: specific to AHB LPCAC controller and Cortex-M4 core (supported on some older devices such as K32L3A)libahb_lmem.so: specific to AHB LMEM controller and Cortex-M4 core (RT116x/RT117x devices)libahb_xcache.so: specific to XCACHE controller and Cortex-M33 core (RT118x/RT7xx devices)libm7_cache.so: specific to internal I/D-Cache of Cortex-M7 core (RT10xx/RT11xx devices)
Note: The GDB server loads these libraries at runtime. Although they use .so extension, they are native libraries for each operating system (DLL on Windows, dylib on macOS).