Import Repository
The first operation in the proposed development flow in MCUXpresso for VS Code is to import a software repository. A software repository may have different sources supported by this extension: MCUXpresso SDK or Zephyr.
In order to achieve this, go to the MCUXpresso for VS Code extension, Imported Repositories option and press the ‘+’ symbol in the upper right of the toolbar (Help text will display ‘Import Local/Remote Repository’ when hovering over symbol. Alternatively use link found in Quickstart Panel)
Note: The big blue “Import repository” button is only available until the first repository is imported to the workspace.

MCUXpresso SDK
For MCUXpresso SDK repository installation, please follow MCUXpresso SDK related documentation on MCUXpresso SDK
Zephyr
For Zephyr repository installation, please follow Zephyr related documentation on Zephyr
Other repository operations
Import local Git repository
If a user already has a software repository in a local directory, they can directly import the folder by using the “LOCAL” option.

Remove or delete a repository
Each repository can be removed from the visible area without deleting it from disk:

Confirmation dialog will appear before removing the repository from the visible area:

This behavior can be disabled in the Settings page, using the Repository Removal Confirmation setting.
Repositories can also be deleted permanently from disk by selecting the delete option from the context menu:

Refresh repositories
If changes were made to one or more repositories, the “Refresh repositories” button from the toolbar can be used to update the information displayed in the view.

Note: The button also invalidates the cached data so a subsequent load will be slower.
Update repository
An existing repository may also be updated via the west update command.

Source Control extension
Once a repository is imported, the Source Control view within Visual Studio Code will track all sub-repositories that constitute the given git repository. This is a useful utility for monitoring changes made during development.

Terminal
Context menu for an imported repository provides access to the integrated terminal, allowing direct command execution within the repository directory.