This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

FRDM-KE15Z

Overview

The FRDM-KE15Z Freedom Board is designed to work in standalone mode or as the main board of FRDM-TOUCH, FRDM-MC-LVBLDC, and Arduino boards. This Freedom board is compatible with DC 5v and 3.3v power supply, and features a KL15Z, a device boasting up to 256KB Flash and 32KB SRAM and numerous analog and digital peripherals. The on-board interfaces include an RGB LED, a 6-axis digital sensor, a 3-axis digital angular rate gyroscope, an ambient light sensor, and a capacitive touch slider.

FRDM-KE15Z

MCU device and part on board is shown below:

  • Device: MKE15Z7

  • PartNumber: MKE15Z256VLL7

Getting Started

Getting Started with MCUXpresso SDK for FRDM-KE15Z