This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

FRDM-KE17Z512

Overview

he FRDM-KE17Z512 Freedom Board is designed to work in standalone mode or as the main board of FRDM-TOUCH, FRDM-MC-LVBLDC, and Arduino boards. This Freedom board is compatible with DC 5v and 3.3v power supply and features a KE17Z, a device boasting up to 512KB Flash and 96KB SRAM, and numerous analog and digital peripherals.The onboard interfaces include an RGB LED, a 6-axis digital sensor, a 3-axis digital angular rate gyroscope, an ambient temperature sensor, and two capacitive touch pads.
FRDM-KE17Z512

MCU device and part on board is shown below:

  • Device: MKE17Z9

  • PartNumber: MKE17Z512VLL9

Getting Started

Getting Started with MCUXpresso SDK for FRDM-KE17Z512