This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

afe_qtimer

Overview

The AFE Example project is a demonstration program that uses the KSDK software. In this case the example provide two functions. Measure the voltage difference two pin of the channel 2 and 3. And monitor AC frequency on two pins of channel 2.

Supported Boards