dsc_dac_pin_sync_triangle_waveform
Overview
The dac_pin_sync_triangle_waveform demo sets the DAC module as Automatic mode to generate repeated triangle waveform, the frequency of triangle waveform is 100Hz. The SYNC signal is selected as external SYNC_IN signal(GPIO signal connected by XBAR), user can press on-board button to generate SYNC_IN signal.