This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

ftm_pdb_adc16_peripheral

Overview

The FTM / PDB demo application demonstrates how to use the FTM external trigger to start the ADC conversion using the PDB. FTM0 is configured as a pwm combined mode, and each channel output frequency is 16 KHz.The PDB pre-trigger works in back-to-back mode. The ADC0 and ADC1 work in single-end mode.The ADC0 uses channel 9 and channel 26, and ADC1 uses channel 9 and channel 8.

Supported Boards