This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

lin_stack_slave

Overview

The lin_stack_slave demo is used to demonstrate how to use the lin stack as slave node.

  • The master node is in NormalTable schedule table and it uses the LIN frame Motor1State_Cycl to receive data from slave node and send selection signal Motor1Selection command to slave node by Motor1Control.

  • If the command from master is STOP, slave will STOP current data count.

  • If the command from master is INCREASE, slave will countinue increase the tick count every 500us.

  • If the command from master is DECREASE, slave will countinue decrease the tick count every 500us. So, the value from slave will keep changing between MOTOR1_MAX_VALUE and MOTOR_MIN_VALUE.

  • If the button 1 was pressed, the slave will change the tick count higher than MOTOR1_STOP_VALUE and send the data to master node.

  • If button 2 was pressed, the slave will set the tick count to 0, and start another loop count.

  • Once running successfully, the state of LEDs on master node and slave node will keep aligned.

Supported Boards