This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

lpadc_high_sample_rate_sample_signal

Overview

This demo application demonstrates the use of the LPADC to sample the analog signal. In this demo, the ADC clock is set as the maximum frequency, users should input analog signals to the ADC channel, press any keys to trigger the ADC conversion. After sampling enough sample points, the ADC will be disabled and the sample data will be print via UART. Users can use some tools such as EXCEL to recover the input signal based on those printed data.

Supported Boards