This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

pwm_fault

Overview

This demo application demonstrates the EflexPWM fault demo. This application demonstrates the pulse with modulation function of EflexPWM module. It outputs the PWM to control the intensity of the LED. PWM shut down when a fault signal is detected on the CMP output. One input of CMP, other input is from internal DAC.

Supported Boards