This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

rtc_func

Overview

The RTC demo application demonstrates the important features of the RTC Module by using the RTC Peripheral Driver.

The RTC demo supports the following features:

  • Calendar

    • Get the current date time with Year, Month, Day, Hour, Minute, and Second.

    • Set the current date time with Year, Month, Day, Hour, Minute, and Second.

  • Alarm

    • Set the alarm based on the current time.

    • Application prints a notification when the alarm expires.

  • Seconds interrupt

    • Use second interrupt function to display a digital time blink every second.

Supported Boards