This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

xrdc_hard_fault_handler

Overview

The XRDC hard fault demo application demonstrates how the resources (memory regions and peripherals) can be protected by XRDC peripheral. XRDC is configured by the RDMGR component, which uses configuration file (config block) generated by PAM tool. In this example is used configuration where CPU0 has no access to memory region from address deffined by macro MEM_REG_START and WDOG0 peripheral. Access to this resources causes hard fault event, this example also shows how can be handled and read information about violent access from XRDC peripheral. The first memory region (kXRDC_MemMrc0_0) is configured with option “lock”, it means the XRDC registers for this memory region will be set only once, changes will not be possible until the next reset. The application try change the configuration of locked memory region, but the configuration remains unchanged.