This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

dsp_audio_demo_bm

Overview

The audio baremetal demo demonstrates audio processing using DSP core. It uses the DMIC working with I2S. One channel Audio data is converted to samples in the DMIC module. Then, the data is placed into the memory buffer. Last, it is sent to the I2S buffer and output to the CODEC, where the audio data will be heard from lineout.

Supported Boards