This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

dsp_xaf_usb_demo

Overview

The dsp_xaf_usb_demo application demonstrates audio processing using the DSP core, the Xtensa Audio Framework (XAF) middleware library.

When the application is started, a shell interface is displayed on the terminal that executes from the ARM application. User can control this with shell commands which are relayed via RPMsg-Lite IPC to the DSP where they are processed and response is returned.

Type “help” to see the command list.

This demo contains two applications:

  • cm33/ is the ARM application for Cortex-M33 core

  • dsp/ is the DSP application for DSP core

The release configurations of the demo will combine both applications into one ARM image. With this, the ARM core will load and start the DSP application on startup. Pre-compiled DSP binary images are provided under dsp/binary/ directory. If you make changes to the DSP application in release configuration, rebuild ARM application after building the DSP application. If you plan to use MCUXpresso IDE for cm33 you will have to make sure that the preprocessor symbol DSP_IMAGE_COPY_TO_RAM, found in IDE project settings, is defined to the value 1 when building release configuration.

The debug configurations will build two separate applications that need to be loaded independently. DSP application can be built by the following tools: Xtensa Xplorer or Xtensa C Compiler. Required tool versions can be found in MCUXpresso SDK Release Notes for the board. Application for cm33 can be built by the other toolchains listed there. If you plan to use MCUXpresso IDE for cm33 you will have to make sure that the preprocessor symbol DSP_IMAGE_COPY_TO_RAM, found in IDE project settings, is defined to the value 0 when building debug configuration. The ARM application will power and clock the DSP, so it must be loaded prior to loading the DSP application.

There are limited features in release SRAM target because of memory limitations. To enable/disable components, set appropriate preprocessor define in project settings to 0/1. Debug and flash targets have full functionality enabled.

In order to get TRACE debug output from the XAF it is necessary to define XF_TRACE 1 in the project settings. It is possible to save the TRACE output into RAM using DUMP_TRACE_TO_BUF 1 define on project level. Please see the initalization of the TRACE function in the xaf_main_dsp.c file. For more details see XAF documentation.

Supported Boards