This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

dsp_mu_interrupt

Overview

The dsp_mu_interrupt demo application demonstrates starting DSP core with DSP image.

In this example:

  1. M33 core send message to DSP in interrupt mode via MU module.

  2. DSP send message back to M33 core in interrupt mode.

  3. M33 core receive message sent from DSP in interrupt mode.

Supported Boards