This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

freertos_gpio

Overview

This document explains the freertos_gpio example. It shows the CPU enter at sleep mode and then it is waked up by expired time delay that using GPT Timer module or occur any a hardware interrupt.

The example application creates two identical instances task,gpio_task and print_task. Each task will lock the mutex before executing task and unlock it after the task finishes.

Running the demo

After the board is flashed the Tera Term will start periodically printing strings synchronized by mutex.

Freertos Gpio example

The LED is blinking.

The gpio task is running:1times.

The LED is blinking.

The gpio task is running:2times.

The LED is blinking.

The gpio task is running:3times. …… ……

Explanation of the example

The example application will get tick count number after every period time delay vTaskDelay(time) When this function called the CPU enter to sleep mode a period of time that called by vTaskDelay function.

Supported Boards