This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

freertos_lpsci

Overview

The LPSCI example for FreeRTOS demonstrates the possibility to use the LPSCI driver in the RTOS. The example uses single instance of LPSCI IP and writes string into, then reads back chars. After every 4B received, these are sent back on LPSCI.

Supported Boards