This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

freertos_lpc_vusart

Overview

The USART example for FreeRTOS demonstrates the possibility to use the USART driver in the RTOS. The example uses single instance of USART IP and writes string into, then reads back chars. After every 4B received, these are sent back on USART.

Supported Boards