Memory attribution map after doing handshake

The memory attribution map settings after the handshake procedure is successful between Cortex-M33 and Cortex-A35.

Name

Memory block checker/ Memory region checker (MBC/MRC)

Resulting access level

FLEXSPI1 (alias)

Non Secure

Non Secure

0x5FFF_FFFF

0x5000_0000

FLEXSPI1

Non Secure

Non Secure

0x4FFF_FFFF

0x4000_0000

PBridge1 FlexCAN0 (alias)

Non Secure

Non Secure

0x380A_BFFF

0x380A_8000

PBridge1 SAI0 (alias)

Non Secure

Non Secure

0x3809_C0FF

0x3809_C000

PBridge1 LPUART1 (alias)

Non Secure

Non Secure

0x3809_B02F

0x3809_B000

PBridge1 LPI2C0 (alias)

Non Secure

Non Secure

0x3809_8173

0x3809_8000

PBridge1 FlexSPI1 (alias)

Non Secure

Non Secure

0x3809_22FF

0x3809_2000

PBridge0 LPSPI1 (alias)

Non Secure

Non Secure

0x3803_F7FF

0x3803_F000

PBridge0 FlexIO0 (alias)

Non Secure

Non Secure

0x3803_C91F

0x3803_C000

PBridge0 FlexSPI0 (alias)

Non Secure

Non Secure

0x3803_92FF

0x3803_9000

PBridge1 FlexCAN0

Non Secure

Non Secure

0x280A_BFFF

0x280A_8000

PBridge1 SAI0

Non Secure

Non Secure

0x2809_C0FF

0x2809_C000

PBridge1 LPUART1

Non Secure

Non Secure

0x2809_B02F

0x2809_B000

PBridge1 LPI2C0

Non Secure

Non Secure

0x2809_8173

0x2809_8000

PBridge1 FlexSPI1

Non Secure

Non Secure

0x2809_22FF

0x2809_2000

PBridge0 LPSPI1

Non Secure

Non Secure

0x2803_F7FF

0x2803_F000

PBridge0 FlexIO0

Non Secure

Non Secure

0x2803_C91F

0x2803_C000

PBridge0 FlexSPI0

Non Secure

Non Secure

0x2803_92FF

0x2803_9000

SSRAM P6 (alias)

Non Secure

Non Secure

0x3007_FFFF

0x3006_0000

SSRAM P5 (alias)

Non Secure

Non Secure

0x3005_FFFF

0x3004_0000

SSRAM P4 (alias)

Non Secure

Non Secure

0x3003_FFFF

0x3003_0000

SSRAM P3 (alias)

Non Secure

Non Secure

0x3002_FFFF

0x3002_0000

SSRAM P2 (alias)

Non Secure

Non Secure

0x3001_FFFF

0x3001_0000

SSRAM P1 (alias)

Non Secure

Non Secure

0x3000_FFFF

0x3000_8000

SSRAM P0 (alias)

Non Secure

Non Secure

0x3000_7FFF

0x3000_0000

SSRAM P6

Non Secure

Non Secure

0x2007_FFFF

0x2006_0000

SSRAM P5

Non Secure

Non Secure

0x2005_FFFF

0x2004_0000

SSRAM P4

Non Secure

Non Secure

0x2003_FFFF

0x2003_0000

SSRAM P3

Non Secure

Non Secure

0x2002_FFFF

0x2002_0000

SSRAM P2

Non Secure

Non Secure

0x2001_FFFF

0x2001_0000

SSRAM P1

Non Secure

Non Secure

0x2000_FFFF

0x2000_8000

SSRAM P0

Non Secure

Non Secure

0x2000_7FFF

0x2000_0000

SSRAM P7 (alias)

Non Secure

Non Secure

0x1FFF_FFFF

0x1FFC_0000

FlexSPI0 (alias)

Non Secure

Non Secure

0x1BFF_FFFF

0x1400_0000

SSRAM P7

Non Secure

Non Secure

0x0FFF_FFFF

0x0FFC_0000

FlexSPI0

Non Secure

Non Secure

0x0BFF_FFFF

0x0400_0000

Note:

  1. Assign Domain 1 for DMA1, USB0, USB1, ENET, USDHC0, USDHC1, USDHC2, and CAAM Master.

  2. The bus attribute for DMA1, USB0, USB1, ENET, USDHC0, USDHC1, and USDHC2 is Non Secure.

  3. The bus attribute for CAAM Master is Secure.

  4. Security level of MBC/MRC settings of other memory space that are not be shown in the table for Domain 1 are Secure, so master cannot access resources that are controlled by MBC/MRC in other memory spaces when master is in Non Secure state.

|Name|MBC/MRC|Resulting access level| | |—-|:—–:|:——————–:|::| |PBridge1|Non Secure|Non Secure|0x280F_FFFF| |0x2808_0000| |SSRAM P2|Secure|No Access|0x2001FFFF| |0x20018000| |Non Secure|Non Secure|0x20017FFF| |0x20010000|

Note:

  1. Assign Domain 1 for DMA1, USB0, USB1, ENET, UDSHC0, USDHC1, UDSHC2, and CAAM Master.

  2. Security level of MBC/MRC settings of other memory space that are not shown in the table for Domain 1 are Secure, so the master cannot access resources that are controlled by MBC/MRC in other memory spaces.

|Name|SAU|IDAU|MBC/MRC|Resulting access level| | |—-|—|—-|——-|:——————–:|::| |GPIOC_REGS (alias)|Secure|Secure|Secure|Secure|0x3882_FFFF| |0x3882_0000| |GPIOB_REGS (alias)|Secure|Secure|Secure|Secure|0x3881_FFFF| |0x3881_0000| |GPIOA_REGS (alias)|Secure|Secure|Secure|Secure|0x3880_FFFF| |0x3880_0000| |MICFIL (alias)|Secure|Secure|Secure|Secure|0x3811_10AB| |0x3811_1000| |SAI3 (alias)|Secure|Secure|Secure|Secure|0x3811_00FF| |0x3811_0000| |SAI2 (alias)|Secure|Secure|Secure|Secure|0x3810_F0FF| |0x3810_F000| |LPSPI3 (alias)|Secure|Secure|Secure|Secure|0x3810_E7FF| |0x3810_E000| |LPSPI2 (alias)|Secure|Secure|Secure|Secure|0x3810_D7FF| |0x3810_D000| |LPUART3 (alias)|Secure|Secure|Secure|Secure|0x3810_C02F| |0x3810_C000| |LPUART2 (alias)|Secure|Secure|Secure|Secure|0x3810_B02F| |0x3810_B000| |I3C1 (alias)|Secure|Secure|Secure|Secure|0x3810_AFFF| |0x3810_A000| |LPI2C3 (alias)|Secure|Secure|Secure|Secure|0x3810_9173| |0x3810_9000| |LPI2C2 (alias)|Secure|Secure|Secure|Secure|0x3810_8173| |0x3810_8000| |MRT (alias)|Secure|Secure|Secure|Secure|0x3810_70FF| |0x3810_7000| |TPM3 (alias)|Secure|Secure|Secure|Secure|0x3810_6087| |0x3810_6000| |TPM2 (alias)|Secure|Secure|Secure|Secure|0x3810_5087| |0x3810_5000| |PCC2 (alias)|Secure|Secure|Secure|Secure|0x3810_2047| |0x3810_2000| |WDOG2 (alias)|Secure|Secure|Secure|Secure|0x3810_100F| |0x3810_1000| |MU1_B (alias)|Secure|Secure|Secure|Secure|0x3810_028F| |0x3810_0000| |FlexCAN0 (alias)|Secure|Secure|Secure|Secure|0x380A_BFFF| |0x380A_8000| |ADC1 (alias)|Secure|Secure|Secure|Secure|0x380A_2303| |0x380A_2000| |IOMUXC0 (alias)|Secure|Secure|Secure|Secure|0x380A_1AEB| |0x380A_1000| |SAI1 (alias)|Secure|Secure|Secure|Secure|0x3809_D0FF| |0x3809_D000|

Note:

  1. SAU is disabled.

  2. Cortex-M33 can access all of the secure resources. All of the resources (the security level of these resources that are controlled by MBC/MRC) are secure when Cortex-M33 is in secure state.

  3. Assign domain 6 for Cortex-M33.

Name

MBC/MRC

Resulting access level

PBridge1 IOMUXC0

Non Secure

Non Secure

0x280A_1AEB

0x280A_1000

PBridge1 LPI2C0

Non Secure

Non Secure

0x2809_8173

0x2809_8000

PBridge1 TPM0

Non Secure

Non Secure

0x2809_5087

0x2809_5000

PBridge1 PCC1

Non Secure

Non Secure

0x2809_10BF

0x2809_1000

PBridge0 FlexSPI0

Non Secure

Non Secure

0x2803_92FF

0x2803_9000

PBridge0 SEMA42_0

Non Secure

Non Secure

0x2803_7043

0x2803_7000

PBridge0 CGC0

Non Secure

Non Secure

0x2802_FFFF

0x2802_F000

PBridge0 SIM0-S

Non Secure

Non Secure

0x2802_B3FF

0x2802_B000

S400 MU-AP of EdgeLock secure enclave

Non Secure

Non Secure

0x2702_028C

0x2702_0000

FSB of EdgeLock secure enclave

Non Secure

Non Secure

0x2701_0BFC

0x2701_0000

SSRAM P7

Non Secure

Non Secure

0x1FFF_FFFF

0x1FFF_8000

Secure

Secure

0x1FFF_7FFF

0x1FFC_0000

FlexSPI0

Non Secure

Non Secure

0x0BFF_FFFF

0x0400_0000

Note:

  1. Security level of MBC/MRC settings of Other memory space that are not shown in the table for Domain 7 are Secure. The master can access resources that are controlled by MBC/MRC in other memory spaces when the master is in secure state.

  2. Assign domain 7 for Cortex-A35.