Toolchain introduction
The MCUXpresso SDK release for i.MX 95 includes the build system to be used with some toolchains. In this chapter, the toolchain support is presented and detailed.
Compiler/Debugger
The MCUXpresso SDK i.MX 95 release supports building and debugging with the toolchains listed in Table 1.
The user can choose the appropriate one for development.
For supported toolchain versions, see MCUXpresso SDK Release Notes for for IMX95LPD5EVK-19, IMX95LP4XEVK-15, and IMX95VERDINEVK (document: MCUXSDKIMX95SERIESRN).
Arm GCC + SEGGER J-Link GDB Server. This is a command line tool option and it supports both Windows OS and Linux OS.
IAR Embedded Workbench for Arm and SEGGER J-Link software. The IAR Embedded Workbench is an IDE integrated with editor, compiler, debugger, and other components. The SEGGER J-Link software provides the driver for the J-Link Plus debugger probe and supports the device to attach, debug, and download.
Compiler/Debugger |
Supported host OS |
Debug probe |
Tool website |
---|---|---|---|
ArmGCC/J-Link GDB server |
Windows OS/Linux OS |
J-Link Plus |
| |IAR/J-Link|Windows OS|J-Link Plus|www.iar.com
|
Download the corresponding tools for the specific host OS from the website.
Note:
To support i.MX 95, the patch for IAR and Segger J-Link must be installed. To get the patch, download it from the NXP website or contact your local field applications engineer (FAE) or the sales representative.
Parent topic:Toolchain introduction