call_terminal
Overview
Application demonstrating how to use the telephone call terminal feature of LE Audio.
Prepare the Demo
Open example’s project and build it.
Connect a USB cable between the PC host and the OpenSDA USB port on the target board.
Provide 5V voltage for the target board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Note: the example can work with call_gateway example. Please refer to the readme of call_gateway to prepare the call_gateway exmaple.
Running the demo
The log below shows the output of the example in the terminal window.
Copyright 2022 NXP
call_terminal>> Bluetooth initialized
Advertising successfully started
Procedures to run 1 input “help” to show command list, 2 the advertising of the device is started automatically, 3 Aftert the conenction is estabilished, the log is following. Please note that if the Security is changed with error 0x02, it means the key is missing. Please clear bonding information by sending commander “unpair”. And, retry again.
MTU exchanged: 23/23
Starting TBS server discover
Connected to peer: A0:CD:F3:77:E3:E9 (public)
MTU exchanged: 65/65
Security changed: A0:CD:F3:77:E3:E9 (public) level 2 (error 0)
4 After the message “Discover complete (err 0)! TBS count 1, GTBS found? Yes” is printed on call_terminal side. All feature are ready.
5.1. Start the call by local.
Enter “call_outgoing 0
List current state of current calls (err 0). TBS Index 255, call count 1, call state list,
call index 1, state 1, flags 1.
List current calls (err 0). TBS Index 255, call count 1, call list,
call index 1, state 1, flags 1, remote uri tel:qq
List current state of current calls (err 0). TBS Index 0, call count 1, call state list,
call index 1, state 1, flags 1.
List current state of current calls (err 0). TBS Index 255, call count 1, call state list,
call index 1, state 2, flags 1.
List current calls (err 0). TBS Index 255, call count 1, call list,
call index 1, state 2, flags 1, remote uri tel:qq
List current state of current calls (err 0). TBS Index 0, call count 1, call state list,
call index 1, state 2, flags 1.
ASE Codec Config: conn 202DE340 ep 202D9214 dir 2
Codec configurations:
Frequency 16000
Duration 10000
Frame bytes 40
Frame blocks per SDU 1
Location 3, channel count 2.
ASE Codec Config: conn 202DE340 ep 202D92DC dir 1
Codec configurations:
Frequency 16000
Duration 10000
Frame bytes 40
Frame blocks per SDU 1
Location 3, channel count 2.
QoS: stream 202EFF80 qos 202D9284
interval 10000 framing 0x00 phy 0x02 sdu 80 rtn 2 latency 10 pd 40000
QoS: stream 202F6350 qos 202D934C
interval 10000 framing 0x00 phy 0x02 sdu 80 rtn 2 latency 10 pd 40000
Enable: stream 202EFF80 meta_count 1
Enable: stream 202F6350 meta_count 1
Init Audio SAI and CODEC, samplingRate :16000 bitWidth:16
Set default headphone volume 70
Start: stream 202F6350
Start: stream 202EFF80
Or, enter “call_outgoing 0
outgoing call: callee uri tel:qq, TBS index 0
Return code 0
call_terminal>> List current state of current calls (err 0). TBS Index 255, call count 1, call state list,
call index 1, state 1, flags 1.
List current calls (err 0). TBS Index 255, call count 1, call list,
call index 1, state 1, flags 1, remote uri tel:qq
List current state of current calls (err 0). TBS Index 0, call count 1, call state list,
call index 1, state 1, flags 1.
List current state of current calls (err 0). TBS Index 255, call count 1, call state list,
call index 1, state 2, flags 1.
List current calls (err 0). TBS Index 255, call count 1, call list,
call index 1, state 2, flags 1, remote uri tel:qq
List current state of current calls (err 0). TBS Index 0, call count 1, call state list,
call index 1, state 2, flags 1.
Control Point status update. A call outgoing (err 0). TBS Index 0, call index 1
List current state of current calls (err 0). TBS Index 255, call count 1, call state list,
call index 1, state 2, flags 1.
List current calls (err 0). TBS Index 255, call count 1, call list,
call index 1, state 2, flags 1, remote uri tel:qq
List current state of current calls (err 0). TBS Index 0, call count 1, call state list,
call index 1, state 2, flags 1.
List current state of current calls (err 0). TBS Index 255, call count 1, call state list,
call index 1, state 2, flags 1.
List current calls (err 0). TBS Index 255, call count 1, call list,
call index 1, state 2, flags 1, remote uri tel:qq
List current state of current calls (err 0). TBS Index 0, call count 1, call state list,
call index 1, state 2, flags 1.
ASE Codec Config: conn 202DE340 ep 202D9214 dir 2
Codec configurations:
Frequency 16000
Duration 10000
Frame bytes 40
Frame blocks per SDU 1
Location 3, channel count 2.
ASE Codec Config: conn 202DE340 ep 202D92DC dir 1
Codec configurations:
Frequency 16000
Duration 10000
Frame bytes 40
Frame blocks per SDU 1
Location 3, channel count 2.
QoS: stream 202EFF80 qos 202D9284
interval 10000 framing 0x00 phy 0x02 sdu 80 rtn 2 latency 10 pd 40000
QoS: stream 202F6350 qos 202D934C
interval 10000 framing 0x00 phy 0x02 sdu 80 rtn 2 latency 10 pd 40000
Enable: stream 202EFF80 meta_count 1
Enable: stream 202F6350 meta_count 1
Init Audio SAI and CODEC, samplingRate :16000 bitWidth:16
Set default headphone volume 70
Start: stream 202F6350
Start: stream 202EFF80
5.2 Start a call by remote. Enter “remote_call_incoming 0
Read incoming call URI tel:qq (err 0). TBS Index 0.
incoming call inst_index 0, call_index = 1, uri tel:qq
Read Friendly name qq (err 0). TBS Index 0.
Read incoming call URI tel:qq (err 0). TBS Index 255.
incoming call inst_index 255, call_index = 1, uri tel:qq
Read Friendly name (err 0). TBS Index 255.
List current state of current calls (err 0). TBS Index 255, call count 1, call state list,
call index 1, state 0, flags 0.
List current calls (err 0). TBS Index 255, call count 1, call list,
call index 1, state 0, flags 0, remote uri tel:qq
List current state of current calls (err 0). TBS Index 0, call count 1, call state list,
call index 1, state 0, flags 0.
ASE Codec Config: conn 202DE340 ep 202D9214 dir 2
Codec configurations:
Frequency 16000
Duration 10000
Frame bytes 40
Frame blocks per SDU 1
Location 3, channel count 2.
ASE Codec Config: conn 202DE340 ep 202D92DC dir 1
Codec configurations:
Frequency 16000
Duration 10000
Frame bytes 40
Frame blocks per SDU 1
Location 3, channel count 2.
QoS: stream 202EFF80 qos 202D9284
interval 10000 framing 0x00 phy 0x02 sdu 80 rtn 2 latency 10 pd 40000
QoS: stream 202F6350 qos 202D934C
interval 10000 framing 0x00 phy 0x02 sdu 80 rtn 2 latency 10 pd 40000
Enable: stream 202EFF80 meta_count 1
Enable: stream 202F6350 meta_count 1
Init Audio SAI and CODEC, samplingRate :16000 bitWidth:16
Set default headphone volume 70
Start: stream 202F6350
Start: stream 202EFF80
6.1 Reject/end the remote call, enter “call_term <call_index>” on the call_gateway side
Call terminated(err 0). TBS Index 0, call index 1, reason 3.
Speaker mute
Call terminated(err 0). TBS Index 255, call index 1, reason 3.
Disable: stream 202EFF80
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Stop: stream 202EFF80
Disable: stream 202F6350
Audio Stream 202F6350 stopped with reason 0x13
Audio Stream 202EFF80 stopped with reason 0x13
Release: stream 202EFF80
Release: stream 202F6350
Or, enter “call_term 0 <call_index>” on the call_terminal side
Terminate call: TBS index 0, call index 1
Return code 0
call_terminal>> Call terminated(err 0). TBS Index 0, call index 1, reason 6.
Speaker mute
Call terminated(err 0). TBS Index 255, call index 1, reason 6.
Control Point status update. A call has been terminated (err 0). TBS Index 0, call index 1
List current state of current calls (err 0). TBS Index 255, call count 0, call state list,
List current calls (err 0). TBS Index 255, call count 0, call list,
List current state of current calls (err 0). TBS Index 0, call count 0, call state list,
List current calls (err 0). TBS Index 0, call count 0, call list,
Disable: stream 202EFF80
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Stop: stream 202EFF80
Disable: stream 202F6350
Audio Stream 202F6350 stopped with reason 0x13
Audio Stream 202EFF80 stopped with reason 0x13
Release: stream 202EFF80
Release: stream 202F6350
6.2 Reject/end the call by remote. enter “remote_call_term <call_index>” on the call_gateway side
Call terminated(err 0). TBS Index 0, call index 1, reason 2.
Speaker mute
Call terminated(err 0). TBS Index 255, call index 1, reason 2.
Disable: stream 202EFF80
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Stop: stream 202EFF80
Disable: stream 202F6350
Audio Stream 202F6350 stopped with reason 0x13
Audio Stream 202EFF80 stopped with reason 0x13
Release: stream 202EFF80
Release: stream 202F6350
7.1 Accept the remote call. enter “call_accept <call_index>” on the call_gateway side
List current state of current calls (err 0). TBS Index 255, call count 1, call state list,
call index 1, state 3, flags 0.
List current calls (err 0). TBS Index 255, call count 1, call list,
call index 1, state 3, flags 0, remote uri tel:qq
List current state of current calls (err 0). TBS Index 0, call count 1, call state list,
call index 1, state 3, flags 0.
Disable: stream 202EFF80
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Stop: stream 202EFF80
Disable: stream 202F6350
Audio Stream 202F6350 stopped with reason 0x13
Audio Stream 202EFF80 stopped with reason 0x13
Enable: stream 202EFF80 meta_count 1
Enable: stream 202F6350 meta_count 1
Init Audio SAI and CODEC, samplingRate :16000 bitWidth:16
Set default headphone volume 70
Start: stream 202F6350
Start: stream 202EFF80
Or, enter “call_accept 0 <call_index>” on the call_terminal side
accept call: TBS index , call index 1
Return code 0
call_terminal>> Control Point status update. A call has been accepted (err 0). TBS Index 0, call index 1
List current state of current calls (err 0). TBS Index 255, call count 1, call state list,
call index 1, state 3, flags 0.
List current calls (err 0). TBS Index 255, call count 1, call list,
call index 1, state 3, flags 0, remote uri tel:qq
List current state of current calls (err 0). TBS Index 0, call count 1, call state list,
call index 1, state 3, flags 0.
Disable: stream 202EFF80
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Stop: stream 202EFF80
Disable: stream 202F6350
Audio Stream 202F6350 stopped with reason 0x13
Audio Stream 202EFF80 stopped with reason 0x13
Enable: stream 202EFF80 meta_count 1
Enable: stream 202F6350 meta_count 1
Init Audio SAI and CODEC, samplingRate :16000 bitWidth:16
Set default headphone volume 70
Start: stream 202F6350
Start: stream 202EFF80
7.2 Accept the call by remote device. enter “remote_call_answer <call_index>” on the call_gateway side
List current state of current calls (err 0). TBS Index 255, call count 1, call state list,
call index 1, state 3, flags 1.
List current calls (err 0). TBS Index 255, call count 1, call list,
call index 1, state 3, flags 1, remote uri tel:qq
List current state of current calls (err 0). TBS Index 0, call count 1, call state list,
call index 1, state 3, flags 1.
Disable: stream 202EFF80
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Fail to send stream (error -77)
Stop: stream 202EFF80
Disable: stream 202F6350
Audio Stream 202F6350 stopped with reason 0x13
Audio Stream 202EFF80 stopped with reason 0x13
Enable: stream 202EFF80 meta_count 1
Enable: stream 202F6350 meta_count 1
Init Audio SAI and CODEC, samplingRate :16000 bitWidth:16
Set default headphone volume 70
Start: stream 202F6350
Start: stream 202EFF80