handsfree_ag
Overview
This example demonstrates the HFP Ag basic functionality, currently support simulate an incoming call, and the call could be answered and ended. The HFP Ag can connected a HFP HF device like headphone or device running HFP HF device.
Prepare the Demo
Open example’s project and build it.
Connect a USB cable between the PC host and the OpenSDA USB port on the target board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
The log below shows the output of the example in the terminal window. USB Host stack successfully initialized Bluetooth initialized
SHELL build: Mar 1 2021 Copyright 2020 NXP
the bellow commands have been supported: “bt”: BT related function USAGE: bt [discover|connect|disconnect|delete] discover start to find BT devices connect connect to the device that is found, for example: bt connect n (from 1) openaudio open audio connection without calls closeaudio close audio connection without calls sincall start an incoming call. aincall accept the call. eincall end an call. set_tag set phone num tag, for example: bt set_tag 123456789. select_codec codec select for codec Negotiation, for example: bt select_codec 2, it will select the codec 2 as codec. set_mic_volume update mic Volume, for example: bt set_mic_volume 14. set_speaker_volume update Speaker Volume, for example: bt set_speaker_volume 14. stwcincall start multiple an incoming call. disconnect disconnect current connection. delete delete all devices. Ensure to disconnect the HCI link connection with the peer device before attempting to delete the bonding information.
“discover” start to find BT devices, it will list all device can be found, usage
“connect” is used to connect to the device that is found, for example: bt connect n (from 1), usage : bt connect 1
“openaudio” is used to open audio connection without calls
“closeaudio” is used to close audio connection without calls
“sincall” is used to start an incoming call
“aincall” is used to accept an incoming call
“eincall” is used to end or reject an incoming call
“set_tag” is used to set phone num tag, for example: bt set_tag 123456789
“select_codec” is used to codec select for codec Negotiation, for example: bt select_codec 2, it will select the codec 2 as codec, usage: bt select_codec 2
“set_mic_volume” is used to set mic volume, the value is from 1 to 15, usage as: bt set_mic_volume 8
“set_speaker_volume” is used to set speaker volume, the value is from 1 to 15, usage as: bt set_speaker_volume 8
“stwcincall” to start multiple an incoming call, need run “sincall” is used to start an incoming call before run the command
“disconnect” to disconnect current connection
“delete” is used to delete all devices. Ensure to disconnect the HCI link connection with the peer device before attempting to delete the bonding information.
Note: There is a short noise can be heard at headset at the begin audio streaming when in running HFP Ag . The codec power on pop noise cannot eliminate.