Evaluate an Example Project
Supported Boards
Use the west extension west list_project to understand the board support scope for a specified example. All supported build command will be listed in output:
west list_project -p examples/demo_apps/hello_world [-t armgcc]
INFO: [ 1][west build -p always examples/demo_apps/hello_world --toolchain armgcc --config release -b evk9mimx8ulp -Dcore_id=cm33]
INFO: [ 2][west build -p always examples/demo_apps/hello_world --toolchain armgcc --config release -b evkbimxrt1050]
INFO: [ 3][west build -p always examples/demo_apps/hello_world --toolchain armgcc --config release -b evkbmimxrt1060]
INFO: [ 4][west build -p always examples/demo_apps/hello_world --toolchain armgcc --config release -b evkbmimxrt1170 -Dcore_id=cm4]
INFO: [ 5][west build -p always examples/demo_apps/hello_world --toolchain armgcc --config release -b evkbmimxrt1170 -Dcore_id=cm7]
INFO: [ 6][west build -p always examples/demo_apps/hello_world --toolchain armgcc --config release -b evkcmimxrt1060]
INFO: [ 7][west build -p always examples/demo_apps/hello_world --toolchain armgcc --config release -b evkmcimx7ulp]
...
Build the project
Use west build -h to see help information for west build command.
Compared to zephyr’s west build, MCUXpresso SDK’s west build command provides following additional options for mcux examples:
–toolchain: specify the toolchain for this build, default
armgcc.–config: value for
CMAKE_BUILD_TYPE, default debug.
Here are some typical usage for generating a SDK example:
# Generate example with default settings
west build -b frdmk22f examples/demo_apps/hello_world
# Just print cmake commands, do not execute it
west build -b frdmk22f examples/demo_apps/hello_world --dry-run
# Generate other toolchain like iar, default armgcc
west build -b frdmk22f examples/demo_apps/hello_world --toolchain iar
# Generate config type, default debug
west build -b frdmk22f examples/demo_apps/hello_world --config release
For multicore devices, you shall specify the corresponding core id by passing the command line argument -Dcore_id. For example
west build -b evkmimxrt1170 examples/demo_apps/hello_world --toolchain iar -Dcore_id=cm7 --config flexspi_nor_debug
For shield, please use the --shield to specify the shield to run, like
west build -b mimxrt700evk --shield a8974 examples examples/issdk_examples/sensors/fxls8974cf/fxls8974cf_poll -Dcore_id=cm33_core0
Sysbuild(System build)
To support multicore project building, we ported Sysbuild from Zephyr. It supports combine multiple projects for compilation. You can build all projects by adding --sysbuild for main application. For example:
west build -b evkmimxrt1170 --sysbuild ./examples/middleware/multicore/multicore_examples/hello_world/primary -Dcore_id=cm7 --config flexspi_nor_debug -p always
For more details, please refer to System build.
Config a project
Example in MCUXpresso SDK is configured and tested with pre-defined configuration. You can follow steps blow to change the configuration.
Run cmake configuration
west build -b frdmk22f examples/demo_apps/hello_world --cmake-only
Please note the project will be built without --cmake-only parameter.
Run guiconfig target
west build -t guiconfig
Then you will get the Kconfig GUI launched, like

You can reconfigure the project by selecting/deselecting Kconfig options.
After saving and closing the Kconfig GUI, you can directly run west build to build with the new configuration.
Flash
Note: Please refer Flash and Debug The Example to enable west flash/debug support.
Flash the hello_world example:
west flash -r linkserver
Debug
Start a gdb interface by following command:
west debug -r linkserver