Features
This section provides an overview of Bluetooth features, toolchain support, and RTOS support.
Bluetooth features
Bluetooth 5.0 compliant
Protocol support
L2CAP, GAP, GATT, RFCOMM, SDP, and SM
Note: The Enhanced Attribute (EATT) protocol is not supported in the current version. However, the support will be available in a future version.
Classic profile
SPP, A2DP, and HFP
LE profile
HTP, PXP, IPSP, HPS
Integrated the Fatfs based on USB Host MSD in SDK
Digital Audio Interface including PCM interface for HFP
Parent topic:Features
Toolchain support
IAR Embedded Workbench for ARM®
MCUXpresso IDE
Keil® MDK/μVision
Makefiles support with GCC from Arm Embedded
Note: For details on IDE Development tools version details, see Section 3, Development tools in MCUXpresso SDK Release Notes (document MCUXSDKMIMXRT106XRN). The Release Notes document is available at root/docs/ MCUXpresso SDK Release Notes for EVK-MIMXRT1060.pdf.
Parent topic:Features
RTOS support
FreeRTOSTMOS
Parent topic:Features
Parent topic:Overview