Hardware overview

This section provides information on hardware support and instructions to connect the CMWC1ZZABR-107-EVB adapter to the evaluation boards. The guide uses LPC55S69 as reference, but same steps apply to other supported products from the LPC55 family products.

Supported platforms

The SDK supports the following hardware:

  • LPCXpresso55S16

  • LPCXpresso55S28

  • LPCXpresso55S69

  • LPCXpresso55S3x/3x

  • EVK-MIMXRT1020

  • LPCXpresso54628

  • LPCXpresso54S018

  • LPCXpresso54S018M

Parent topic:Hardware overview

Assembly instructions

Mount the CMWC1ZZABR-107-EVB adapter to the mikroBUS connector on your board. Make sure that the pin labeling matches the pin orientation between the boards.

|

|

|

|

Parent topic:Hardware overview

Additional hardware

The additional hardware required includes:

  • USB A to micro USB cable

  • Personal computer

The Wi-Fi demo application does not require any special hardware configuration. However, when running the Wi-Fi demo, it is recommended to leave the development board jumper settings and configurations in the default state.

Parent topic:Hardware overview