cns_adc_software_trigger

Overview

The adc_software_trigger example shows how to software trigger ADC conversion.

In this example, ADC resolution is set as 16bit, the reference voltage is selected as the internal 1.8V bandgap, and input gain is set as 1. So the input voltage range is from 0 to 1.8V. Users can trigger ADC conversion by pressing any key in the terminal. ADC interrupt will be asserted once the conversion is completed.

The conversion result can be calculated via the following formula: Conversion Result = (Vin / Vref) * 32767

Supported Boards