gdma_wrap

Overview

This project shows how to use GDMA functional APIs to do the wrap transfer.

Both the source address and destination address can be wrapped.

In this example, there are 2 buffer, s_wrappedData is 16-byte buffer, s_unwrappedData is 64-byte buffer.

In case APP_GdmaSrcWrap, s_wrappedData is filled with 0, 1, 2, …, 15, s_unwrappedData is empty. GDMA copies s_wrappedData to s_unwrappedData, and the source address wrap is set to 16. When transfer finished, the s_unwrappedData is: 0, 1, 2, …, 15, 0, 1, 2, …, 15, 0, 1, 2, …, 15, 0, 1, 2, …, 15.

In case APP_GdmaDestWrap, s_unwrappedData is filled with 0, 1, 2, …, 63, s_wrappedData is empty. GDMA copies s_unwrappedData to s_wrappedData, and the destination address wrap is set to 16. When transfer finished, the s_wrappedData is: 48, 49, 50, …, 63.

The project checks the data and shows the result in terminal.

Supported Boards