lpc_dac_interrupt

Overview

The dac_interrupt example shows how to use DAC with interrupts and produce an arbitrary, user-defined waveform of selectable frequency.The output can be observed with an oscilloscope.

When the DAC’s double-buffer feature is enabled, any write to the CR register will only load the pre-buffer, which shares its register address with the CR register. The CR itself will be loaded from the pre-buffer whenever the counter reaches zero and the interrupt would occur. At the same time the counter is reloaded with the COUNTVAL register value. In the DAC ISR, user-defined waveform array would be transfered to pre-buffer in order.

Supported Boards