spi_interrupt_master

Overview

The spi_interrupt_master example shows how to use spi functional API to do interrupt transfer as a master:

In this example, the spi instance as master. Master sends a piece of data to slave, receive data from slave, and check if the data master received is correct. This example needs to work with spi_interrupt_slave example.

Supported Boards