lpspi_polling_b2b_transfer_slave

Overview

The lpspi_polling_b2b_transfer example shows how to use LPSPI driver in polling way:

In this example , we need two boards, one board used as LPSPI master and another board used as LPSPI slave. The file ‘lpspi_polling_b2b_transfer_slave.c’ includes the LPSPI slave code.

  1. LPSPI master send/received data to/from LPSPI slave in polling . (LPSPI Slave using interrupt to receive/send the data)

Supported Boards