queued_spi_polling_b2b_transfer_master
Overview
The queued_spi_polling_b2b_transfer examples show how to use QUEUEDSPI driver in polling way:
In this example we need two boards, one board is used as QUEUEDSPI master and another board is used as QUEUEDSPI slave. The file ‘queued_spi_polling_b2b_transfer_master.c’ includes the QUEUEDSPI master code.
QUEUEDSPI master sends/receiveds data to/from QUEUEDSPI slave in polling. (QUEUEDSPI Slave uses interrupt to receive/send the data)