ZPS Configuration Editor wizard
Before you can start to create a new ZigBee PRO stack configuration, the ZPS Configuration Editor plug-in must be installed in MCUXpresso.
To check if the plug-in is already installed, start MCUXpresso and select
File > New > Other from the main menu. Check that a Jennic option exists in the Select a Wizard dialogue box - expanding the Jennic option should show “ZBPro Configuration”, as illustrated in the screenshot below.
Selecting a Wizard
Using the wizard highlighted in the screenshot above, you can start to create a new ZigBee PRO configuration, as described in Section 12.4.1.
If the wizard is not present, install the ZPS Configuration Editor plug-in, which is supplied in the ZigBee 3.0 SDK.
Parent topic:ZPS Configuration Editor