ZPS_eAplAfGetNodeDescriptor

ZPS\_teStatus ZPS\_eAplAfGetNodeDescriptor\(
            ZPS\_tsAplAfNodeDescriptor *psDesc);

Description

This function copies the Node descriptor (for the local node) from the context area of the stack to the specified structure (the descriptor is returned through the function’s parameter).

Parent topic:ZPS_eAplAfGetNodeDescriptor

Parameters

* psDesc: Pointer to structure (see Section 8.2.1.1) to receive Node descriptor.

Parent topic:ZPS_eAplAfGetNodeDescriptor

Returns

Parent topic:ZPS_eAplAfGetNodeDescriptor

Parent topic:Descriptor functions