Descriptor functions
The AF Descriptor functions allow ZigBee descriptors for the local node to be copied to and from the context area of the ZigBee PRO stack. The functions are listed below.
ZPS_eAplAfGetNodeDescriptor
ZPS\_teStatus ZPS\_eAplAfGetNodeDescriptor\(
ZPS\_tsAplAfNodeDescriptor *psDesc);
Description
This function copies the Node descriptor (for the local node) from the context area of the stack to the specified structure (the descriptor is returned through the function’s parameter).
Parent topic:ZPS_eAplAfGetNodeDescriptor
Parameters
* psDesc: Pointer to structure (see Section 8.2.1.1) to receive Node descriptor.
Parent topic:ZPS_eAplAfGetNodeDescriptor
Returns
ZPS_E_SUCCESS
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplAfGetNodeDescriptor
Parent topic:Descriptor functions
ZPS_eAplAfGetNodePowerDescriptor
ZPS\_teStatus ZPS\_eAplAfGetNodePowerDescriptor\(
ZPS\_tsAplAfNodePowerDescriptor *psDesc);
Description
This function copies the Node Power descriptor (for the local node) from the context area of the stack to the specified structure (the descriptor is returned through the function’s parameter).
Parent topic:ZPS_eAplAfGetNodePowerDescriptor
Parameters
* psDesc Pointer to structure (see Section 8.2.1.2) to receive Node Power descriptor
Parent topic:ZPS_eAplAfGetNodePowerDescriptor
Returns
ZPS_E_SUCCESS
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplAfGetNodePowerDescriptor
Parent topic:Descriptor functions
ZPS_eAplAfGetSimpleDescriptor
ZPS\_teStatus ZPS\_eAplAfGetSimpleDescriptor\(
uint8 u8Endpoint,
ZPS\_tsAplAfSimpleDescriptor *psDesc);
Description
This function copies the Simple descriptor for the specified endpoint (on the local node) from the context area of the stack to the specified structure (the descriptor is returned through the function’s parameter).
Parent topic:ZPS_eAplAfGetSimpleDescriptor
Parameters
* psDesc Pointer to structure (see Section 8.2.1.3) to receive Simple descriptor
Parent topic:ZPS_eAplAfGetSimpleDescriptor
Returns
ZPS_E_SUCCESS
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplAfGetSimpleDescriptor
Parent topic:Descriptor functions
Parent topic:AF API functions